Zigbee Configuration

These instructions cover all Z-Stack sample applications. Configurables differ between standard Zigbee device types (ie. Coordinator, Router, End Device) and Green Power Devices (GPD).

Note

SysConfig will only make changes to selected files, listed in the Generated Files view. Any required changes to your application files must be done on your own.

Open An Example Project

Open the stand-alone SysConfig tool or import a SysConfig-enabled example project (found in the {SDK_INSTALL_DIR}/examples/syscfg_preview folder) and open the .syscfg file with the System Configuration Editor.

Zigbee Settings

In the RF STACKS → Z-Stack view, you can configure Zigbee stack parameters. Parameters are explained in the tooltip that appears when you hover over it but further explanations are provided in the Z-Stack Overview and 4. Migrate Configuration Header File sections. Zigbee stack settings are stored in default/sysconfig/ti_zstack_config.h (which appears after building the project).

Here is an example of what you would see for a coordinator example:

../_images/syscfg_settings_zigbee.png

Device Type and Power Management Configuration

Standard Zigbee Device

The Device Type (Coordinator, Router, End Device) is pre-determined for each example project and cannot be changed. The Power Mode of Operation (see End Device) and poll period (see Child Management) are only configurable for End Device types.

Green Power Device

The device type is Green Power Device. The Power Mode of Operation determines whether the Green Power Device is assumed to have a constant power source (eg. battery) or not. For more details, see BATTERYLESS_DEVICE in Green Power Device Configuration.

Radio Configuration

Standard Zigbee Device

The basic Radio parameters to consider for the Zigbee stack include primary and secondary channel mask selection (Configuring Channel) as well as minimum transmissions (Network Manager).

Green Power Device

Configure the channel which the GPD will operate on.

Network Configuration

Standard Zigbee Device

The network configurations involve basic Zigbee network settings, such as the PAN ID (Configuring the PAN ID and Network to Join), extended PAN ID (Extended PAN IDs), default network key (Security), and link status jitter mask (Asynchronous Links).

Green Power Device

Green Power Device Type determines what function the GPD embodies in the network (eg. switch, temperature sensor, etc). Green Power Device ID Type determines how the GPD identifies itself (eg. Configurable GPD ID, IEEE address). If Configurable GPD ID is selected, the developer may choose a 32-bit ID which the GPD will use.

Security Configuration

Green Power Device

Security settings which are specific towards Green Power devices, such as level and key type, and key, which are further discussed in Green Power Device Configuration.

Advanced Configuration

Standard Zigbee Device

The advanced configuration parameters require in-depth knowledge of the Zigbee network operation. They are separated into different sections for joining (Miscellaneous), routing (Routing Protocol), packet sending (End-to-End Acknowledgements), and maximum table sizes (Network Address Assignment). Specific poll rates (Portable Devices) are only configurable for End Device projects. Several of these settings are also explained in Network Configurations.

Green Power Device

Data Frame Retries determines how many times the GPD will transmit each packet. Auto-commissioning determines whether the GPD will set the auto-commissioning bit in the packets. Radio Receive After Transmit determines whether the GPD should expect to receive a packet after transmitting. Sequence Number Capability determines whether the GPD will use sequential MAC sequence numbers.

Adjust Your Application

When you have finished adjusting the parameters, save the .syscfg file.

You can preview the files which will be generated by clicking the <> symbol. In this example, ti_devices_config.c, ti_drivers_config.c/h, and ti_zstack_config.h were generated respectively by the TI DEVICES, TI DRIVERS, and RF STACKS → Z-Stack views.

../_images/show_generated_zigbee.png

If you are using the System Configuration stand-alone tool, you will have to import every generated file to your IDE. For the SysConfig CCS plug-in, you can generate all the files by building your project. After the build has completed, you will find the generated files in the output folder of your project, called default/syscfg. All parameters configured in the Zigbee view of SysConfig will result in a #define in ti_zstack_config.h alongside other macros which are not included in SysConfig.

Attention

Whenever you re-build the project, SysConfig will re-generate the files. Because of this, any changes made directly to ti_zstack_config.h will be overwritten.