module ti.uia.family.dm.dra7xx.TimestampProvider

System-wide timestamp provider

This timestamp provider is used by UIA to provide a common time base for all processors. This allows System Analyzer to correlate the log events from all processors to a common time base. Event correlation is required for the multi-core execution graph. Use this module as the global timestamp proxy for the ti.uia.runtime.LogSync module. [ more ... ]
C synopsis target-domain sourced in ti/uia/family/dm/dra7xx/TimestampProvider.xdc
#include <ti/uia/family/dm/dra7xx/TimestampProvider.h>
Functions common to all ITimestampClient modules
Bits32 
Void 
Void 
Functions common to all target modules
Typedefs
typedef struct
typedef enum
Constants
extern const Int 
extern const Bool 
extern const Int 
extern const Log_Event 
extern const Log_Event 
extern const Types_FreqHz 
extern const Types_FreqHz 
extern const Bool 
extern const UInt 
extern const UInt 
 
DETAILS
This timestamp provider is used by UIA to provide a common time base for all processors. This allows System Analyzer to correlate the log events from all processors to a common time base. Event correlation is required for the multi-core execution graph. Use this module as the global timestamp proxy for the ti.uia.runtime.LogSync module.
This module requires the use of a timer to provide a common system tick. The timer needs to have access to the 32 KHz clock. Not all timers are suitable for use by this module. See the timerId configuration parameter for a list of recommended timers. Exactly one processor must be the owner of the timer. See owner for details.
Ledgers are used internally by this module to keep track of the other processors in the system. The ledgers are shared across processor boundaries. You must provide the base address of a ledger so that all processors know where to find it. See the ledgers configuration parameter for details. There are two types of ledgers: a group ledger, and a private ledger. One group ledger is mandatory, private ledgers are typically used by the EVE processors. Ledgers are defined by the role used to access them. See the Role enumeration for details.
CONFIGURATION EXAMPLE
This is a four processor example: DSP1 DSP2 EVE1 EVE2. In this example, DSP1 is to be the owner of the timer. Three ledgers will be used, one group ledger and two private ledgers. The group ledger is used by DSP1 and DSP2. One private ledger is used by DSP1 and EVE1. The other private ledger is used by DSP2 and EVE2.
Add the following to your DSP1 configuration script.
  // add Timer3 (id=2) to SYS/BIOS available mask //
  var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');
  TimerSupport.availMask |= (0x1 << 2);

  // configure timestamp proxy //
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');
  TimestampProvider.timerId = 2;
  TimestampProvider.owner = true;
  TimestampProvider.eventId = 65;
  TimestampProvider.cpuIntrNum = 13;
  TimestampProvider.syncInterval = 33;

  // group ledger
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Ledger_PEER,
          base: 0x40500000,
          size: 2, // DSP1 DSP2
          index: 0 // DSP1
      })
 );

  // eve1 ledger
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_USER,
          base: 0x42020000
      })
  );

  // enable event correlation
  var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
  LogSync.GlobalTimestampProxy = TimestampProvider;
  LogSync.enableEventCorrelationForJTAG = true;
Add the following to your DSP2 configuration script.
  // configure timestamp proxy for event correlation
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');

  TimestampProvider.timerId = 2;
  TimestampProvider.owner = false; // DSP1 is owner
  TimestampProvider.eventId = 65;
  TimestampProvider.cpuIntrNum = 13;
  TimestampProvider.syncInterval = 33;

  // group ledger
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_PEER,
          base: 0x40500000,
          size: 2, // DSP1 DSP2
          index: 1 // DSP2
      })
 );

  // eve2 ledger
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_USER,
          base: 0x42120000
      })
  );

  // enable event correlation
  var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
  LogSync.GlobalTimestampProxy = TimestampProvider;
  LogSync.enableEventCorrelationForJTAG = true;
Add the following to your EVE1 configuration script.
  // configure timestamp proxy for event correlation
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');

  TimestampProvider.timerId = 2;
  TimestampProvider.owner = false; // DSP1 is owner
  TimestampProvider.eventId = 35;
  TimestampProvider.cpuIntrNum = 9;
  TimestampProvider.syncInterval = 33;

  // use private ledger, role = owner
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_OWNER,
          base: 0x40020000
      })
 );

  // enable event correlation
  var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
  LogSync.GlobalTimestampProxy = TimestampProvider;
  LogSync.enableEventCorrelationForJTAG = true;
Add the following to your EVE2 configuration script.
  // configure timestamp proxy for event correlation
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');

  TimestampProvider.timerId = 2;
  TimestampProvider.owner = false; // DSP1 is owner
  TimestampProvider.eventId = 35;
  TimestampProvider.cpuIntrNum = 9;
  TimestampProvider.syncInterval = 33;

  // use private ledger, role = owner
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_OWNER,
          base: 0x40020000
      })
 );

  // enable event correlation
  var LogSync = xdc.useModule('ti.uia.runtime.LogSync');
  LogSync.GlobalTimestampProxy = TimestampProvider;
  LogSync.enableEventCorrelationForJTAG = true;
CPU FREQUENCY CONFIGURATION
In order for event correlation to be accurate, the cpu frequency must be set as accurately as possible. This module can be used to determine you actual cpu frequency.
Enable the timestamp sample buffer with the estCpuFreq configuration parameter. Run your program continuously for 30 seconds. Use ROV to view the cpu frequency in the TimestampProvider module view.
Once you have determined your cpu frequency, use that value to configure the SYS/BIOS cpu frequency.
  var BIOS = xdc.useModule('ti.sysbios.BIOS');
  BIOS.cpuFreq = { hi: 0, lo: 609024002 };
Hint: disable the estCpuFreq when done to reduce your data footprint.
 
enum TimestampProvider_Role

Define roles for each ledger instance

C synopsis target-domain
typedef enum TimestampProvider_Role {
    TimestampProvider_Role_PEER,
    // shared by multiple processors
    TimestampProvider_Role_OWNER,
    // shared with one remote processor
    TimestampProvider_Role_USER
    // shared with one remote processor
} TimestampProvider_Role;
 
DETAILS
There may be multiple ledger instances in a system. There are two types of ledgers: 1. a group ledger, and 2. a private ledger. A group ledger may have two or more users. A private ledger has exactly two users. When a processor creates a private ledger, that processor may not create any additional ledgers of any type. A private ledger is typicaly used by the ARP32 processor.
The ledger type is identified by the role used to access it.
Role_PEER
This role is used to access a group ledger instance. This ledger instance is used by multiple processors. The ledger is an array of GroupLedgerElem elements. Each processor uses one entry in the ledger. The size of the ledger must equal the number of users.

All users of this ledger are peers. The ledger is not created by any processor, it must be defined in the memory map.

Role_OWNER
This role is used to access a private ledger. This ledger is used by only two processors: the local processor (the owner) and a remote processor (the user). The ledger is allocated in the local processor's memory map. This same ledger must be defined by a Role_USER role on one other processor.

Role_USER
This role is used to access a private ledger. This role is the complement of the Role_OWNER role. When using a private ledger, the actual ledger is created by the other processor.

A processor using the Role_USER role, will access the ledger with the given address, but it does not allocate the ledger.

It is possible to access multiple private ledgers from the same processor. Each Role_USER corresponds to a private ledger created by another processor.

 
struct TimestampProvider_Ledger

Define a ledger used in the system

C synopsis target-domain
typedef struct TimestampProvider_Ledger {
    TimestampProvider_Role role;
    // role used to access the ledger
    Ptr base;
    // base address of the ledger
    Int size;
    // number of users
    Int index;
    // entry assigned to this processor
} TimestampProvider_Ledger;
 
FIELDS
role — Defines how this processor will be using the ledger. The role also implicitly defines which type of ledger is created. See the Role enumeration for details.
base — The base address of the ledger as seen by the local processor.
size — The number of users of the current ledger. When adding a new user to a ledger, be sure to update this value for all processors using the same ledger.
index — The entry index in the ledger to be used by this processor. Each processor must have its own unique entry. The index is zero based (as in array indexing). Index values range from 0 - (size-1).
DETAILS
A ledger is used to keep track of which processors are running. Depending on the ledger role, there can be two or more users of the same ledger instance. You can define multiple ledgers. See ledgers for examples of creating ledgers.
 
config TimestampProvider_L_latch  // module-wide

Log event raised at the end of the timer isr

C synopsis target-domain
extern const Log_Event TimestampProvider_L_latch;
 
DETAILS
The timer isr maintains a global tick value used by System Analyzer to correlate the log events across processor boundaries. This event is raised at the end of the timer isr. The latch count should be the same on all processors. The isr timestamp is also reported. This value can be used to measure the accuracy of the event correlation. The isr timestamp is captured at the very beginning of the timer isr.
 
config TimestampProvider_L_suspend  // module-wide

Log event raised when loggers are to be suspended

C synopsis target-domain
extern const Log_Event TimestampProvider_L_suspend;
 
DETAILS
The module has determined that the system state is not nominal. To preserve the events in the log buffers leading up to this point, the loggers will be suspended. This event is raised shortly before the loggers are actually suspended.
 
config TimestampProvider_cpuIntrNum  // module-wide

Specify cpu interrupt to receive timer interrupt

C synopsis target-domain
extern const Int TimestampProvider_cpuIntrNum;
 
DETAILS
For accurate event correlation in System Analyzer, it is recommended not to share this interrupt.
The following table indicates possible interrupt numbers, but this is device specific. Please consult your manual.
Processor Timer ID
DSP 4-15
EVE 8-11
 
config TimestampProvider_estCpuFreq  // module-wide

Estimate the cpu frequency using timestamp sample buffer

C synopsis target-domain
extern const Bool TimestampProvider_estCpuFreq;
 
DETAILS
When enabled, this module will save timestamps in the sample buffer which are then used to calculate an estimate of the cpu frequency. Run the processor continuously for 30 seconds to ensure the sample buffer is full. Open ROV and select the Module tab. The calculated cpu frequency is displayed in the estCpuFreq column. The timestamp samples are displayed in the Sample Buffer tab.
Set this config param to false to reduce the data footprint in your released product.
 
config TimestampProvider_eventId  // module-wide

Specify interrupt controller event to receive timer interrupt

C synopsis target-domain
extern const Int TimestampProvider_eventId;
 
DETAILS
The eventId specifies which interrupt controller event should receive the timer interrupt. This value is used to route the timer interrupt through the Interrupt Crossbar to the interrupt controller event. It is also used to route the interrupt event to the cpu interrupt specified in cpuIntrNum.
The following table indicates possible event ids, but this is device specific. Please consult your manual.
Processor Event ID
DSP 63-78, 81
EVE 32-39
 
config TimestampProvider_ledgers  // module-wide

Define the ledgers to be managed by this processor

C synopsis target-domain
extern const TimestampProvider_Ledger TimestampProvider_ledgers[length];
 
DETAILS
Ledgers are used to keep track of the other processors. This is needed to support the auto-logging feature and to issue LogSync events. Each processor must define at least one ledger.
There are two types of ledgers: a group ledger, and a private ledger. See the Role enumeration for details.
Use as few ledgers as possible. However, some system constraints will require additional ledgers. For example, the EVE processors have very slow data access to on-chip or external memory. Therefore, we recommend that each EVE processor use a private ledger. Place the private ledger in DMEM to ensure fast memory access.
Add the following to your EVE1 configuration script.
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');

  // use private ledger, role = owner
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_OWNER,
          base: 0x40020000
      })
 );
Each private ledger has exactly two users: an owner (Role_OWNER) and a user (Role_USER). In the example above, the EVE would always be the owner. Typically, the DSP would be the corresponding user.
Add the following to your DSP1 configuration script.
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');

  // eve1 ledger, role = user
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_USER,
          base: 0x42020000
      })
 );
Note in the example above, the EVE defines the ledger address using its local address (e.g. 0x40020000). However, the DSP must use the interconnect address (e.g. 0x42020000).
For the remaining processors in the system, you could use one group ledger. All processors using the same group must agree on the ledger address, and the number of entries. Each processor must be assigned its own entry in the ledger.
The following example defines a single group ledger used by two processors: DSP1 and DSP2. Add the following to your DSP1 configuration script.
  var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');

  // group ledger, role = peer
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Ledger_PEER,
          base: 0x40500000,
          size: 2, // DSP1 DSP2
          index: 0 // DSP1
      })
 );
Add the following to your DSP2 configuration script.
  var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');

  // group ledger, role = peer
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_PEER,
          base: 0x40500000,
          size: 2, // DSP1 DSP2
          index: 1 // DSP2
      })
 );
It is also possible to partition the remaining processors into groups and assign a group ledger to each processor group. This might be done to support independent application domains. However, one requirement is that the processor which owns the timer must participate in all group ledgers. For example, if DSP1 has
  TimestampProvider.owner = true;
then DSP1 must participate in all group ledgers (i.e. Role_PEER).
 
config TimestampProvider_maxBusClockFreq  // module-wide

The highest bus clock frequency used to drive the timer

C synopsis target-domain
extern const Types_FreqHz TimestampProvider_maxBusClockFreq;
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 MSBs of the highest bus clock frequency used to drive the timer.
 
config TimestampProvider_maxTimerClockFreq  // module-wide

The highest timer clock frequency

C synopsis target-domain
extern const Types_FreqHz TimestampProvider_maxTimerClockFreq;
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 LSBs of the highest timer clock frequency (i.e. ticksPerSecond).
 
config TimestampProvider_owner  // module-wide

Determine ownership of the timer

C synopsis target-domain
extern const Bool TimestampProvider_owner;
 
DETAILS
When set to true, the timer will be enabled and configured during the boot phase. The owner should run before any other processor using this same timer. Only one processor should be configured as the owner of the timer. This processor will also listen for the timer interrupt and acknowledge it.
When set to false, it is expected that another processor will enable and configure the timer. This processor will simply listen for the timer interrupt and acknowledge it.
Note: The ARP32 does not support timer ownership. This config param must always be false when running on the ARP32.
 
config TimestampProvider_syncInterval  // module-wide

Specify the interval for logging sync events

C synopsis target-domain
extern const UInt TimestampProvider_syncInterval;
 
DETAILS
UIA Sync events are used by System Analyzer to correlate the events from each processor onto a global time base. Only the last sync event is actually used.
This configuration parameter specifies how frequently the sync events should be raised. In order to maintain accurate event correlation, you should raise one sync event within each log data window. For example, if your log buffer contains 100 ms of data, then you should raise a sync event each 0.1 seconds (100 ms = 0.1 sec).
Each syncInterval is 0.001953125 seconds. Divide the data window by this value to get the syncInterval (round down).
      0.1 sec / 0.001953125 sec = 51.2

      TimestampProvider.syncInterval = 51;
When using multiple logger instances, the data window for each instance is probably different. Use System Analyzer to measure the data overlap of your region of interest. Use the length of this region to calculate the syncInterval.
The syncInterval should be as large as possible to reduce logging overhead, yet small enough to yield accurate event correlation.
 
config TimestampProvider_timerId  // module-wide

Identify which timer to use as the timestamp clock source

C synopsis target-domain
extern const UInt TimestampProvider_timerId;
 
DETAILS
The timers are named Timer1-Timer16; their corresponding ids are 0-15 (e.g. for Timer3, use id=2). Not all timers are appropriate clock sources for this module. Use one of the following timers:
Timer Name Description
Timer[3,4,9,11,13,14,15,16] PD_L4PER power domain
Timer[5,6,7,8] PD_IPU power domain
All executables must use the same timer in order to support event correlation in System Analyzer.
 
TimestampProvider_get32()  // module-wide

Return a 32-bit timestamp

C synopsis target-domain
Bits32 TimestampProvider_get32();
 
RETURNS
Returns a 32-bit timestamp value. Use getFreq to convert this value into units of real time.
SEE
 
TimestampProvider_get64()  // module-wide

Return a 64-bit timestamp

C synopsis target-domain
Void TimestampProvider_get64(Types_Timestamp64 *result);
 
ARGUMENTS
result — pointer to 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide timestamp value where the current timestamp is written.
If the underlying hardware does not support 64-bit resolution, the hi field of result is always set to 0; see xdc.runtime.Types.Timestamp64. So, it is possible for the lo field to wrap around without any change to the hi field. Use getFreq to convert this value into units of real time.
SEE
 
TimestampProvider_getFreq()  // module-wide

Get the timestamp timer's frequency (in Hz)

C synopsis target-domain
Void TimestampProvider_getFreq(Types_FreqHz *freq);
 
ARGUMENTS
freq — pointer to a 64-bit result
This parameter is a pointer to a structure representing a 64-bit wide frequency value where the timer's frequency (in Hz) is written; see xdc.runtime.Types.FreqHz. This function provides a way of converting timestamp values into units of real time.
SEE
Module-Wide Built-Ins

C synopsis target-domain
Types_ModuleId TimestampProvider_Module_id();
// Get this module's unique id
 
Bool TimestampProvider_Module_startupDone();
// Test if this module has completed startup
 
IHeap_Handle TimestampProvider_Module_heap();
// The heap from which this module allocates memory
 
Bool TimestampProvider_Module_hasMask();
// Test whether this module has a diagnostics mask
 
Bits16 TimestampProvider_Module_getMask();
// Returns the diagnostics mask for this module
 
Void TimestampProvider_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
 
Configuration settings sourced in ti/uia/family/dm/dra7xx/TimestampProvider.xdc
var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');
module-wide constants & types
 
        obj.base// base address of the ledger = Ptr  ...
        obj.size// number of users = Int  ...
        obj.index// entry assigned to this processor = Int  ...
module-wide config parameters
        mask: Diags.INFO,
        msg: "L_latch: latch=0x%x:0x%x, isr ts=0x%x:0x%x"
    };
        mask: Diags.INFO,
        msg: "L_suspend: loggers suspended"
    };
 
 
 
enum TimestampProvider.Role

Define roles for each ledger instance

Configuration settings
values of type TimestampProvider.Role
    const TimestampProvider.Role_PEER;
    // shared by multiple processors
    const TimestampProvider.Role_OWNER;
    // shared with one remote processor
    const TimestampProvider.Role_USER;
    // shared with one remote processor
 
DETAILS
There may be multiple ledger instances in a system. There are two types of ledgers: 1. a group ledger, and 2. a private ledger. A group ledger may have two or more users. A private ledger has exactly two users. When a processor creates a private ledger, that processor may not create any additional ledgers of any type. A private ledger is typicaly used by the ARP32 processor.
The ledger type is identified by the role used to access it.
Role_PEER
This role is used to access a group ledger instance. This ledger instance is used by multiple processors. The ledger is an array of GroupLedgerElem elements. Each processor uses one entry in the ledger. The size of the ledger must equal the number of users.

All users of this ledger are peers. The ledger is not created by any processor, it must be defined in the memory map.

Role_OWNER
This role is used to access a private ledger. This ledger is used by only two processors: the local processor (the owner) and a remote processor (the user). The ledger is allocated in the local processor's memory map. This same ledger must be defined by a Role_USER role on one other processor.

Role_USER
This role is used to access a private ledger. This role is the complement of the Role_OWNER role. When using a private ledger, the actual ledger is created by the other processor.

A processor using the Role_USER role, will access the ledger with the given address, but it does not allocate the ledger.

It is possible to access multiple private ledgers from the same processor. Each Role_USER corresponds to a private ledger created by another processor.

C SYNOPSIS
 
struct TimestampProvider.Ledger

Define a ledger used in the system

Configuration settings
var obj = new TimestampProvider.Ledger;
 
    obj.role = TimestampProvider.Role  ...
    // role used to access the ledger
    obj.base = Ptr  ...
    // base address of the ledger
    obj.size = Int  ...
    // number of users
    obj.index = Int  ...
    // entry assigned to this processor
 
FIELDS
role — Defines how this processor will be using the ledger. The role also implicitly defines which type of ledger is created. See the Role enumeration for details.
base — The base address of the ledger as seen by the local processor.
size — The number of users of the current ledger. When adding a new user to a ledger, be sure to update this value for all processors using the same ledger.
index — The entry index in the ledger to be used by this processor. Each processor must have its own unique entry. The index is zero based (as in array indexing). Index values range from 0 - (size-1).
DETAILS
A ledger is used to keep track of which processors are running. Depending on the ledger role, there can be two or more users of the same ledger instance. You can define multiple ledgers. See ledgers for examples of creating ledgers.
C SYNOPSIS
 
config TimestampProvider.L_latch  // module-wide

Log event raised at the end of the timer isr

Configuration settings
TimestampProvider.L_latch = Log.EventDesc {
    mask: Diags.INFO,
    msg: "L_latch: latch=0x%x:0x%x, isr ts=0x%x:0x%x"
};
 
DETAILS
The timer isr maintains a global tick value used by System Analyzer to correlate the log events across processor boundaries. This event is raised at the end of the timer isr. The latch count should be the same on all processors. The isr timestamp is also reported. This value can be used to measure the accuracy of the event correlation. The isr timestamp is captured at the very beginning of the timer isr.
C SYNOPSIS
 
config TimestampProvider.L_suspend  // module-wide

Log event raised when loggers are to be suspended

Configuration settings
TimestampProvider.L_suspend = Log.EventDesc {
    mask: Diags.INFO,
    msg: "L_suspend: loggers suspended"
};
 
DETAILS
The module has determined that the system state is not nominal. To preserve the events in the log buffers leading up to this point, the loggers will be suspended. This event is raised shortly before the loggers are actually suspended.
C SYNOPSIS
 
config TimestampProvider.cpuIntrNum  // module-wide

Specify cpu interrupt to receive timer interrupt

Configuration settings
TimestampProvider.cpuIntrNum = Int undefined;
 
DETAILS
For accurate event correlation in System Analyzer, it is recommended not to share this interrupt.
The following table indicates possible interrupt numbers, but this is device specific. Please consult your manual.
Processor Timer ID
DSP 4-15
EVE 8-11
C SYNOPSIS
 
config TimestampProvider.estCpuFreq  // module-wide

Estimate the cpu frequency using timestamp sample buffer

Configuration settings
TimestampProvider.estCpuFreq = Bool false;
 
DETAILS
When enabled, this module will save timestamps in the sample buffer which are then used to calculate an estimate of the cpu frequency. Run the processor continuously for 30 seconds to ensure the sample buffer is full. Open ROV and select the Module tab. The calculated cpu frequency is displayed in the estCpuFreq column. The timestamp samples are displayed in the Sample Buffer tab.
Set this config param to false to reduce the data footprint in your released product.
C SYNOPSIS
 
config TimestampProvider.eventId  // module-wide

Specify interrupt controller event to receive timer interrupt

Configuration settings
TimestampProvider.eventId = Int undefined;
 
DETAILS
The eventId specifies which interrupt controller event should receive the timer interrupt. This value is used to route the timer interrupt through the Interrupt Crossbar to the interrupt controller event. It is also used to route the interrupt event to the cpu interrupt specified in cpuIntrNum.
The following table indicates possible event ids, but this is device specific. Please consult your manual.
Processor Event ID
DSP 63-78, 81
EVE 32-39
C SYNOPSIS
 
config TimestampProvider.ledgers  // module-wide

Define the ledgers to be managed by this processor

Configuration settings
TimestampProvider.ledgers = TimestampProvider.Ledger[length] undefined;
 
DETAILS
Ledgers are used to keep track of the other processors. This is needed to support the auto-logging feature and to issue LogSync events. Each processor must define at least one ledger.
There are two types of ledgers: a group ledger, and a private ledger. See the Role enumeration for details.
Use as few ledgers as possible. However, some system constraints will require additional ledgers. For example, the EVE processors have very slow data access to on-chip or external memory. Therefore, we recommend that each EVE processor use a private ledger. Place the private ledger in DMEM to ensure fast memory access.
Add the following to your EVE1 configuration script.
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');

  // use private ledger, role = owner
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_OWNER,
          base: 0x40020000
      })
 );
Each private ledger has exactly two users: an owner (Role_OWNER) and a user (Role_USER). In the example above, the EVE would always be the owner. Typically, the DSP would be the corresponding user.
Add the following to your DSP1 configuration script.
  var TimestampProvider = xdc.useModule('ti.uia.family.dm.dra7xx.TimestampProvider');

  // eve1 ledger, role = user
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_USER,
          base: 0x42020000
      })
 );
Note in the example above, the EVE defines the ledger address using its local address (e.g. 0x40020000). However, the DSP must use the interconnect address (e.g. 0x42020000).
For the remaining processors in the system, you could use one group ledger. All processors using the same group must agree on the ledger address, and the number of entries. Each processor must be assigned its own entry in the ledger.
The following example defines a single group ledger used by two processors: DSP1 and DSP2. Add the following to your DSP1 configuration script.
  var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');

  // group ledger, role = peer
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Ledger_PEER,
          base: 0x40500000,
          size: 2, // DSP1 DSP2
          index: 0 // DSP1
      })
 );
Add the following to your DSP2 configuration script.
  var TimerSupport = xdc.useModule('ti.sysbios.family.shared.vayu.TimerSupport');

  // group ledger, role = peer
  TimestampProvider.ledgers.$add(
      new TimestampProvider.Ledger({
          role: TimestampProvider.Role_PEER,
          base: 0x40500000,
          size: 2, // DSP1 DSP2
          index: 1 // DSP2
      })
 );
It is also possible to partition the remaining processors into groups and assign a group ledger to each processor group. This might be done to support independent application domains. However, one requirement is that the processor which owns the timer must participate in all group ledgers. For example, if DSP1 has
  TimestampProvider.owner = true;
then DSP1 must participate in all group ledgers (i.e. Role_PEER).
C SYNOPSIS
 
config TimestampProvider.maxBusClockFreq  // module-wide

The highest bus clock frequency used to drive the timer

Configuration settings
TimestampProvider.maxBusClockFreq = Types.FreqHz undefined;
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 MSBs of the highest bus clock frequency used to drive the timer.
C SYNOPSIS
 
config TimestampProvider.maxTimerClockFreq  // module-wide

The highest timer clock frequency

Configuration settings
TimestampProvider.maxTimerClockFreq = Types.FreqHz undefined;
 
DETAILS
The default ticks per second rate of the timer is calculated by dividing the timer's bus clock frequency by the cyclesPerTick config parameter.
RETURNS
the 32 LSBs of the highest timer clock frequency (i.e. ticksPerSecond).
C SYNOPSIS
 
config TimestampProvider.owner  // module-wide

Determine ownership of the timer

Configuration settings
TimestampProvider.owner = Bool undefined;
 
DETAILS
When set to true, the timer will be enabled and configured during the boot phase. The owner should run before any other processor using this same timer. Only one processor should be configured as the owner of the timer. This processor will also listen for the timer interrupt and acknowledge it.
When set to false, it is expected that another processor will enable and configure the timer. This processor will simply listen for the timer interrupt and acknowledge it.
Note: The ARP32 does not support timer ownership. This config param must always be false when running on the ARP32.
C SYNOPSIS
 
config TimestampProvider.syncInterval  // module-wide

Specify the interval for logging sync events

Configuration settings
TimestampProvider.syncInterval = UInt 50;
 
DETAILS
UIA Sync events are used by System Analyzer to correlate the events from each processor onto a global time base. Only the last sync event is actually used.
This configuration parameter specifies how frequently the sync events should be raised. In order to maintain accurate event correlation, you should raise one sync event within each log data window. For example, if your log buffer contains 100 ms of data, then you should raise a sync event each 0.1 seconds (100 ms = 0.1 sec).
Each syncInterval is 0.001953125 seconds. Divide the data window by this value to get the syncInterval (round down).
      0.1 sec / 0.001953125 sec = 51.2

      TimestampProvider.syncInterval = 51;
When using multiple logger instances, the data window for each instance is probably different. Use System Analyzer to measure the data overlap of your region of interest. Use the length of this region to calculate the syncInterval.
The syncInterval should be as large as possible to reduce logging overhead, yet small enough to yield accurate event correlation.
C SYNOPSIS
 
config TimestampProvider.timerId  // module-wide

Identify which timer to use as the timestamp clock source

Configuration settings
TimestampProvider.timerId = UInt undefined;
 
DETAILS
The timers are named Timer1-Timer16; their corresponding ids are 0-15 (e.g. for Timer3, use id=2). Not all timers are appropriate clock sources for this module. Use one of the following timers:
Timer Name Description
Timer[3,4,9,11,13,14,15,16] PD_L4PER power domain
Timer[5,6,7,8] PD_IPU power domain
All executables must use the same timer in order to support event correlation in System Analyzer.
C SYNOPSIS
 
metaonly config TimestampProvider.common$  // module-wide

Common module configuration parameters

Configuration settings
TimestampProvider.common$ = Types.Common$ undefined;
 
DETAILS
All modules have this configuration parameter. Its name contains the '$' character to ensure it does not conflict with configuration parameters declared by the module. This allows new configuration parameters to be added in the future without any chance of breaking existing modules.
generated on Wed, 28 Aug 2019 19:03:36 GMT