![]() |
![]() |
UART2 Global configuration. More...
#include <UART2.h>
Data Fields | |
UART2_FxnTable const * | fxnTablePtr |
void * | object |
void const * | hwAttrs |
UART2 Global configuration.
The UART2_Config structure contains a set of pointers used to characterize the UART2 driver implementation.
UART2_FxnTable const* UART2_Config::fxnTablePtr |
Pointer to a table of driver-specific implementations of UART APIs
void* UART2_Config::object |
Pointer to a driver specific data object
void const* UART2_Config::hwAttrs |
Pointer to a driver specific hardware attributes structure