Functions | Variables
doxygen_drivers.txt File Reference

Functions

This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming interface (API) which enables seamless migration across the SimpleLink SDK portfolio. Unless specifically stated otherwise
 [drivers_common_overview] More...
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating system (RTOS) application. All TI-Driver implementations utilize the Power driver APIs to ensure low power consumption at all times. The drivers support TI-RTOS(SYS/BIOS) and NoRTOS with examples provided for each variant. Lastly
 

Variables

This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par Features
 
This file contains snippets to be used in the TI Driver s documentation *******************************************************************************TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par block execution
 

Function Documentation

§ interface()

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming interface ( API  )

[drivers_common_overview]

§ system()

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating system ( RTOS  )

Variable Documentation

§ Features

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par Features

§ execution

This file contains snippets to be used in the TI Driver s documentation******************************************************************************* TI Drivers is a collective of peripheral drivers for TI s SimpleLink portfolio The drivers are centered around a portable application programming TI Drivers are designed to be thread safe and work seamlessly inside of a real time operating the drivers are supported by SysConfig to enable easy re configuration of the drivers par block execution
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale