Ubiqua Protocol Analyzer¶
Install the Required Software¶
Download and install the following software:
- Ubiqua Protocol Analyzer software
- SmartRF Protocol Packet Sniffer, which contains sniffer firmware for the CC2531
- Flash Programmer, used to program the CC2531
Note
Download SmartRF Protocol Packet Sniffer and SmartRF Flash Programmer, not SmartRF Packet Sniffer 2 and SmartRF Flash Programmer 2.
Required Hardware¶
It is recommended to use the CC2531 USB Dongle with Ubiqua Protocol Analyzer. The device comes pre-programmed with the packet sniffer firmware. However, if it is not programmed with the sniffer firmware, the CC-Debugger is required to flash the device.
The Cebal driver must be installed to use the CC-Debugger. The driver should already be installed if you have installed Flash Programmer. This can be verified by connecting a device to the debugger, opening up Flash Programmer, and observing the device showing up as connected.
Ubiqua Protocol Analyzer also provides the necessary files for installing the Cebal driver.
The installation files are found under C:\Program Files
(x86)\Ubilogix\Drivers\TI\, with cebal2.* files for 32-bit Windows and
cebal2_x64.* files for 64-bit Windows. Depending on which Windows version
you are using, refer to a corresponding guide for how to install Windows
drivers.
Hardware Setup¶
Connect the CC2531 USB Dongle to the computer with Ubiqua installed.
If the device is not programmed with the sniffer firmware, connect a CC-Debugger to it and use Flash Programmer to program the sniffer firmware.
- The firmware image for CC2531 is called
sniffer_fw_cc2531.hex, and is found underbin/general/firmwarein the SmartRF Protocol Packet Sniffer installation. - Refer to the CC-Debugger User’s Guide for how to flash the firmware.
- The firmware image for CC2531 is called
Running the Packet Sniffer¶
Connect the CC2531 USB Dongle.
Start Ubiqua Protocol Analyzer.
Select
Device→Add Device, and choose the CC2531.Set the Default Protocol to Thread. Select
Tools→Optionsthen selectGeneral→Default Protocol Stackand set it to Thread.In options, select
Security Tab→KeyChain. ClickAdd, then select typeThread Master Key. By default, the Thread Master Key for OpenThread is00112233445566778899aabbccddeeff. Click OK.Choose the Channel.
CLI device: to choose the channel via the channelcommand.NCP device: is told via wpantund what channel to use via various configuration steps. See Linux Border Router Quick Start for more details.
Figure 27. TI-OpenThread channel configuration
In Ubiqua, select
Device→Channel, and select the matching channel.Start a sniffer capture.
If required, select
View→Traffic View(or other selections) to view activity.