rflib
Data Fields
rfc_CMD_TRIGGER_s Struct Reference

Generate Command Trigger. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0404. More...
 
uint8_t triggerNo
 Command trigger number. More...
 

Detailed Description

Generate Command Trigger.

Field Documentation

§ commandNo

uint16_t rfc_CMD_TRIGGER_s::commandNo

The command ID number 0x0404.

§ triggerNo

uint8_t rfc_CMD_TRIGGER_s::triggerNo

Command trigger number.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale