rflib
Data Fields
rfc_CMD_SYNC_START_RAT_s Struct Reference

Synchrously Start Radio Timer Command. More...

#include <rf_common_cmd.h>

Collaboration diagram for rfc_CMD_SYNC_START_RAT_s:
Collaboration graph
[legend]

Data Fields

uint16_t commandNo
 The command ID number 0x080A. More...
 
uint16_t status
 An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time. More...
 
rfc_radioOp_tpNextOp
 Pointer to the next operation to run after this operation is done. More...
 
ratmr_t startTime
 Absolute or relative start time (depending on the value of startTrigger) More...
 
struct {
   uint8_t   triggerType:4
 The type of trigger. More...
 
   uint8_t   bEnaCmd:1
 0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger More...
 
   uint8_t   triggerNo:2
 The trigger number of the CMD_TRIGGER command that triggers this action. More...
 
   uint8_t   pastTrig:1
 0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible More...
 
startTrigger
 Identification of the trigger that starts the operation. More...
 
struct {
   uint8_t   rule:4
 Condition for running next command: Rule for how to proceed. More...
 
   uint8_t   nSkip:4
 Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ... More...
 
condition
 
uint16_t __dummy0
 
ratmr_t rat0
 The desired RAT timer value corresponding to the value the RAT would have had when the RTC was zero. This parameter is returned by CMD_SYNC_STOP_RAT. More...
 

Detailed Description

Synchrously Start Radio Timer Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_SYNC_START_RAT_s::commandNo

The command ID number 0x080A.

§ status

uint16_t rfc_CMD_SYNC_START_RAT_s::status

An integer telling the status of the command. This value is updated by the radio CPU during operation and may be read by the system CPU at any time.

§ pNextOp

rfc_radioOp_t* rfc_CMD_SYNC_START_RAT_s::pNextOp

Pointer to the next operation to run after this operation is done.

§ startTime

ratmr_t rfc_CMD_SYNC_START_RAT_s::startTime

Absolute or relative start time (depending on the value of startTrigger)

§ triggerType

uint8_t rfc_CMD_SYNC_START_RAT_s::triggerType

The type of trigger.

§ bEnaCmd

uint8_t rfc_CMD_SYNC_START_RAT_s::bEnaCmd

0: No alternative trigger command
1: CMD_TRIGGER can be used as an alternative trigger

§ triggerNo

uint8_t rfc_CMD_SYNC_START_RAT_s::triggerNo

The trigger number of the CMD_TRIGGER command that triggers this action.

§ pastTrig

uint8_t rfc_CMD_SYNC_START_RAT_s::pastTrig

0: A trigger in the past is never triggered, or for start of commands, give an error
1: A trigger in the past is triggered as soon as possible

§ startTrigger

struct { ... } rfc_CMD_SYNC_START_RAT_s::startTrigger

Identification of the trigger that starts the operation.

§ rule

uint8_t rfc_CMD_SYNC_START_RAT_s::rule

Condition for running next command: Rule for how to proceed.

§ nSkip

uint8_t rfc_CMD_SYNC_START_RAT_s::nSkip

Number of skips + 1 if the rule involves skipping. 0: same, 1: next, 2: skip next, ...

§ condition

struct { ... } rfc_CMD_SYNC_START_RAT_s::condition

§ __dummy0

uint16_t rfc_CMD_SYNC_START_RAT_s::__dummy0

§ rat0

ratmr_t rfc_CMD_SYNC_START_RAT_s::rat0

The desired RAT timer value corresponding to the value the RAT would have had when the RTC was zero. This parameter is returned by CMD_SYNC_STOP_RAT.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale