rflib
Data Fields
rfc_CMD_SET_TX_POWER_s Struct Reference

Set Transmit Power. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0010. More...
 
uint16_t txPower
 New TX power setting. More...
 

Detailed Description

Set Transmit Power.

Field Documentation

§ commandNo

uint16_t rfc_CMD_SET_TX_POWER_s::commandNo

The command ID number 0x0010.

§ txPower

uint16_t rfc_CMD_SET_TX_POWER_s::txPower

New TX power setting.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale