rflib
Data Fields
rfc_CMD_SET_RAT_OUTPUT_s Struct Reference

Set Radio Timer Output to a Specified Mode. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0604. More...
 
struct {
   uint16_t   __pad0__:2
 
   uint16_t   outputSel:3
 Output event indicator. More...
 
   uint16_t   outputMode:3
 0: Set output line low as default; and pulse on event. Duration of pulse is one RF Core clock period (ca. 41.67 ns).
1: Set output line high on event
2: Set output line low on event
3: Toggle (invert) output line state on event
4: Immediately set output line to low (does not change upon event)
5: Immediately set output line to high (does not change upon event)
Others: Reserved More...
 
   uint16_t   ratCh:4
 The radio timer channel number. More...
 
config
 

Detailed Description

Set Radio Timer Output to a Specified Mode.

Field Documentation

§ commandNo

uint16_t rfc_CMD_SET_RAT_OUTPUT_s::commandNo

The command ID number 0x0604.

§ __pad0__

uint16_t rfc_CMD_SET_RAT_OUTPUT_s::__pad0__

§ outputSel

uint16_t rfc_CMD_SET_RAT_OUTPUT_s::outputSel

Output event indicator.

§ outputMode

uint16_t rfc_CMD_SET_RAT_OUTPUT_s::outputMode

0: Set output line low as default; and pulse on event. Duration of pulse is one RF Core clock period (ca. 41.67 ns).
1: Set output line high on event
2: Set output line low on event
3: Toggle (invert) output line state on event
4: Immediately set output line to low (does not change upon event)
5: Immediately set output line to high (does not change upon event)
Others: Reserved

§ ratCh

uint16_t rfc_CMD_SET_RAT_OUTPUT_s::ratCh

The radio timer channel number.

§ config

struct { ... } rfc_CMD_SET_RAT_OUTPUT_s::config

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale