rflib
Data Fields
rfc_CMD_MODIFY_FS_s Struct Reference

Set New Synthesizer Frequency without Recalibration. More...

#include <rf_common_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x0013. More...
 
uint16_t frequency
 The frequency in MHz to tune to. More...
 
uint16_t fractFreq
 Fractional part of the frequency to tune to. More...
 

Detailed Description

Set New Synthesizer Frequency without Recalibration.

Field Documentation

§ commandNo

uint16_t rfc_CMD_MODIFY_FS_s::commandNo

The command ID number 0x0013.

§ frequency

uint16_t rfc_CMD_MODIFY_FS_s::frequency

The frequency in MHz to tune to.

§ fractFreq

uint16_t rfc_CMD_MODIFY_FS_s::fractFreq

Fractional part of the frequency to tune to.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale