rflib
Data Fields
rfc_CMD_IEEE_MOD_FILT_s Struct Reference

IEEE 802.15.4 Modify Frame Filtering Parameter Command. More...

#include <rf_ieee_cmd.h>

Data Fields

uint16_t commandNo
 The command ID number 0x2002. More...
 
struct {
   uint16_t   frameFiltEn:1
 0: Disable frame filtering
1: Enable frame filtering More...
 
   uint16_t   frameFiltStop:1
 0: Receive all packets to the end
1: Stop receiving frame once frame filtering has caused the frame to be rejected. More...
 
   uint16_t   autoAckEn:1
 0: Disable auto ACK
1: Enable auto ACK. More...
 
   uint16_t   slottedAckEn:1
 0: Non-slotted ACK
1: Slotted ACK. More...
 
   uint16_t   autoPendEn:1
 0: Auto-pend disabled
1: Auto-pend enabled More...
 
   uint16_t   defaultPend:1
 The value of the pending data bit in auto ACK packets that are not subject to auto-pend. More...
 
   uint16_t   bPendDataReqOnly:1
 0: Use auto-pend for any packet
1: Use auto-pend for data request packets only More...
 
   uint16_t   bPanCoord:1
 0: Device is not PAN coordinator
1: Device is PAN coordinator More...
 
   uint16_t   maxFrameVersion:2
 Reject frames where the frame version field in the FCF is greater than this value. More...
 
   uint16_t   fcfReservedMask:3
 Value to be AND-ed with the reserved part of the FCF; frame rejected if result is non-zero. More...
 
   uint16_t   modifyFtFilter:2
 Treatment of MSB of frame type field before frame-type filtering:
0: No modification
1: Invert MSB
2: Set MSB to 0
3: Set MSB to 1. More...
 
   uint16_t   bStrictLenFilter:1
 0: Accept acknowledgement frames of any length >= 5
1: Accept only acknowledgement frames of length 5 More...
 
newFrameFiltOpt
 New value of frameFiltOpt for the running background level operation. More...
 
struct {
   uint8_t   bAcceptFt0Beacon:1
 Treatment of frames with frame type 000 (beacon):
0: Reject
1: Accept. More...
 
   uint8_t   bAcceptFt1Data:1
 Treatment of frames with frame type 001 (data):
0: Reject
1: Accept. More...
 
   uint8_t   bAcceptFt2Ack:1
 Treatment of frames with frame type 010 (ACK):
0: Reject, unless running ACK receive command
1: Always accept. More...
 
   uint8_t   bAcceptFt3MacCmd:1
 Treatment of frames with frame type 011 (MAC command):
0: Reject
1: Accept. More...
 
   uint8_t   bAcceptFt4Reserved:1
 Treatment of frames with frame type 100 (reserved):
0: Reject
1: Accept. More...
 
   uint8_t   bAcceptFt5Reserved:1
 Treatment of frames with frame type 101 (reserved):
0: Reject
1: Accept. More...
 
   uint8_t   bAcceptFt6Reserved:1
 Treatment of frames with frame type 110 (reserved):
0: Reject
1: Accept. More...
 
   uint8_t   bAcceptFt7Reserved:1
 Treatment of frames with frame type 111 (reserved):
0: Reject
1: Accept. More...
 
newFrameTypes
 New value of frameTypes for the running background level operation. More...
 

Detailed Description

IEEE 802.15.4 Modify Frame Filtering Parameter Command.

Field Documentation

§ commandNo

uint16_t rfc_CMD_IEEE_MOD_FILT_s::commandNo

The command ID number 0x2002.

§ frameFiltEn

uint16_t rfc_CMD_IEEE_MOD_FILT_s::frameFiltEn

0: Disable frame filtering
1: Enable frame filtering

§ frameFiltStop

uint16_t rfc_CMD_IEEE_MOD_FILT_s::frameFiltStop

0: Receive all packets to the end
1: Stop receiving frame once frame filtering has caused the frame to be rejected.

§ autoAckEn

uint16_t rfc_CMD_IEEE_MOD_FILT_s::autoAckEn

0: Disable auto ACK
1: Enable auto ACK.

§ slottedAckEn

uint16_t rfc_CMD_IEEE_MOD_FILT_s::slottedAckEn

0: Non-slotted ACK
1: Slotted ACK.

§ autoPendEn

uint16_t rfc_CMD_IEEE_MOD_FILT_s::autoPendEn

0: Auto-pend disabled
1: Auto-pend enabled

§ defaultPend

uint16_t rfc_CMD_IEEE_MOD_FILT_s::defaultPend

The value of the pending data bit in auto ACK packets that are not subject to auto-pend.

§ bPendDataReqOnly

uint16_t rfc_CMD_IEEE_MOD_FILT_s::bPendDataReqOnly

0: Use auto-pend for any packet
1: Use auto-pend for data request packets only

§ bPanCoord

uint16_t rfc_CMD_IEEE_MOD_FILT_s::bPanCoord

0: Device is not PAN coordinator
1: Device is PAN coordinator

§ maxFrameVersion

uint16_t rfc_CMD_IEEE_MOD_FILT_s::maxFrameVersion

Reject frames where the frame version field in the FCF is greater than this value.

§ fcfReservedMask

uint16_t rfc_CMD_IEEE_MOD_FILT_s::fcfReservedMask

Value to be AND-ed with the reserved part of the FCF; frame rejected if result is non-zero.

§ modifyFtFilter

uint16_t rfc_CMD_IEEE_MOD_FILT_s::modifyFtFilter

Treatment of MSB of frame type field before frame-type filtering:
0: No modification
1: Invert MSB
2: Set MSB to 0
3: Set MSB to 1.

§ bStrictLenFilter

uint16_t rfc_CMD_IEEE_MOD_FILT_s::bStrictLenFilter

0: Accept acknowledgement frames of any length >= 5
1: Accept only acknowledgement frames of length 5

§ newFrameFiltOpt

struct { ... } rfc_CMD_IEEE_MOD_FILT_s::newFrameFiltOpt

New value of frameFiltOpt for the running background level operation.

§ bAcceptFt0Beacon

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt0Beacon

Treatment of frames with frame type 000 (beacon):
0: Reject
1: Accept.

§ bAcceptFt1Data

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt1Data

Treatment of frames with frame type 001 (data):
0: Reject
1: Accept.

§ bAcceptFt2Ack

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt2Ack

Treatment of frames with frame type 010 (ACK):
0: Reject, unless running ACK receive command
1: Always accept.

§ bAcceptFt3MacCmd

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt3MacCmd

Treatment of frames with frame type 011 (MAC command):
0: Reject
1: Accept.

§ bAcceptFt4Reserved

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt4Reserved

Treatment of frames with frame type 100 (reserved):
0: Reject
1: Accept.

§ bAcceptFt5Reserved

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt5Reserved

Treatment of frames with frame type 101 (reserved):
0: Reject
1: Accept.

§ bAcceptFt6Reserved

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt6Reserved

Treatment of frames with frame type 110 (reserved):
0: Reject
1: Accept.

§ bAcceptFt7Reserved

uint8_t rfc_CMD_IEEE_MOD_FILT_s::bAcceptFt7Reserved

Treatment of frames with frame type 111 (reserved):
0: Reject
1: Accept.

§ newFrameTypes

struct { ... } rfc_CMD_IEEE_MOD_FILT_s::newFrameTypes

New value of frameTypes for the running background level operation.


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale