rflib
Data Structures | Macros | Functions
Rfc_api

Data Structures

struct  rfTrim_t
 

Macros

#define RFC_MAX_SEARCH_DEPTH   5
 
#define RFC_PA_TYPE_ADDRESS   0x21000385
 
#define RFC_PA_TYPE_MASK   0x04
 
#define RFC_PA_GAIN_ADDRESS   0x21000398
 
#define RFC_PA_GAIN_MASK   0x003FFFFF
 
#define RFC_FE_MODE_ESCAPE_VALUE   0xFF
 
#define RFC_FE_OVERRIDE_ADDRESS   0x0703
 
#define RFC_FE_OVERRIDE_MASK   0x0000FFFF
 
#define RFCCpeIntGetAndClear   NOROM_RFCCpeIntGetAndClear
 
#define RFCDoorbellSendTo   NOROM_RFCDoorbellSendTo
 
#define RFCSynthPowerDown   NOROM_RFCSynthPowerDown
 
#define RFCCpePatchReset   NOROM_RFCCpePatchReset
 
#define RFCOverrideSearch   NOROM_RFCOverrideSearch
 
#define RFCOverrideUpdate   NOROM_RFCOverrideUpdate
 
#define RFCHwIntGetAndClear   NOROM_RFCHwIntGetAndClear
 
#define RFCAnaDivTxOverride   NOROM_RFCAnaDivTxOverride
 

Functions

__STATIC_INLINE void RFCClockEnable (void)
 Enable the RF core clocks. More...
 
__STATIC_INLINE void RFCClockDisable (void)
 Disable the RF core clocks. More...
 
__STATIC_INLINE void RFCCpeIntClear (uint32_t ui32Mask)
 Clear HW interrupt flags. More...
 
__STATIC_INLINE void RFCHwIntClear (uint32_t ui32Mask)
 Clear CPE interrupt flags. More...
 
__STATIC_INLINE void RFCCpe0IntSelect (uint32_t ui32Mask)
 Select interrupt sources to CPE0 (assign to INT_RFC_CPE_0 interrupt vector). More...
 
__STATIC_INLINE void RFCCpe1IntSelect (uint32_t ui32Mask)
 Select interrupt sources to CPE1 (assign to INT_RFC_CPE_1 interrupt vector). More...
 
__STATIC_INLINE void RFCCpeIntEnable (uint32_t ui32Mask)
 Enable CPEx interrupt sources. More...
 
__STATIC_INLINE void RFCCpe0IntSelectClearEnable (uint32_t ui32Mask)
 Select, clear, and enable interrupt sources to CPE0. More...
 
__STATIC_INLINE void RFCCpe1IntSelectClearEnable (uint32_t ui32Mask)
 Select, clear, and enable interrupt sources to CPE1. More...
 
__STATIC_INLINE void RFCHwIntEnable (uint32_t ui32Mask)
 Enable HW interrupt sources. More...
 
__STATIC_INLINE void RFCCpeIntDisable (uint32_t ui32Mask)
 Disable CPE interrupt sources. More...
 
__STATIC_INLINE void RFCHwIntDisable (uint32_t ui32Mask)
 Disable HW interrupt sources. More...
 
uint32_t NOROM_RFCCpeIntGetAndClear (uint32_t ui32Mask)
 Get and clear CPE interrupt flags. More...
 
__STATIC_INLINE void RFCAckIntClear (void)
 Clear ACK interrupt flag. More...
 
uint32_t NOROM_RFCDoorbellSendTo (uint32_t pOp)
 Send a radio operation to the doorbell and wait for an acknowledgment. More...
 
void NOROM_RFCSynthPowerDown (void)
 This function implements a fast way to turn off the synthesizer. More...
 
void NOROM_RFCCpePatchReset (void)
 Reset previously patched CPE RAM to a state where it can be patched again. More...
 
uint8_t NOROM_RFCOverrideSearch (const uint32_t *pOverride, const uint32_t pattern, const uint32_t mask, const uint8_t searchDepth)
 
uint8_t NOROM_RFCOverrideUpdate (rfc_radioOp_t *pOpSetup, uint32_t *pParams)
 Function to update override list. More...
 
uint32_t NOROM_RFCHwIntGetAndClear (uint32_t ui32Mask)
 Get and clear HW interrupt flags. More...
 
__STATIC_INLINE bool RFCGetPaType (void)
 Get the type of currently selected PA. More...
 
__STATIC_INLINE uint32_t RFCGetPaGain (void)
 Get the gain of currently selected PA. More...
 
uint32_t NOROM_RFCAnaDivTxOverride (uint8_t loDivider, uint8_t frontEndMode)
 Function to calculate the proper override run-time for the High Gain PA. More...
 

Detailed Description

Macro Definition Documentation

§ RFC_MAX_SEARCH_DEPTH

#define RFC_MAX_SEARCH_DEPTH   5

§ RFC_PA_TYPE_ADDRESS

#define RFC_PA_TYPE_ADDRESS   0x21000385

Referenced by RFCGetPaType().

§ RFC_PA_TYPE_MASK

#define RFC_PA_TYPE_MASK   0x04

Referenced by RFCGetPaType().

§ RFC_PA_GAIN_ADDRESS

#define RFC_PA_GAIN_ADDRESS   0x21000398

Referenced by RFCGetPaGain().

§ RFC_PA_GAIN_MASK

#define RFC_PA_GAIN_MASK   0x003FFFFF

Referenced by RFCGetPaGain().

§ RFC_FE_MODE_ESCAPE_VALUE

#define RFC_FE_MODE_ESCAPE_VALUE   0xFF

§ RFC_FE_OVERRIDE_ADDRESS

#define RFC_FE_OVERRIDE_ADDRESS   0x0703

§ RFC_FE_OVERRIDE_MASK

#define RFC_FE_OVERRIDE_MASK   0x0000FFFF

§ RFCCpeIntGetAndClear

#define RFCCpeIntGetAndClear   NOROM_RFCCpeIntGetAndClear

Referenced by RFCHwIntDisable().

§ RFCDoorbellSendTo

#define RFCDoorbellSendTo   NOROM_RFCDoorbellSendTo

Referenced by RFCAckIntClear().

§ RFCSynthPowerDown

#define RFCSynthPowerDown   NOROM_RFCSynthPowerDown

Referenced by RFCAckIntClear().

§ RFCCpePatchReset

#define RFCCpePatchReset   NOROM_RFCCpePatchReset

Referenced by RFCAckIntClear().

§ RFCOverrideSearch

#define RFCOverrideSearch   NOROM_RFCOverrideSearch

Referenced by RFCAckIntClear().

§ RFCOverrideUpdate

#define RFCOverrideUpdate   NOROM_RFCOverrideUpdate

Referenced by RFCAckIntClear().

§ RFCHwIntGetAndClear

#define RFCHwIntGetAndClear   NOROM_RFCHwIntGetAndClear

Referenced by RFCAckIntClear().

§ RFCAnaDivTxOverride

#define RFCAnaDivTxOverride   NOROM_RFCAnaDivTxOverride

Referenced by RFCGetPaGain().

Function Documentation

§ RFCClockEnable()

__STATIC_INLINE void RFCClockEnable ( void  )

Enable the RF core clocks.

As soon as the RF core is started it will handle clock control autonomously. No check should be performed to check the clocks. Instead the radio can be ping'ed through the command interface.

Returns
None

§ RFCClockDisable()

__STATIC_INLINE void RFCClockDisable ( void  )

Disable the RF core clocks.

As soon as the RF core is started it will handle clock control autonomously. No check should be performed to check the clocks. Instead the radio can be ping'ed through the command interface.

When disabling clocks it is the programmers responsibility that the RF core clocks are safely gated. I.e. the RF core should be safely 'parked'.

Returns
None

§ RFCCpeIntClear()

__STATIC_INLINE void RFCCpeIntClear ( uint32_t  ui32Mask)

Clear HW interrupt flags.

Referenced by RFCCpe0IntSelectClearEnable(), and RFCCpe1IntSelectClearEnable().

§ RFCHwIntClear()

__STATIC_INLINE void RFCHwIntClear ( uint32_t  ui32Mask)

Clear CPE interrupt flags.

§ RFCCpe0IntSelect()

__STATIC_INLINE void RFCCpe0IntSelect ( uint32_t  ui32Mask)

Select interrupt sources to CPE0 (assign to INT_RFC_CPE_0 interrupt vector).

Referenced by RFCCpe0IntSelectClearEnable().

§ RFCCpe1IntSelect()

__STATIC_INLINE void RFCCpe1IntSelect ( uint32_t  ui32Mask)

Select interrupt sources to CPE1 (assign to INT_RFC_CPE_1 interrupt vector).

Referenced by RFCCpe1IntSelectClearEnable().

§ RFCCpeIntEnable()

__STATIC_INLINE void RFCCpeIntEnable ( uint32_t  ui32Mask)

Enable CPEx interrupt sources.

Referenced by RFCCpe0IntSelectClearEnable(), and RFCCpe1IntSelectClearEnable().

§ RFCCpe0IntSelectClearEnable()

__STATIC_INLINE void RFCCpe0IntSelectClearEnable ( uint32_t  ui32Mask)

Select, clear, and enable interrupt sources to CPE0.

References RFCCpe0IntSelect(), RFCCpeIntClear(), and RFCCpeIntEnable().

§ RFCCpe1IntSelectClearEnable()

__STATIC_INLINE void RFCCpe1IntSelectClearEnable ( uint32_t  ui32Mask)

Select, clear, and enable interrupt sources to CPE1.

References RFCCpe1IntSelect(), RFCCpeIntClear(), and RFCCpeIntEnable().

§ RFCHwIntEnable()

__STATIC_INLINE void RFCHwIntEnable ( uint32_t  ui32Mask)

Enable HW interrupt sources.

§ RFCCpeIntDisable()

__STATIC_INLINE void RFCCpeIntDisable ( uint32_t  ui32Mask)

Disable CPE interrupt sources.

§ RFCHwIntDisable()

__STATIC_INLINE void RFCHwIntDisable ( uint32_t  ui32Mask)

Disable HW interrupt sources.

References RFCCpeIntGetAndClear.

§ NOROM_RFCCpeIntGetAndClear()

uint32_t NOROM_RFCCpeIntGetAndClear ( uint32_t  ui32Mask)

Get and clear CPE interrupt flags.

§ RFCAckIntClear()

__STATIC_INLINE void RFCAckIntClear ( void  )

§ NOROM_RFCDoorbellSendTo()

uint32_t NOROM_RFCDoorbellSendTo ( uint32_t  pOp)

Send a radio operation to the doorbell and wait for an acknowledgment.

§ NOROM_RFCSynthPowerDown()

void NOROM_RFCSynthPowerDown ( void  )

This function implements a fast way to turn off the synthesizer.

§ NOROM_RFCCpePatchReset()

void NOROM_RFCCpePatchReset ( void  )

Reset previously patched CPE RAM to a state where it can be patched again.

§ NOROM_RFCOverrideSearch()

uint8_t NOROM_RFCOverrideSearch ( const uint32_t *  pOverride,
const uint32_t  pattern,
const uint32_t  mask,
const uint8_t  searchDepth 
)

§ NOROM_RFCOverrideUpdate()

uint8_t NOROM_RFCOverrideUpdate ( rfc_radioOp_t pOpSetup,
uint32_t *  pParams 
)

Function to update override list.

§ NOROM_RFCHwIntGetAndClear()

uint32_t NOROM_RFCHwIntGetAndClear ( uint32_t  ui32Mask)

Get and clear HW interrupt flags.

§ RFCGetPaType()

__STATIC_INLINE bool RFCGetPaType ( void  )

Get the type of currently selected PA.

References RFC_PA_TYPE_ADDRESS, and RFC_PA_TYPE_MASK.

§ RFCGetPaGain()

__STATIC_INLINE uint32_t RFCGetPaGain ( void  )

Get the gain of currently selected PA.

References RFC_PA_GAIN_ADDRESS, RFC_PA_GAIN_MASK, and RFCAnaDivTxOverride.

§ NOROM_RFCAnaDivTxOverride()

uint32_t NOROM_RFCAnaDivTxOverride ( uint8_t  loDivider,
uint8_t  frontEndMode 
)

Function to calculate the proper override run-time for the High Gain PA.

© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale