Data structure for experimental HPOSC polynomials calculation. More...
#include <osc.h>
Data Fields | |
uint32_t | meas_1 |
Measurement set 1 (typically at room temp) More... | |
uint32_t | meas_2 |
Measurement set 2 (typically at high temp) More... | |
uint32_t | meas_3 |
Measurement set 3 (typically at low temp) More... | |
int32_t | offsetD1 |
Offset to measurement set 1. More... | |
int32_t | offsetD2 |
Offset to measurement set 2. More... | |
int32_t | offsetD3 |
Offset to measurement set 3. More... | |
int32_t | polyP3 |
The P3 polynomial. More... | |
Data structure for experimental HPOSC polynomials calculation.
The structure of the meas_1, meas_2 and meas_3 parameter is as defined in FCFG1_O_HPOSC_MEAS_1, 2 and 3.
uint32_t HposcDebugData_t::meas_1 |
Measurement set 1 (typically at room temp)
Referenced by OSC_HPOSC_Debug_InitFreqOffsetParams().
uint32_t HposcDebugData_t::meas_2 |
Measurement set 2 (typically at high temp)
Referenced by OSC_HPOSC_Debug_InitFreqOffsetParams().
uint32_t HposcDebugData_t::meas_3 |
Measurement set 3 (typically at low temp)
Referenced by OSC_HPOSC_Debug_InitFreqOffsetParams().
int32_t HposcDebugData_t::offsetD1 |
Offset to measurement set 1.
Referenced by OSC_HPOSC_Debug_InitFreqOffsetParams().
int32_t HposcDebugData_t::offsetD2 |
Offset to measurement set 2.
Referenced by OSC_HPOSC_Debug_InitFreqOffsetParams().
int32_t HposcDebugData_t::offsetD3 |
Offset to measurement set 3.
Referenced by OSC_HPOSC_Debug_InitFreqOffsetParams().
int32_t HposcDebugData_t::polyP3 |
The P3 polynomial.
Referenced by OSC_HPOSC_Debug_InitFreqOffsetParams().