|
void | AUXADCDisable (void) |
| Disables the ADC. More...
|
|
void | AUXADCEnableAsync (uint32_t refSource, uint32_t trigger) |
| Enables the ADC for asynchronous operation. More...
|
|
void | AUXADCEnableSync (uint32_t refSource, uint32_t sampleTime, uint32_t trigger) |
| Enables the ADC for synchronous operation. More...
|
|
void | AUXADCDisableInputScaling (void) |
| Disables scaling of the ADC input. More...
|
|
void | AUXADCFlushFifo (void) |
| Flushes the ADC FIFO. More...
|
|
uint32_t | AUXADCReadFifo (void) |
| Waits for and returns the first sample in the ADC FIFO. More...
|
|
uint32_t | AUXADCPopFifo (void) |
| Returns the first sample in the ADC FIFO, without waiting. More...
|
|
int32_t | AUXADCGetAdjustmentGain (uint32_t refSource) |
| Returns the gain value used when adjusting for ADC gain/offset. More...
|
|
int32_t | AUXADCGetAdjustmentOffset (uint32_t refSource) |
| Returns the offset value used when adjusting for ADC gain/offset. More...
|
|
int32_t | AUXADCValueToMicrovolts (int32_t fixedRefVoltage, int32_t adcValue) |
| Converts an "adjusted" ADC value to microvolts. More...
|
|
int32_t | AUXADCMicrovoltsToValue (int32_t fixedRefVoltage, int32_t microvolts) |
| Converts a number of microvolts to corresponding "adjusted" ADC value. More...
|
|
int32_t | AUXADCAdjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset) |
| Performs ADC value gain and offset adjustment. More...
|
|
int32_t | AUXADCUnadjustValueForGainAndOffset (int32_t adcValue, int32_t gain, int32_t offset) |
| Performs the inverse of the ADC value gain and offset adjustment. More...
|
|