![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.01.00
|
This file contains the interface to the SM.
Go to the source code of this file.
Data Structures | |
struct | authReq_t |
struct | keyDist_t |
struct | smDhKeyEvt_t |
struct | smEccKeys_t |
struct | smEccKeysEvt_t |
struct | smEventHdr_t |
struct | smIdentityInfo_t |
struct | smLinkSecurityReq_t |
struct | smNewRandKeyEvent_t |
struct | smSecurityInfo_t |
struct | smSigningInfo_t |
Macros | |
#define | DISPLAY_ONLY 0x00 |
Display Only Device. | |
#define | DISPLAY_YES_NO 0x01 |
Display and Yes and No Capable. | |
#define | KEYBOARD_DISPLAY 0x04 |
Both Keyboard and Display Capable. | |
#define | KEYBOARD_ONLY 0x02 |
Keyboard Only. | |
#define | NO_INPUT_NO_OUTPUT 0x03 |
No Display or Input Device. | |
#define | PASSKEY_LEN 6 |
Passkey Character Length (ASCII Characters) | |
#define | SM_AUTH_MITM_MASK(a) (((a) & 0x04) >> 2) |
MITM Mask. | |
#define | SM_AUTH_REQ_BONDING 0x01 |
Bonding. | |
#define | SM_AUTH_REQ_NO_BONDING 0x00 |
No bonding. | |
#define | SM_AUTH_STATE_AUTHENTICATED 0x04 |
Authenticate requested. | |
#define | SM_AUTH_STATE_BONDING 0x01 |
Bonding requested. | |
#define | SM_AUTH_STATE_SECURECONNECTION 0x08 |
Secure Connection requested. | |
#define | SM_DH_KEY_EVENT 0x01 |
Diffie-Hellman key. | |
#define | SM_ECC_KEY_LEN 32 |
ECC Key length in bytes. | |
#define | SM_ECC_KEYS_EVENT 0x00 |
ECC Keys. | |
#define | SM_ECC_KEYS_NOT_AVAILABLE 0xFF |
Initial state of recycled keys before they exist. | |
#define | SM_ECC_KEYS_REGENERATE_ALWAYS 0x00 |
Always regenerate the keys. | |
#define | SM_ECC_KEYS_REGNENERATE_NEVER 0xFF |
Never regenerate the keys. | |
#define | SM_PASSKEY_TYPE_DISPLAY 0x02 |
Display the passkey. | |
#define | SM_PASSKEY_TYPE_INPUT 0x01 |
Input the passkey. | |
Typedefs | |
typedef void(* | smCB_t) (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY) |
Functions | |
bStatus_t | SM_Encrypt (uint8 *pKey, uint8 *pPlainText, uint8 *pResult) |
Encrypt the plain text data with the key.. More... | |
bStatus_t | SM_GenerateAuthenSig (uint8 *pData, uint16 len, uint8 *pAuthenSig, uint16 connHandle) |
void | SM_GenerateRandBuf (uint8 *random, uint8 len) |
bStatus_t | SM_GetDHKey (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY) |
Request a Diffie-Hellman key from the ECC engine. Key is returned through the callback registered in SM_RegisterCb, in the first parameter. More... | |
bStatus_t | SM_GetEccKeys (void) |
Get ECC private and public keys. Keys are returned through the callback registered in SM_RegisterCb. More... | |
bStatus_t | SM_GetScConfirmOob (uint8 *publicKey, uint8 *oob, uint8 *pOut) |
Generate a confirm value for OOB data. More... | |
bStatus_t | SM_InitiatorInit (void) |
Initialize SM Initiator on a master device. More... | |
bStatus_t | SM_NewRandKey (uint8 taskID) |
Generate a key with a random value. More... | |
bStatus_t | SM_PasskeyUpdate (uint8 *pPasskey, uint16 connectionHandle) |
Update the passkey for the pairing process. More... | |
void | SM_RegisterTask (uint8 taskID) |
Register Task with the Security Manager to receive ECC keys or a ECDH shared secret. More... | |
bStatus_t | SM_ResponderInit (void) |
Initialize SM Responder on a slave device. More... | |
void | SM_SetECCRegenerationCount (uint8 count) |
Update the regeneration count for ECC key re-usage. More... | |
bStatus_t | SM_StartEncryption (uint16 connHandle, uint8 *pLTK, uint16 div, uint8 *pRandNum, uint8 keyLen) |
Send Start Encrypt through HCI. More... | |
bStatus_t | SM_StartPairing (uint8 initiator, uint8 taskID, uint16 connectionHandle, smLinkSecurityReq_t *pSecReqs) |
Start the pairing process. More... | |
bStatus_t | SM_VerifyAuthenSig (uint16 connHandle, uint8 authentication, uint8 *pData, uint16 len, uint8 *pAuthenSig) |
Verify an Authentication Signature. More... | |
typedef void(* smCB_t) (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY) |
Application callback to the SM for ECC keys and Diffie-Hellman Shared Secret (ECDH).
bStatus_t SM_Encrypt | ( | uint8 * | pKey, |
uint8 * | pPlainText, | ||
uint8 * | pResult | ||
) |
Encrypt the plain text data with the key..
pKey | - key data |
pPlainText | - Plain text data |
pResult | - place to put the encrypted result |
bStatus_t SM_GenerateAuthenSig | ( | uint8 * | pData, |
uint16 | len, | ||
uint8 * | pAuthenSig, | ||
uint16 | connHandle | ||
) |
Generate an outgoing Authentication Signature.
pData | message data |
len | length of pData |
pAuthenSig | place to put new signature |
connHandle | connection handle |
bStatus_t SM_GetDHKey | ( | uint8 * | secretKey, |
uint8 * | publicKeyX, | ||
uint8 * | publicKeyY | ||
) |
Request a Diffie-Hellman key from the ECC engine. Key is returned through the callback registered in SM_RegisterCb, in the first parameter.
secretKey | - the local private key |
publicKeyX | - the remote public key, X-Coordinate. |
publicKeyY | - the remote public key, Y-Coordinate. |
bStatus_t SM_GetEccKeys | ( | void | ) |
Get ECC private and public keys. Keys are returned through the callback registered in SM_RegisterCb.
bStatus_t SM_GetScConfirmOob | ( | uint8 * | publicKey, |
uint8 * | oob, | ||
uint8 * | pOut | ||
) |
Generate a confirm value for OOB data.
publicKey | - the local public key X-coordinate |
oob | - the random string to be sent to the remote device via oob |
pOut | - pointer to the generated confirm value. The calling application must copy this data into its own buffer. |
bStatus_t SM_InitiatorInit | ( | void | ) |
Initialize SM Initiator on a master device.
bStatus_t SM_NewRandKey | ( | uint8 | taskID | ) |
Generate a key with a random value.
taskID | - task ID to send results. |
bStatus_t SM_PasskeyUpdate | ( | uint8 * | pPasskey, |
uint16 | connectionHandle | ||
) |
Update the passkey for the pairing process.
pPasskey | - pointer to the 6 digit passkey |
connectionHandle | - connection handle to link. |
void SM_RegisterTask | ( | uint8 | taskID | ) |
Register Task with the Security Manager to receive ECC keys or a ECDH shared secret.
taskID | - Application's task ID. |
bStatus_t SM_ResponderInit | ( | void | ) |
Initialize SM Responder on a slave device.
void SM_SetECCRegenerationCount | ( | uint8 | count | ) |
Update the regeneration count for ECC key re-usage.
count | - number of times a keypair can be reused before regeneration. |
bStatus_t SM_StartEncryption | ( | uint16 | connHandle, |
uint8 * | pLTK, | ||
uint16 | div, | ||
uint8 * | pRandNum, | ||
uint8 | keyLen | ||
) |
Send Start Encrypt through HCI.
connHandle | - Connection Handle |
pLTK | - pointer to 16 byte lkt |
div | - div or ediv |
pRandNum | - pointer to 8 byte random number |
keyLen | - length of LTK (bytes) |
bStatus_t SM_StartPairing | ( | uint8 | initiator, |
uint8 | taskID, | ||
uint16 | connectionHandle, | ||
smLinkSecurityReq_t * | pSecReqs | ||
) |
Start the pairing process.
This function is also called if the device is already bound.
initiator | - TRUE to start pairing as Initiator. |
taskID | - task ID to send results. |
connectionHandle | - Link's connection handle |
pSecReqs | - Security parameters for pairing |
bStatus_t SM_VerifyAuthenSig | ( | uint16 | connHandle, |
uint8 | authentication, | ||
uint8 * | pData, | ||
uint16 | len, | ||
uint8 * | pAuthenSig | ||
) |
Verify an Authentication Signature.
connHandle | - connection to verify against. |
authentication | - TRUE if requires an authenticated CSRK, FALSE if not |
pData | - message data |
len | - length of pData |
pAuthenSig | - message signature to verify |