![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.01.00
|
Data Structures | |
struct | ToF_BurstStat |
TOF Burst Stats Structure. More... | |
struct | ToF_Params |
TOF Parameters Structure. More... | |
struct | ToF_Status |
TOF Burst Stats Structure. More... | |
struct | ToF_Sync |
TOF Sync Structure. More... | |
Typedefs | |
typedef void(* | TOF_ApplicationCB) (void) |
Callback to a handler supplied by the application. | |
typedef uint8_t * | ToF_RX_Buf |
Pointer to RX buffer. | |
typedef rfc_CMD_TOF_sample_extended_t | ToF_Sample |
TOF Sample. | |
typedef rfc_CMD_TOF_synthCal_t | ToF_SynthCal |
Pointer to frequency calibration struct, used for the pre-calibration of the synth. | |
typedef uint8_t * | ToF_TX_Buf |
Pointer to TX buffer. | |
Enumerations | |
enum | ToF_Role { ToF_ROLE_SLAVE = 0, ToF_ROLE_MASTER, ToF_ROLE_PASSIVE } |
Enumeration for TOF roles of operation. | |
enum | TofHandshakeState_e { TOF_HANDSHAKE_STARTED = 0, TOF_HANDSHAKE_IN_PROGRESS, TOF_HANDSHAKE_RECOVERING, TOF_HANDSHAKE_COMPLETE, TOF_HANDSHAKE_FAILED } |
TOF Handshake State. | |
enum | TofStatus_e { TOF_SUCCESS = 0, TOF_FAILED } |
TOF Errors. | |
enum | TofSyncState_e { TOF_SYNC_WAIT_FOR_SYNC = 0, TOF_SYNC_SYNCHRONIZED, TOF_SYNC_OUT_OF_SYNC } |
TOF Sync State. | |