![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.01.00
|
Enumerations | |
enum | GapScan_ParamId_t { SCAN_PARAM_RPT_FIELDS, SCAN_PARAM_PRIM_PHYS, SCAN_PARAM_FLT_POLICY, SCAN_PARAM_FLT_PDU_TYPE, SCAN_PARAM_FLT_MIN_RSSI, SCAN_PARAM_FLT_DISC_MODE, SCAN_PARAM_FLT_DUP, SCAN_PARAM_NUM_ADV_RPT = SCAN_NUM_RW_PARAM } |
Params used in the GapAdv module
enum GapScan_ParamId_t |
GAP Scanner Parameters
These can be set with GapScan_setParam and read with GapScan_getParam. The default values below refer to the values that are set at initialization.
Enumerator | |
---|---|
SCAN_PARAM_RPT_FIELDS | Advertising Report Fields (R/W) Bit mask of which fields in the GapScan_Evt_AdvRpt_t need to be stored in the AdvRptList
size: uint16_t default: SCAN_PARAM_DFLT_RPT_FIELDS range: combination of individual values in GapScan_AdvRptField_t |
SCAN_PARAM_PRIM_PHYS | Primary Scanning Channel PHYs (R/W) PHYs on which advertisements should be received on the primary advertising channel.
size: uint8_t default: SCAN_PARAM_DFLT_PHYS range: GapScan_PrimPhy_t |
SCAN_PARAM_FLT_POLICY | Scanning Filter Policy (R/W) Policy of how to apply white list to filter out unwanted packets
size: uint8_t default: SCAN_PARAM_DFLT_FLT_POLICY range: GapScan_FilterPolicy_t |
SCAN_PARAM_FLT_PDU_TYPE | Filter by PDU Type (R/W) This filter value specifies packets of which types in 6 different category sets are wanted. The 6 sets include Connectable/Non-Connectable, Scannable/Non-Scannable, Directed/Undirected, ScanRsp/Adv, Legacy/Extended, and Complete/Incomplete category sets. Each set has two mutually exclusive types. Only one type in a set can be* chosen. For example, SCAN_FLT_PDU_NONSCANNABLE_ONLY and SCAN_FLT_PDU_SCANNABLE_ONLY cannot be chosen together. Only either one can be used. If neither type is selected in a set, the filter will not care about the category. For example, if neither SCAN_FLT_PDU_NONCONNECTABLE_ONLY nor SCAN_FLT_PDU_CONNECTABLE_ONLY is set in the parameter value, the scanner will accept both connectable packets and non-connectable packets.
With the call above, the scanner will receive only connectable, undirected, extended(non-legacy), and complete packets. It will not be examined whether the packets are scannable or non-scannable and whether they are scan responses or advertisements. size: uint16_t default: SCAN_PARAM_DFLT_FLT_PDU range: combination of individual values in GapScan_FilterPduType_t |
SCAN_PARAM_FLT_MIN_RSSI | Filter by Minimum RSSI (R/W) Only packets received with the specified RSSI or above will be accepted.
size: int8_t default: -128 (ignore) range: -128 - 127 (dBm) |
SCAN_PARAM_FLT_DISC_MODE | Filter by Discoverable Mode (R/W)
size: uint8_t default: SCAN_PARAM_DFLT_FLT_DISC range: GapScan_FilterDiscMode_t |
SCAN_PARAM_FLT_DUP | Duplicate Filtering (R/W) Specify whether and when to filter out duplicated packets by DID and address
size: uint8_t default: SCAN_PARAM_DFLT_FLT_DUP range: GapScan_FilterDuplicate_t |
SCAN_PARAM_NUM_ADV_RPT | Number of Reports Recorded (R) Number of advertising reports recorded since the current scanning started.
size: uint8_t range: 0 up to maxNumReport specified when GapScan_enable() is called |