![]() |
![]() |
TI BLE5-Stack API Documentation
2.01.01.00
|
Macros | |
#define | GAP_ADV_REMOVE_SET_EVENT 0x13 |
Sent when an advertising set needs to be removed. This is an internal event. | |
#define | GAP_AUTHENTICATION_COMPLETE_EVENT 0x0A |
#define | GAP_AUTHENTICATION_FAILURE_EVT 0x10 |
#define | GAP_BOND_COMPLETE_EVENT 0x0E |
#define | GAP_BOND_LOST_EVENT 0x17 |
#define | GAP_CONNECTING_CANCELLED_EVENT 0x15 |
#define | GAP_DEVICE_INIT_DONE_EVENT 0x00 |
#define | GAP_LINK_ESTABLISHED_EVENT 0x05 |
#define | GAP_LINK_PARAM_UPDATE_EVENT 0x07 |
#define | GAP_LINK_TERMINATED_EVENT 0x06 |
#define | GAP_PAIRING_REQ_EVENT 0x0F |
#define | GAP_PASSKEY_NEEDED_EVENT 0x0B |
#define | GAP_SCAN_SESSION_END_EVENT 0x12 |
Sent when an advertising report session ends. This is an internal event. | |
#define | GAP_SIGNATURE_UPDATED_EVENT 0x09 |
#define | GAP_SLAVE_REQUESTED_SECURITY_EVENT 0x0C |
#define | GAP_UPDATE_LINK_PARAM_REQ_EVENT 0x11 |
These events are received as GAP_MSG_EVENT
#define GAP_AUTHENTICATION_COMPLETE_EVENT 0x0A |
Sent when the pairing process is complete as gapAuthCompleteEvent_t.
This event will be consumed by the gapbondmgr if it is present
#define GAP_AUTHENTICATION_FAILURE_EVT 0x10 |
Sent when pairing fails due a connection termination before the process completed. This event does not have any payload.
This event will be consumed by the gapbondmgr if it is present.
#define GAP_BOND_COMPLETE_EVENT 0x0E |
Sent when the bonding process is complete as gapBondCompleteEvent_t.
This event will be consumed by the gapbondmgr if it is present
#define GAP_BOND_LOST_EVENT 0x17 |
Sent as gapBondLostEvent_t when bond has been removed on peer
#define GAP_CONNECTING_CANCELLED_EVENT 0x15 |
Sent as gapConnCancelledEvent_t when an a connecting attempt is canceled
#define GAP_DEVICE_INIT_DONE_EVENT 0x00 |
Sent after a call to GAP_DeviceInit when the Device Initialization is complete as gapDeviceInitDoneEvent_t.
#define GAP_LINK_ESTABLISHED_EVENT 0x05 |
Sent after a link has been established as gapEstLinkReqEvent_t.
#define GAP_LINK_PARAM_UPDATE_EVENT 0x07 |
Sent after the completion of a parameter update gapLinkUpdateEvent_t.
This same event is received for both the LL and L2CAP procedures.
#define GAP_LINK_TERMINATED_EVENT 0x06 |
Sent when a connection was terminated as gapTerminateLinkEvent_t.
#define GAP_PAIRING_REQ_EVENT 0x0F |
Sent when an unexpected Pairing Request is received as gapPairingReqEvent_t.
This event will be consumed by the gapbondmgr if it is present
#define GAP_PASSKEY_NEEDED_EVENT 0x0B |
Sent when a passkey is needed during pairing as gapPasskeyNeededEvent_t.
This event will be consumed by the gapbondmgr if it is present
#define GAP_SIGNATURE_UPDATED_EVENT 0x09 |
Sent when the peer device's signature counter is updated as gapSignUpdateEvent_t.
This event will be consumed by the gapbondmgr if it is present
#define GAP_SLAVE_REQUESTED_SECURITY_EVENT 0x0C |
Sent when a Slave Security Request is received as gapSlaveSecurityReqEvent_t.
This event will be consumed by the gapbondmgr if it is present
#define GAP_UPDATE_LINK_PARAM_REQ_EVENT 0x11 |
Sent when a parameter update request is received. This event is only received when GAP_PARAM_LINK_UPDATE_DECISION is set to GAP_UPDATE_REQ_PASS_TO_APP. This event is sent as gapUpdateLinkParamReqEvent_t.