Zigbee Network Processor (ZNP) Interface

Introduction

The Z-Stack Zigbee Network Processor (ZNP) is a cost-effective, low power solution that provides full Zigbee functionality with a minimal development effort. An example is already provided for the SimpleLink CC13x2 / 26x2 SDK at the following location:

<SDK_DIR>\examples\rtos\<DEVICE>_LAUNCHXL\zstack\<zc/zr/zed>_sw_ota_client\tirtos\<ccs/iar>

In this solution, the Z-Stack runs on a SoC, i.e. the CC13x2 or CC26x2 and the application runs on an external microcontroller, being any host processor. The Z-Stack ZNP handles all the Zigbee protocol tasks, and leaves the resources of the application microcontroller free to handle the application.

This makes it easy for users to add Zigbee to new or existing products at the same time as it provides great flexibility in choice of microcontroller.

Z-Stack ZNP interfaces to any microcontroller through a range of serial interfaces.

../_images/fig-single-device-znp-configuration.png

Figure 71. Single Device and ZNP Configuration

Acronyms

AF Zigbee Application Framework
API Application Programming Interface
AREQ Asynchronous Request
BDB Base Device Behavior
CTS Clear To Send
FCS Frame Check Sequence
GP Green Power
GPIO General Purpose I/O
NPI Network Processor Interface
NV Non-Volatile
PA/LNA Power Amplifier / Low Noise Amplifier (CC259x)
RTS Ready To Send
SoC System on Chip
SREQ Synchronous request
SRSP Synchronous response
UART Universal Asynchronous Receiver Transmitter
ZDO Zigbee Device Object
ZNP Zigbee Network Processor

Physical Interface

The following sections describe the physical interfaces for the ZNP.

Network Processor Signals

The figure below shows how an application processor interfaces with the CC13x2 or CC26x2.

The CC13x2 or CC26x2 ZNP uses RX/TX/RTS/CTS for UART communication. See Signal Description for details.

Pin Configurations

The CC13x2 or CC26x2 ZNP pin configurations are described in the following sections.

Default Pin Configuration

By default, the pin configurations are the following:

Transport CC13x2 or CC26x2 ZNP signal CC26x2 PIN CC23x2 PIN Direction
UART TX DIO_3 DIO_13 Out
UART RX DIO_2 DIO_12 In
UART GND GND GND In/Out
Optional Pin Configuration

If NPI_FLOW_CTRL is enabled then the following pins also apply:

Transport CC13x2 or CC26x2 ZNP signal CC13x2 or CC26x2 PIN Direction
UART CTS DIO_19 In
UART RTS DIO_18 Out

For additional information of different parameters which can be modified, refer to the Application Preprocessor Configuration.

UART Transport

Configuration

The following UART configuration is supported:

  • Baud rate: 115200
  • CTS/RTS flow control with NPI_FLOW_CTRL enabled (disabled by default)
  • 8-N-1 byte format

Frame Format

UART transport frame format is shown in the following figure. The left-most field is transmitted first over the wire. This is the same General Serial Packet defined by the Z-Stack Monitor and Test API.

Table 2. UART Transport Frame Format
SOF General Frame Format FCS
Bytes: 1 3-253 1

SOF (Start of Frame): This is always set to 0xFE.

General Frame Format: This is the general frame format as described in General Frame Format.

FCS (Frame Check Sequence): This field is computed as an XOR of all the bytes in the general format frame fields.

Sample FCS Calculation

Shown below is a C example for the FCS calculation:

unsigned char calcFCS(unsigned char *pMsg, unsigned char len)
{
  unsigned char result = 0;
  while (len--)
  {
    result ^= *pMsg++;
  }
  return result;
}

Signal Description

The following standard UART signals are used:

  • TX: Transmit data
  • RX: Receive data
  • CTS: Clear to Send
  • RTS: Ready to Send

Note

CTS/RTS are disabled by default, and are optional. You may enable CTS/RTS by defining NPI_FLOW_CTRL in the predefined symbols. For more information, refer to the Application Preprocessor Configuration.

The figure below shows the RTS/CTS flow control connections to the host processor. On the CC13x2 or CC26x2, RTS and CTS are active-low signals. The RT output is driven low when the receive register is empty and reception is enabled. Transmission of a byte does not occur before the CTS input is low.

../_images/ditaa-aa992416f2539cae865f99d24344f4701942bcf1.png

Signal Operation

UART transport sends and receives data asynchronously. Data can be sent and received simultaneously and the transfer of a frame can be initiated at any time by either the application processor or the ZNP SoC.

General Frame Format

The general frame format is shown in Table 3.. The left-most field is transmitted first over the wire. For multi-byte fields, the lowest order byte is transmitted first. This is the same General Frame Format defined by the Z-Stack Monitor and Test API.

Table 3. General Frame Format
Length Command Data
Bytes: 1 2 0-250

Length: The length of the data field of the frame. The length can range from 0-250.

Command: The Command ID for the message. Refer to Command Field for more information about the Command field.

Data: The frame data. This field contains actual data to be transmitted. This depends on the command field and is described for each command in ZNP Software Command Interface. The size can range from 0-250 bytes.

Command Field

The command field is constructed of two bytes. The bytes are formatted as shown in the following figure. The Cmd0 byte is transmitted first, followed by the Cmd1 byte.

Table 4. Command Field
Cmd0 Cmd1
Bit: 7-5 4-0 7-0
Type Subsystem Id

Type: The command type described by bits 5, 6, 7 of the Cmd0 byte. The command type has one of the following values:

Type Cmd0 Value
POLL 0x00
SREQ 0x20
AREQ 0x40
SRSP 0x60
  • 0: POLL. Not used in Z-Stack.
  • 1: SREQ: A synchronous request that requires an immediate response. For example, a function call with a return value would use an SREQ command.
  • 2: AREQ: An asynchronous request. For example, a callback event or a function call with no return value would use an AREQ command.
  • 3: SRSP: A synchronous response. This type of command is only sent in response to a SREQ command. For an SRSP command the subsystem and ID are set to the same values as the corresponding SREQ. The length of an SRSP is generally nonzero, so an SRSP with length=0 can be used to indicate an error.
  • 4-7: Reserved.

Subsystem: The subsystem of the command is described by bits 0-4 of Cmd0. The command subsystem values are shown below:

Subsystem Value Subsystem Name
0x00 RPC Error interface
0x01 SYS interface
0x02 MAC interface
0x03 NWK interface
0x04 AF interface
0x05 ZDO interface
0x06 Simple API interface
0x07 UTIL interface
0x08 DEBUG interface
0x09 APP Interface
0x0F APP config
0x15 GreenPower

ID: The command ID. The ID maps to a particular interface message.

Cmd1 provides an 8-bit command ID code, which maps to a specific interface message for the Subsystem specified in Cmd0. Therefore, each MT subsystem can provide up to 256 message handling functions.

Command Error

When an SREQ command from the Host Processor is not recognized by the ZNP, an error SRSP is returned, detailed in the two tables below.

SRSP:

Bytes: 1 1 1 1 1 1
Length = 0x03 Cmd0 = 0x60 Cmd1 = 0x00 ErrorCode ReqCmd0 ReqCmd1

Attributes:

Attribute Length (byte) Description
ErrorCode 1

The error code maps to one of the following enumerated values.

Value Description
0x01 Invalid subsystem
0x02 Invalid command ID
0x03 Invalid parameter
0x04 Invalid length
ReqCmd0 1 The Cmd0 value of the processed SREQ
ReqCmd1 1 The Cmd1 value of the processed SREQ

Initialization Procedures

CC13x2 or CC26x2 ZNP Power-up Procedure

The recommended power-up procedure is as follows:

  1. Application processor and CC13x2 or CC26x2 power up.
  2. The application processor initializes its UART interface.
  3. The application processor receives the SYS_RESET_IND message.

The CC13x2 or CC26x2 ZNP can be reset when the application processor sends a SYS_RESET_REQ message.

ZNP Software Command Interface

The ZNP software command interface is sub-divided into the following categories

  • The SYS interface (MT_SYS) provides the application processor with a low level interface to the ZNP hardware and software.
  • The AF (MT_AF) and ZDO (MT_ZDO) interfaces feature the complete Zigbee interface and can be used to create a full range of Zigbee compliant applications. The AF (Application Framework) interface allows the application processor to register its application with the ZNP and send and receive data. The ZDO (Zigbee Device Object) interface provides various Zigbee management functions like device and service discovery.
  • The UTIL (MT_UTIL) interface provides support functionalities such as setting PAN-ID, getting device info, getting NV info, subscribing callbacks, etc.
  • The APP CONF (MT_APP_CNF) interface provides support for BDB functionality such as set Install Codes, Primary or Secondary Channel, trigger different commissioning methods and other Trust Center configurations.

For further details on the MT interface, refer to the Z-Stack Monitor and Test API.

Configuration Interface

The ZNP device has numerous parameters that can be configured by the application processor. These configuration parameters are stored in non-volatile memory on the ZNP device and their values persist across a device reset.

The configuration parameters are divided into “network-specific” and “device-specific” parameters. The “network-specific” configuration parameters should be set to the same value for all ZNP devices in a Zigbee network to ensure proper network operation. The “device-specific” parameters can be set to different values on each device. These parameters are listed in detail in Device Specific Configuration Parameters and Network Specific Configuration Parameters. These configuration parameters must be written in NV for which the host processor must use the MT interface to write NV parameters into the ZNP device. Refer to the Z-Stack Monitor and Test API for further details on how to write into NV.

When the ZNP device powers up, it reads two of the configuration parameters immediately. These are the STARTOPT_CLEAR_CONFIG bit (part of the ZCD_NV_STARTUP_OPTION parameter) and the ZCD_NV_LOGICAL_TYPE parameters. Any modification of these parameters will require a ZNP device reset before they can take effect.

Device Specific Configuration Parameters

ZCD_NV_STARTUP_OPTION

These are the ZCD_NV_STARTUP_OPTION values:

  • ZCD_STARTOPT_DEFAULT_CONFIG_STATE (0x01)
  • ZCD_STARTOPT_DEFAULT_NETWORK_STATE (0x02)
  • ZCD_STARTOPT_AUTO_START (0x04)
  • ZCD_STARTOPT_CLEAR_CONFIG (ZCD_STARTOPT_DEFAULT_CONFIG_STATE)
  • ZCD_STARTOPT_CLEAR_STATE (ZCD_STARTOPT_DEFAULT_NETWORK_STATE)
  • ZCD_STARTOPT_CLEAR_NWK_FRAME_COUNTER (0x80)
Item ID Size Default Value
0x0003 1 Byte 0x00

This parameter controls the device startup options. This is a bit mask of the following values:

Bit Position Description
7 ZCD_STARTOPT_CLEAR_NWK_FRAME_COUNTER
6-2 Reserved
1 ZCD_STARTOPT_CLEAR_STATE
0 ZCD_STARTOPT_CLEAR_CONFIG
  • ZCD_STARTOPT_CLEAR_NWK_FRAME_COUNTER – If this option is set, then the network frame counter is cleared for all networks.

Note

This should be use only for debug purposes as the network frame counters must be persistant, even after Factory New resets. The usage of this option during the operation in the networks may lead to undesaried behaviour, such as get the ZNP device ignored by other devices in the network.

  • ZCD_STARTOPT_CLEAR_CONFIG – If this option is set, the device will overwrite all the configuration parameters (except this one) with the “default” values that it is programmed with. This is used to erase the existing configuration and bring the device into a known state.

Note

The ZCD_STARTOPT_CLEAR_CONFIG bit is read by the ZNP device immediately when it powers up after a reset. When the configuration parameters are restored to defaults, the ZCD_NV_STARTUP_OPTION itself is not restored except for clearing the ZCD_STARTOPT_CLEAR_CONFIG bit.

  • ZCD_STARTOPT_CLEAR_STATE – If this option is set, the device will clear its previous network state (which would exist if the device had been operating on a network prior to the reset). This is typically used during application development. During regular device operation, this flag is typically not set, so that an accidental device reset will not cause loss of network state.

The ZNP device has two kinds of information stored in non-volatile memory. The configuration parameters (in this section) and network state information (in Network Specific Configuration Parameters)

The configuration parameters are configured by the user before start of Zigbee operation.

The network state information is collected by the device after it joins a network and creates bindings (at runtime). This is not set by the application processor. This information is stored so that if the device were to reset, it can restore itself without going through the network joining and binding process again.

If the application processor does not wish to continue operating in the previous Zigbee network, it needs to instruct the ZNP device to clear the network state information and start again based on the configuration parameters. This is done by setting the ZCD_STARTOPT_CLEAR_STATE bit in the startup option.

ZCD_NV_LOGICAL_TYPE
Item ID Size Default Value
0x0087 1 Byte 0x00

This is the logical type of the device in the Zigbee network. This can be set to a ZG_DEVICETYPE_COORDINATOR (0x00), ZG_DEVICETYPE_ROUTER (0x01), or ZG_DEVICETYPE_ENDDEVICE (0x02).

Note

This parameter is read by the ZNP device immediately when it powers up after a reset.

ZCD_NV_ZDO_DIRECT_CB

This is set to TRUE by zgZdoDirectCB in zglobals.c

Item ID Size Default Value
0x008F 1 Byte TRUE

This configures the manner in which ZDO responses (hereby referred to as callbacks) are issued to the host processor. By default, this item is set to TRUE, which means that the host processor will receive the “verbose” response. For example, the host processor would receive the ZDO_IEEE_ADDR_RSP command in response to ZDO_IEEE_ADDR_REQ. If ZCD_NV_ZDO_DIRECT_CB is set to FALSE, then the host processor must use the ZDO_MSG_CB_REGISTER command to subscribe to a specific ZDO callback in order to receive it.

Network Specific Configuration Parameters

ZCD_NV_PANID
Item ID Size Default Value
0x0083 2 Bytes 0xFFFF

This parameter identifies the Zigbee network. This should be set to a value between 0 and 0x3FFF. Networks that exist in the same vicinity must have different values for this parameter. It can be set to a special value of 0xFFFF to indicate “don’t care”.

Z-Stack 3.0 ZNP Considerations

Backward compatibility

ZNP is backward compatible with non Z3.0 devices by using the same API that already existed in previous releases of the Z-Stack, or by using Base Device Behavior commissioning MT interface with exception of the new security schemas for Z3.0 such as Distributed Security Network or Install Code Derived Trust Center Link Key.

ZNP for Z3.0

While the ZNP implementation provides a compatible baseline for Zigbee 3.0 devices, a full implementation of a Zigbee 3.0 device involves additional layers on top of the ZNP. These layers shall be implemented by the user on the host-side of the stack, since they are outside the scope of the network processor. The ZNP provides several new interfaces to enable the required functionality on the host.

In order to update a legacy ZNP-based device to support Zigbee 3.0, the following main updates need to be implemented on the host:

Base Device Behavior Specification:

  1. Finding and Binding: Host processor is required to implement Finding and Binding commissioning method (either as Initiator or as Target) according to the cluster supported by the host application.
  2. Touchlink (optional): proximity-based commissioning method.

Green Power Basic Proxy:

Zigbee 3.0 coordinator and router devices must implement Green Power Basic proxy functionality. ZNP includes the necessary GP Stub interfaces which are available to the application and allow it to implement GP basic proxy functionality on the host processor.

ZNP Startup Procedure for Z3.0 Implementation

After executing the power-up procedure, the host processor must call some mandatory APIs before executing any APIs that invoke Zigbee over-the-air messaging. Not following this sequence could result in unexpected behaviour. The recommended startup procedure is as follows:

  1. The host processor must use the ZB_WRITE_CONFIGURATION command to configure at the minimum the ZCD_NV_LOGICAL_TYPE.
  2. If logical device is defined as ZC or ZR, GP basic proxy must be initialized in the host processor (No ZNP commands are required until interaction with GP devices are needed).
  3. Optional configurations to commission the device are:
  1. Set the Primary and/or Secondary channel mask to perform Formation or Network Steering.
  2. Set the PAN ID to create or join by setting ZCD_NV_PAN_ID.
  3. Set Install codes for networks which require it.
  1. AF_REGISTER command should be sent by the host processor to register the application endpoint.
  2. Host should use BDB commissioning API to create or join the network via standard network formation or joining.
  3. The host processor should wait for BDB notifications on the different commissioning methods used by the host. Also host processor can rely on the supported ZDO states reported.

Example Message Exchange

The following sequence chart is provided as a simple example of a message exchange between a Host and ZNP. In this example the following (generalized) events take place:

@startuml
participant "Host Processor" as HP
participant ZNP
note left of HP: **Step 1**: The ZNP is reset
ZNP -> HP: MT_SYS_RESET_IND (AREQ) (0x4180)
HP -> ZNP: MT_SYS_RESET_REQ (SREQ) (0x4100)
activate ZNP
ZNP --> HP: MT_SYS_RESET_IND (AREQ) (0x4180)
deactivate ZNP
note left of HP
  **Step 2**: The Host writes some configuration data
  to the ZNP into NV (""ZCD_NV_LOGICAL_TYPE"")
  which will define the Logical Device Role.
end note
HP -> ZNP: MT_SYS_WRITE_NV_REQ (SREQ) (0x2109)
activate ZNP
ZNP --> HP: MT_SYS_WRITE_NV_RSP (SRSP) (0x6109)
deactivate ZNP
HP -> ZNP: MT_SYS_RESET_REQ (SREQ) (0x4100)
activate ZNP
ZNP --> HP: MT_SYS_RESET_IND (AREQ) (0x4180)
deactivate ZNP
note left of HP
  **Step 3**: An endpoint in the host
  is registered with the ZNP.
end note
HP -> ZNP: MT_AF_REGISTER (SREQ) (0x2400)
activate ZNP
ZNP --> HP: MT_AF_REGISTER (SRSP) (0x6400)
deactivate ZNP
note left of HP
  **Step 4**: ZNP device starts a commissioning
  method according to device role from Step 2
  (e.g. Commissioning Formation for ZC/ZR, or
  Commissioning Network Steering for ZR/ZED)
end note
HP -> ZNP: MT_APP_CNF_BDB_START_COMMISSIONING (SREQ) (0x2F05)
activate ZNP
ZNP --> HP: MT_APP_CNF_BDB_START_COMMISSIONING (SRSP) (0x6F05)
deactivate ZNP
note right of ZNP
  **Step 5**: BDB reports the result of the
  commissioning method execution.
end note
ZNP -> HP: MT_APP_CNF_BDB_NOTIFICATION (AREQ) (0x4F80)
ZNP -> HP: MT_ZDO_STATE_CHANGE_IND (AREQ) (0x45C0)
ZNP -> HP: MT_ZDO_STATE_CHANGE_IND (AREQ) (0x45C0)
note right of ZNP
  **Step 6**: Another device joins the network,
  indicated by the ZDO Device Indications.
end note
ZNP -> HP: MT_ZDO_TC_DEVICE_IND (AREQ) (0x45CA)
ZNP -> HP: MT_ZDO_TC_DEVICE_IND (AREQ) (0x45CA)
note left of HP
  **Step 7**: Data is exchanged between the Host+ZNP
  and joining device through AF Data Requests
  and AF Incoming Messages.
end note
HP -> ZNP: MT_AF_DATA_REQ (SREQ) (0x2401)
activate ZNP
ZNP --> HP: MT_AF_DATA_REQ (SRSP) (0x6401)
deactivate ZNP
HP -> ZNP: MT_AF_DATA_CNF (AREQ) (0x4480)
activate ZNP
ZNP --> HP: MT_AF_INCOMING_MSG (AREQ) (0x4481)
deactivate ZNP
@enduml

Figure 72. Example Message Sequence Chart

Return Values

The status parameter that is returned from the ZNP device may take one of the following values:

Table 5. General Collection of Status Values
Name Value
ZSuccess 0x00
ZFailure 0x01
ZInvalidParameter 0x02
ZDecodeError 0x03
NV_ITEM_UNINIT 0x09
NV_OPER_FAILED 0x0a
NV_BAD_ITEM_LEN 0x0c
ZMemError 0x10
ZBufferFull 0x11
ZUnsupportedMode 0x12
ZMacMemError 0x13
ZSapiInProgress 0x20
ZSapiTimeout 0x21
ZSapiInit 0x22
ZNotAuthorized 0x7E
ZMalformedCmd 0x80
ZUnsupClusterCmd 0x81
ZOtaAbort 0x95
ZOtaImageInvalid 0x96
ZOtaWaitForData 0x97
ZOtaNoImageAvailable 0x98
ZOtaRequireMoreImage 0x99
ZApsFail 0xb1
ZApsTableFull 0xb2
ZApsIllegalRequest 0xb3
ZApsInvalidBinding 0xb4
ZApsUnsupportedAttrib 0xb5
ZApsNotSupported 0xb6
ZApsNoAck 0xb7
ZApsDuplicateEntry 0xb8
ZApsNoBoundDevice 0xb9
ZApsNotAllowed 0xba
ZApsNotAuthenticated 0xbb
ZSecNoKey 0xa1
ZSecOldFrmCount 0xa2
ZSecMaxFrmCount 0xa3
ZSecCcmFail 0xa4
ZNwkInvalidParam 0xc1
ZNwkInvalidRequest 0xc2
ZNwkNotPermitted 0xc3
ZNwkStartupFailure 0xc4
ZNwkTableFull 0xc7
ZNwkUnknownDevice 0xc8
ZNwkUnsupportedAttribute 0xc9
ZNwkNoNetworks 0xca
ZNwkLeaveUnconfirmed 0xcb
ZNwkNoAck 0xcc
ZNwkNoRoute 0xcd
ZMacNoACK 0xe9
ZAfDuplicateEndpoint 0xd0
ZAfEndpointMax 0xd1
Table 6. Common ZDO Status Values
Name Value Description
SUCCESS 0x00 Operation completed successfully
INVALID_REQTYPE 0x80 Supplied request type invalid
DEVICE_NOT_FOUND 0x81 Device not found
INVALID_EP 0x82 Invalid Endpoint value
NOT_ACTIVE 0x83 Endpoint not described by simple description
NOT_SUPPORTED 0x84 Optional feature not supported
TIMEOUT 0x85 Operation timed out
NO_MATCH 0x86 No match for End Device bind
NO_ENTRY 0x88 Unbind request failed, no entry
NO_DESCRIPTOR 0x89 Child descriptor not available
INSUFFICIENT_SPACE 0x8a Insufficient space to support operation
NOT_PERMITTED 0x8b Not in proper state to support operation
TABLE_FULL 0x8c No table space to support operation
NOT_AUTHORIZED 0x8d Permissions indicate request not authorized
BINDING_TABLE_FULL 0x8e No binding table space to support operation

Additional Considerations for ZNP device in Z-Stack 3.0

  1. The current version of ZNP device does not support commissioning GP devices in the network if these devices require the basic proxy device to switch channel during this commissioning process. Other commissioning methods require that a Host Processor drives the commissioning process in the application level.

Additional Information

For additional details of the individual commands, please refer to the Z-Stack Monitor and Test API.