Data Fields
PDMCC26XX_StreamNotification Struct Reference

A PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors. More...

#include <PDMCC26XX.h>

Data Fields

void * arg
 
PDMCC26XX_Status status
 

Detailed Description

A PDMCC26XX_StreamNotification data structure is used with PDMCC26XX_CallbackFxn(). Provides notification about available buffers and potential errors.

Field Documentation

§ arg

void* PDMCC26XX_StreamNotification::arg

Argument to be passed to the callback function

§ status

PDMCC26XX_Status PDMCC26XX_StreamNotification::status

Status code set by PDMCC26XX driver


The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale