Macros | |
#define | I2C_STATUS_SUCCESS (0) |
Successful status code returned by I2C API. More... | |
#define | I2C_STATUS_ERROR (-1) |
Generic error status code returned by I2C API. More... | |
#define | I2C_STATUS_TIMEOUT (-2) |
Timeout status code returned by I2C API. More... | |
#define | I2C_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by I2C_control() for undefined command codes. More... | |
I2C_STATUS_* macros are general status codes returned by the I2C API
I2CCC26XX_STATUS_* macros are command codes only defined in the I2CCC26XX.h driver implementation and need to:
#define I2C_STATUS_SUCCESS (0) |
Successful status code returned by I2C API.
#define I2C_STATUS_ERROR (-1) |
Generic error status code returned by I2C API.
#define I2C_STATUS_TIMEOUT (-2) |
Timeout status code returned by I2C API.
#define I2C_STATUS_UNDEFINEDCMD (-2) |
An error status code returned by I2C_control() for undefined command codes.