TI BLE5-Stack API Documentation
2.01.00.00
|
This module implements Real Time Localization System (RTLS) Control module. More...
Modules | |
RTLS Control Structures | |
Files | |
file | rtls_ble.h |
Stack specific BLE structures needed for RTLS Control. | |
file | rtls_ctrl.h |
RTLS Control module interface. | |
file | rtls_ctrl.h |
RTLS Control module interface. | |
file | rtls_ctrl_api.h |
This file contains the RTLS Control API's. | |
file | rtls_ctrl_tof.h |
This file contains the functions and structures specific to ToF post processing. | |
file | rtls_host.h |
This file contains the host abstraction layer for a RTLS Host. | |
Data Structures | |
struct | rtlsConfiguration_t |
RTLS Configuration structure. More... | |
struct | rtlsCtrlReq_t |
RTLS Control request. More... | |
struct | rtlsPacket_t |
RTLS Packet - Generic structure that will be translated to a specific command. More... | |
Macros | |
#define | CHIP_ID_ADDR ((uint8_t *)(0x50001000 + 0x2E8)) |
Chip Identifier Address. | |
#define | CHIP_ID_SIZE 6 |
Chip Identifier Size. | |
#define | HAL_ASSERT_CAUSE_OUT_OF_MEMORY 0x04 |
RTLS Assert Error code. | |
#define | MAX_SAMPLES_SINGLE_CHUNK 32 |
Max number of samples reported in a single chunk when using RAW mode. | |
#define | MAX_TOF_SAMPLES_SINGLE_CHUNK 16 |
Max Num of Samples. | |
#define | RTLS_CMD_AOA_ENABLE 0x14 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_ANGLE 0x23 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_PAIR_ANGLES 0x25 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_RAW 0x24 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_SET_PARAMS 0x13 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONN_INFO 0x27 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONN_PARAMS 0x02 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONNECT 0x03 |
RTLS Node Manager command. | |
#define | RTLS_CMD_GET_RTLS_PARAM 0x29 |
RTLS Node Manager command. | |
#define | RTLS_CMD_IDENTIFY 0x00 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED 0x01 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESET_DEVICE 0x20 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SCAN 0x04 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SCAN_STOP 0x05 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SET_RTLS_PARAM 0x28 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TERMINATE_LINK 0x22 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_CALIB_NV_READ 0x30 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_CALIBRATE 0x26 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_ENABLE 0x12 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_GET_SEC_SEED 0x10 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_RESULT_DIST 0x06 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_RESULT_RAW 0x08 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_RESULT_STAT 0x07 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_SET_PARAMS 0x11 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_SET_SEC_SEED 0x09 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_SWITCH_ROLE 0x31 |
RTLS Node Manager command. | |
#define | RTLS_CTRL_ALL_EVENTS (RTLS_QUEUE_EVT) |
RTLS Task configuration. | |
#define | RTLS_CTRL_REV 0x1 |
#define | RTLS_CTRL_TASK_PRIORITY 2 |
RTLS Task configuration variable. | |
#define | RTLS_CTRL_TASK_STACK_SIZE 752 |
RTLS Task configuration variable. | |
#define | RTLS_CTRL_TOF_RSSI_THRESHOLD_HYSTERESIS -5 |
RSSI Hysteresis threshold. | |
#define | RTLS_EVT_ASSERT 0x80 |
RTLS async event. | |
#define | RTLS_EVT_CONN_INFO 0x83 |
RTLS async event. | |
#define | RTLS_EVT_DEBUG 0x82 |
RTLS async event. | |
#define | RTLS_EVT_ERROR 0x81 |
RTLS async event. | |
#define | RTLS_FALSE 0 |
FALSE. | |
#define | RTLS_PARAM_2 0x02 |
RTLS Param type RTLS_CMD_SET_RTLS_PARAM command. | |
#define | RTLS_PARAM_3 0x03 |
RTLS Param type RTLS_CMD_SET_RTLS_PARAM command. | |
#define | RTLS_PARAM_CONNECTION_INTERVAL 0x01 |
RTLS Param type RTLS_CMD_SET_RTLS_PARAM command. | |
#define | RTLS_QUEUE_EVT UTIL_QUEUE_EVENT_ID |
Event_Id_30. | |
#define | RTLS_REQ_AOA_ENABLE 0x7 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_CONN 0x2 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_ENABLE_SYNC 0x1 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_SCAN 0x3 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_SEND_DATA 0x4 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_SET_AOA_PARAMS 0x6 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_TERMINATE_LINK 0x5 |
RTLS Application Command Opcode. | |
#define | RTLS_REQ_UPDATE_CONN_INTERVAL 0x8 |
RTLS Application Command Opcode. | |
#define | RTLS_TOF_FREQ_PER_NV_BLOCK 4 |
Max Num of frequencies per NV block. | |
#define | RTLS_TRUE 1 |
TRUE. | |
#define | RTLSUTIL_FREE(pFree) |
RTLSUTIL_FREE memory free without icall. More... | |
#define | RTLSUTIL_MALLOC(pAlloc, size) |
RTLSUTIL_MALLOC memory allocation without icall. More... | |
#define | SNV_ID_CAL_DATA_SET BLE_NVID_CUST_START+1 |
#define | SNV_ID_CAL_PARAMS BLE_NVID_CUST_START |
Typedefs | |
typedef void(* | pfnRtlsAppCb) (uint8_t *cmd) |
Application callback function. | |
Enumerations | |
enum | rtlsCapabilities_e { RTLS_CAP_NOT_INITIALIZED = 0x00000000, RTLS_CAP_CM = 0x00000001, RTLS_CAP_AOA_TX = 0x00000002, RTLS_CAP_AOA_RX = 0x00000004, RTLS_CAP_TOF_SLAVE = 0x00000008, RTLS_CAP_TOF_PASSIVE = 0x00000010, RTLS_CAP_TOF_MASTER = 0x00000020, RTLS_CAP_RTLS_SLAVE = 0x00000040, RTLS_CAP_RTLS_MASTER = 0x00000080, RTLS_CAP_RTLS_PASSIVE = 0x00000100 } |
Enumeration for RTLS Capabilities. | |
enum | rtlsStatus_e { RTLS_SUCCESS, RTLS_FAIL, RTLS_LINK_LOST, RTLS_LINK_ESTAB_FAIL, RTLS_LINK_TERMINATED, RTLS_OUT_OF_MEMORY, RTLS_ILLEGAL_CMD } |
Enumeration for RTLS Status. | |
Functions | |
void | RTLSCtrl_aoaResultEvt (int8_t rssi, uint8_t channel, uint16_t numIqSamples, uint8_t sampleRate, uint8_t sampleCtrl, uint8_t sampleSize, uint8_t numAnt, uint8_t antArraySwitchIo, int8_t *pI, int8_t *pQ) |
RTLSCtrl_aoaResultEvt. More... | |
void | RTLSCtrl_connInfoEvt (uint8_t *connInfo, uint16_t connInfoLen) |
RTLS Control Connection Info. More... | |
void | RTLSCtrl_connResultEvt (uint8_t status) |
RTLS Control Connection Results. More... | |
void | RTLSCtrl_initAoa (void) |
Initialize AoA - has to be called before running AoA. More... | |
rtlsStatus_e | RTLSCtrl_loadAndverifyCalibNVParams (rtlsTof_t *tofControlBlock) |
Verify calibration and load calibration from NV. More... | |
void * | RTLSCtrl_malloc (uint32_t sz) |
This function will allocate memory, if we were unable to allocate we will report to RTLS Host. More... | |
void | RTLSCtrl_open (rtlsConfiguration_t *rtlsConfig) |
RTLSCtrl_open. More... | |
void | RTLSCtrl_outputCalibFromNV (uint8_t cmdId, uint8_t numFreq, uint16_t calibDistance, ToF_BurstStat *pCalibVals) |
Output calibration parameters and values. More... | |
void | RTLSCtrl_outputTofStat (uint8_t cmdId, uint16_t numFreq, ToF_BurstStat *tofStatArray, uint8_t rssi) |
Output array of ToF_BurstStat. More... | |
void | RTLSCtrl_postProcessAoa (rtlsAoaIqEvt_t *pEvt) |
Called at the end of each connection event to extract I/Q samples. More... | |
void | RTLSCtrl_postProcessTof (rtlsTof_t *tofControlBlock, int8_t rssi) |
Post process a ToF run. More... | |
void | RTLSCtrl_processDataSent (uint8_t status) |
RTLS Application Data Sent. More... | |
void | RTLSCtrl_processRtlsPacket (uint8_t *pPkt) |
RTLSCtrl_processRtlsPacket. More... | |
void | RTLSCtrl_readCalibFromNV (rtlsTof_t *tofControlBlock) |
Read calibration From NV. More... | |
void | RTLSCtrl_scanResultEvt (rtlsStatus_e status, uint8_t *scanResult, uint8_t size) |
RTLS Control Scan Results. More... | |
void | RTLSCtrl_sendDebugEvent (uint8_t *debug_string, uint32_t debug_value) |
RTLSCtrl_sendDebugEvent. More... | |
void | RTLSCtrl_setResultMode (uint8_t resultMode) |
Set result mode for AoA post processing function. More... | |
void | RTLSCtrl_syncEventNotify (rtlsStatus_e status, uint32_t timeToNextEvent, int8_t rssi, uint8_t channel) |
RTLSCtrl_syncEventNotify. More... | |
rtlsStatus_e | RTLSCtrl_writeCalibToNV (rtlsTofCalibParams_t calibParams, ToF_BurstStat *pCalibVals) |
Write calibration to NV. More... | |
void | RTLSHost_openHostIf (pfnRtlsCtrlProcessMsgCb rtlsHostMsgCb) |
This function opens the host interface and registers the application callback. More... | |
uint8_t | RTLSHost_sendMsg (uint8_t cmdId, uint8_t cmdType, uint8_t *pData, uint16_t dataLen) |
This function is an abstraction of sending messages to a RTLS Host. More... | |
This module implements Real Time Localization System (RTLS) Control module.
#define RTLSUTIL_FREE | ( | pFree | ) |
RTLSUTIL_FREE memory free without icall.
#define RTLSUTIL_MALLOC | ( | pAlloc, | |
size | |||
) |
RTLSUTIL_MALLOC memory allocation without icall.
void RTLSCtrl_aoaResultEvt | ( | int8_t | rssi, |
uint8_t | channel, | ||
uint16_t | numIqSamples, | ||
uint8_t | sampleRate, | ||
uint8_t | sampleCtrl, | ||
uint8_t | sampleSize, | ||
uint8_t | numAnt, | ||
uint8_t | antArraySwitchIo, | ||
int8_t * | pI, | ||
int8_t * | pQ | ||
) |
RTLSCtrl_aoaResultEvt.
RTLS Control I/Q samples processing function Results will be output to RTLS Node Manager after processing
rssi | - rssi for this CTE |
channel | - channel this CTE was captured on |
numIqSamples- | Number of I/Q samples |
sampleRate | - Sampling rate that was used for the run |
sampleSize | - Sample Size 1 = 8 bit, 2 = 16 bit |
sampleCtrl | - Sampling control flags |
numAnt | - Number of Antennas that were used for the run |
antArraySwitchIo | - GPIO for antenna array switching |
pI | - Pointer to I samples |
pQ | - Pointer to Q samples |
void RTLSCtrl_connInfoEvt | ( | uint8_t * | connInfo, |
uint16_t | connInfoLen | ||
) |
RTLS Control Connection Info.
This function sends connection information and parameters to RTLS Control
connInfo | - Connection information |
connInfoLen | - Connection Information length (needed to send the packet over NPI) |
void RTLSCtrl_connResultEvt | ( | uint8_t | status | ) |
RTLS Control Connection Results.
This function notifies the RTLS Control that a connection has been formed
status | - Whether the connection was formed successfully |
void RTLSCtrl_initAoa | ( | void | ) |
Initialize AoA - has to be called before running AoA.
rtlsStatus_e RTLSCtrl_loadAndverifyCalibNVParams | ( | rtlsTof_t * | tofControlBlock | ) |
Verify calibration and load calibration from NV.
tofControlBlock | - pointer to ToF control block |
void* RTLSCtrl_malloc | ( | uint32_t | sz | ) |
This function will allocate memory, if we were unable to allocate we will report to RTLS Host.
sz | - size (Allocated pointer has to be cast) |
void RTLSCtrl_open | ( | rtlsConfiguration_t * | rtlsConfig | ) |
RTLSCtrl_open.
Used to create and initialize the RTLS Control task
rtlsConfig | - pointer to the RTLS Application callbacks |
void RTLSCtrl_outputCalibFromNV | ( | uint8_t | cmdId, |
uint8_t | numFreq, | ||
uint16_t | calibDistance, | ||
ToF_BurstStat * | pCalibVals | ||
) |
Output calibration parameters and values.
cmdId | - RTLS_CMD_TOF_* - command to the host |
numFreq | - Needed for size calculation |
calibrationOffset | - The distance at which calibration is being performed (will be subtracted from final result) |
tofCalArray | - Calibration array |
void RTLSCtrl_outputTofStat | ( | uint8_t | cmdId, |
uint16_t | numFreq, | ||
ToF_BurstStat * | tofStatArray, | ||
uint8_t | rssi | ||
) |
Output array of ToF_BurstStat.
cmdId | - RTLS_CMD_TOF_* - command to the host |
numFreq | - needed for size calculation |
tofStatArray | - Array to output |
rssi | - current rssi |
void RTLSCtrl_postProcessAoa | ( | rtlsAoaIqEvt_t * | pEvt | ) |
Called at the end of each connection event to extract I/Q samples.
pEvt | - Pointer to IQ Event |
void RTLSCtrl_postProcessTof | ( | rtlsTof_t * | tofControlBlock, |
int8_t | rssi | ||
) |
Post process a ToF run.
tofControlBlock | - pointer to ToF information |
rssi | - current rssi |
void RTLSCtrl_processDataSent | ( | uint8_t | status | ) |
RTLS Application Data Sent.
This function is used by the RTLS Application to report the status of a sent packet This is used to let RTLS Control know whether RTLS data has been successfully transmitted
status | - SUCCESS or FAILURE for sending data to our peer |
void RTLSCtrl_processRtlsPacket | ( | uint8_t * | pPkt | ) |
RTLSCtrl_processRtlsPacket.
This function is used by the RTLS Application to notify RTLS Control that a RTLS packet has been received
pPkt | - The RTLS packet to parse |
void RTLSCtrl_readCalibFromNV | ( | rtlsTof_t * | tofControlBlock | ) |
Read calibration From NV.
tofControlBlock | - pointer to ToF control block |
void RTLSCtrl_scanResultEvt | ( | rtlsStatus_e | status, |
uint8_t * | scanResult, | ||
uint8_t | size | ||
) |
RTLS Control Scan Results.
This function notifies the RTLS Control that a connection has been formed
scanResult | - Pointer to scan results array |
size | - Size of scanResults array |
status | - scanResults status |
void RTLSCtrl_sendDebugEvent | ( | uint8_t * | debug_string, |
uint32_t | debug_value | ||
) |
RTLSCtrl_sendDebugEvent.
Send debug info
debug_string | - 32 bytes debug string |
debug_value | - 32 bits debug value |
void RTLSCtrl_setResultMode | ( | uint8_t | resultMode | ) |
Set result mode for AoA post processing function.
resultMode | - New result mode |
void RTLSCtrl_syncEventNotify | ( | rtlsStatus_e | status, |
uint32_t | timeToNextEvent, | ||
int8_t | rssi, | ||
uint8_t | channel | ||
) |
RTLSCtrl_syncEventNotify.
Synchronization function provided to the Application by RTLS Control This is the function that the application will be calling when a sync event is in place e.g BLE Connection Event
timeToNextEvent | - the time until the next sync event |
rssi | - rssi measurement against the RTLS Slave |
channel | - the channel on which the syncEvent was received |
status |
rtlsStatus_e RTLSCtrl_writeCalibToNV | ( | rtlsTofCalibParams_t | calibParams, |
ToF_BurstStat * | pCalibVals | ||
) |
Write calibration to NV.
pCalibVals | - pointer to calibration values |
calibParams | - calibration parameters |
void RTLSHost_openHostIf | ( | pfnRtlsCtrlProcessMsgCb | rtlsHostMsgCb | ) |
This function opens the host interface and registers the application callback.
rtlsHostMsgCb | - Callback to use when a message arrives |
uint8_t RTLSHost_sendMsg | ( | uint8_t | cmdId, |
uint8_t | cmdType, | ||
uint8_t * | pData, | ||
uint16_t | dataLen | ||
) |
This function is an abstraction of sending messages to a RTLS Host.
cmdId | - RTLS Cmd Id |
cmdType | - Async/Sync message |
pData | - Pointer to message data |
dataLen | - Length of data in pData |