![]() |
![]() |
ADCBuf parameters used with ADCBuf_open(). More...
#include <ADCBuf.h>
Data Fields | |
uint32_t | blockingTimeout |
uint32_t | samplingFrequency |
ADCBuf_Return_Mode | returnMode |
ADCBuf_Callback | callbackFxn |
ADCBuf_Recurrence_Mode | recurrenceMode |
void * | custom |
ADCBuf parameters used with ADCBuf_open().
ADCBuf_Params_init() must be called prior to setting fields in this structure.
uint32_t ADCBuf_Params::blockingTimeout |
Timeout in system clock ticks. This value is only valid when using ADCBuf_RETURN_MODE_BLOCKING. A call to ADCBuf_convert() will block for a duration up to blockingTimeout
ticks. The call to ADCBuf_convert() will return prior if the requested number of samples in ADCBuf_Conversion.samplesRequestedCount are completed. The blockingTimeout
should be large enough to allow for ADCBuf_Conversion.samplesRequestedCount samples to be collected given the ADCBuf_Params.samplingFrequency.
uint32_t ADCBuf_Params::samplingFrequency |
The frequency at which the ADC will sample in Hertz (Hz). After a call to ADCBuf_convert(), the ADC will perform samplingFrequency
samples per second.
ADCBuf_Return_Mode ADCBuf_Params::returnMode |
ADCBuf_Return_Mode for all conversions.
ADCBuf_Callback ADCBuf_Params::callbackFxn |
Pointer to a ADCBuf_Callback function to be invoked after a conversion completes when operating in ADCBuf_RETURN_MODE_CALLBACK.
ADCBuf_Recurrence_Mode ADCBuf_Params::recurrenceMode |
ADCBuf_Recurrence_Mode for all conversions.
void* ADCBuf_Params::custom |
Pointer to a device specific extension of the ADCBuf_Params