![]() |
0.01.00
|
This module includes functions for all Thread roles. More...
Classes | |
| struct | otMasterKey |
| This structure represents a Thread Master Key. More... | |
| struct | otNetworkName |
| This structure represents a Network Name. More... | |
| struct | otExtendedPanId |
| This structure represents an Extended PAN ID. More... | |
| struct | otMeshLocalPrefix |
| This structure represents a Mesh Local Prefix. More... | |
| struct | otPSKc |
| This structure represents PSKc. More... | |
| struct | otSecurityPolicy |
| This structure represent Security Policy. More... | |
| struct | otOperationalDatasetComponents |
| This structure represents presence of different components in Active or Pending Operational Dataset. More... | |
| struct | otOperationalDataset |
| This structure represents an Active or Pending Operational Dataset. More... | |
| struct | otBorderRouterConfig |
| This structure represents a Border Router configuration. More... | |
| struct | otExternalRouteConfig |
| This structure represents an External Route configuration. More... | |
| struct | otLinkModeConfig |
| This structure represents an MLE Link Mode configuration. More... | |
| struct | otNeighborInfo |
| This structure holds diagnostic information for a neighboring Thread node. More... | |
| struct | otLeaderData |
| This structure represents the Thread Leader Data. More... | |
| struct | otRouterInfo |
| This structure holds diagnostic information for a Thread Router. More... | |
| struct | otIpCounters |
| This structure represents the IP level counters. More... | |
| struct | otMleCounters |
| This structure represents the Thread MLE counters. More... | |
| struct | otThreadParentResponseInfo |
| This structure represents the MLE Parent Response data. More... | |
Macros | |
| #define | OT_MASTER_KEY_SIZE 16 |
| Size of the Thread Master Key (bytes) | |
| #define | OT_NETWORK_NAME_MAX_SIZE 16 |
| Maximum size of the Thread Network Name field (bytes) | |
| #define | OT_EXT_PAN_ID_SIZE 8 |
| Size of a Thread PAN ID (bytes) | |
| #define | OT_MESH_LOCAL_PREFIX_SIZE 8 |
| Size of the Mesh Local Prefix (bytes) | |
| #define | OT_PSKC_MAX_SIZE 16 |
| Maximum size of the PSKc (bytes) | |
| #define | OT_CHANNEL_1_MASK (1 << 1) |
| Channel 1. | |
| #define | OT_CHANNEL_2_MASK (1 << 2) |
| Channel 2. | |
| #define | OT_CHANNEL_3_MASK (1 << 3) |
| Channel 3. | |
| #define | OT_CHANNEL_4_MASK (1 << 4) |
| Channel 4. | |
| #define | OT_CHANNEL_5_MASK (1 << 5) |
| Channel 5. | |
| #define | OT_CHANNEL_6_MASK (1 << 6) |
| Channel 6. | |
| #define | OT_CHANNEL_7_MASK (1 << 7) |
| Channel 7. | |
| #define | OT_CHANNEL_8_MASK (1 << 8) |
| Channel 8. | |
| #define | OT_CHANNEL_9_MASK (1 << 9) |
| Channel 9. | |
| #define | OT_CHANNEL_10_MASK (1 << 10) |
| Channel 10. | |
| #define | OT_CHANNEL_11_MASK (1 << 11) |
| Channel 11. | |
| #define | OT_CHANNEL_12_MASK (1 << 12) |
| Channel 12. | |
| #define | OT_CHANNEL_13_MASK (1 << 13) |
| Channel 13. | |
| #define | OT_CHANNEL_14_MASK (1 << 14) |
| Channel 14. | |
| #define | OT_CHANNEL_15_MASK (1 << 15) |
| Channel 15. | |
| #define | OT_CHANNEL_16_MASK (1 << 16) |
| Channel 16. | |
| #define | OT_CHANNEL_17_MASK (1 << 17) |
| Channel 17. | |
| #define | OT_CHANNEL_18_MASK (1 << 18) |
| Channel 18. | |
| #define | OT_CHANNEL_19_MASK (1 << 19) |
| Channel 19. | |
| #define | OT_CHANNEL_20_MASK (1 << 20) |
| Channel 20. | |
| #define | OT_CHANNEL_21_MASK (1 << 21) |
| Channel 21. | |
| #define | OT_CHANNEL_22_MASK (1 << 22) |
| Channel 22. | |
| #define | OT_CHANNEL_23_MASK (1 << 23) |
| Channel 23. | |
| #define | OT_CHANNEL_24_MASK (1 << 24) |
| Channel 24. | |
| #define | OT_CHANNEL_25_MASK (1 << 25) |
| Channel 25. | |
| #define | OT_CHANNEL_26_MASK (1 << 26) |
| Channel 26. | |
| #define | OT_NETWORK_DATA_ITERATOR_INIT 0 |
| Initializer for otNetworkDataIterator. | |
| #define | OT_NETWORK_DIAGNOSTIC_TYPELIST_MAX_ENTRIES 19 |
| Maximum Number of Network Diagnostic TLV Types to Request or Reset. | |
| #define | OT_NEIGHBOR_INFO_ITERATOR_INIT 0 |
| Initializer for otNeighborInfoIterator. | |
Typedefs | |
| typedef struct otMasterKey | otMasterKey |
| This structure represents a Thread Master Key. | |
| typedef struct otNetworkName | otNetworkName |
| This structure represents a Network Name. | |
| typedef struct otExtendedPanId | otExtendedPanId |
| This structure represents an Extended PAN ID. | |
| typedef struct otMeshLocalPrefix | otMeshLocalPrefix |
| This structure represents a Mesh Local Prefix. | |
| typedef struct otPSKc | otPSKc |
| This structure represents a PSKc. | |
| typedef struct otSecurityPolicy | otSecurityPolicy |
| This structure represent Security Policy. | |
| typedef uint32_t | otChannelMask |
| This type represents Channel Mask. | |
| typedef struct otOperationalDatasetComponents | otOperationalDatasetComponents |
| This structure represents presence of different components in Active or Pending Operational Dataset. | |
| typedef struct otOperationalDataset | otOperationalDataset |
| This structure represents an Active or Pending Operational Dataset. More... | |
| typedef enum otMeshcopTlvType | otMeshcopTlvType |
| This enumeration represents meshcop TLV types. | |
| typedef uint32_t | otNetworkDataIterator |
| Used to iterate through Network Data information. | |
| typedef struct otBorderRouterConfig | otBorderRouterConfig |
| This structure represents a Border Router configuration. | |
| typedef struct otExternalRouteConfig | otExternalRouteConfig |
| This structure represents an External Route configuration. | |
| typedef enum otRoutePreference | otRoutePreference |
| Defines valid values for member mPreference in otExternalRouteConfig and otBorderRouterConfig. | |
| typedef struct otLinkModeConfig | otLinkModeConfig |
| This structure represents an MLE Link Mode configuration. | |
| typedef int16_t | otNeighborInfoIterator |
| Used to iterate through neighbor table. | |
| typedef struct otLeaderData | otLeaderData |
| This structure represents the Thread Leader Data. | |
| typedef struct otIpCounters | otIpCounters |
| This structure represents the IP level counters. | |
| typedef struct otMleCounters | otMleCounters |
| This structure represents the Thread MLE counters. | |
| typedef struct otThreadParentResponseInfo | otThreadParentResponseInfo |
| This structure represents the MLE Parent Response data. | |
| typedef void(* | otReceiveDiagnosticGetCallback) (otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext) |
| This function pointer is called when Network Diagnostic Get response is received. More... | |
| typedef void(OTCALL * | otThreadParentResponseCallback) (otThreadParentResponseInfo *aInfo, void *aContext) |
| This function pointer is called every time an MLE Parent Response message is received. More... | |
Functions | |
| OTAPI bool OTCALL | otDatasetIsCommissioned (otInstance *aInstance) |
| This function indicates whether a valid network is present in the Active Operational Dataset or not. More... | |
| OTAPI otError OTCALL | otDatasetGetActive (otInstance *aInstance, otOperationalDataset *aDataset) |
| This function gets the Active Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSetActive (otInstance *aInstance, const otOperationalDataset *aDataset) |
| This function sets the Active Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetGetPending (otInstance *aInstance, otOperationalDataset *aDataset) |
| This function gets the Pending Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSetPending (otInstance *aInstance, const otOperationalDataset *aDataset) |
| This function sets the Pending Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtActiveGet (otInstance *aInstance, const otOperationalDatasetComponents *aDatasetComponents, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress) |
| This function sends MGMT_ACTIVE_GET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtActiveSet (otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_ACTIVE_SET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtPendingGet (otInstance *aInstance, const otOperationalDatasetComponents *aDatasetComponents, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress) |
| This function sends MGMT_PENDING_GET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtPendingSet (otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_PENDING_SET. More... | |
| OTAPI uint32_t OTCALL | otDatasetGetDelayTimerMinimal (otInstance *aInstance) |
| Get minimal delay timer. More... | |
| OTAPI otError OTCALL | otDatasetSetDelayTimerMinimal (otInstance *aInstance, uint32_t aDelayTimerMinimal) |
| Set minimal delay timer. More... | |
| OTAPI otError OTCALL | otNetDataGet (otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength) |
| This method provides a full or stable copy of the Leader's Thread Network Data. More... | |
| OTAPI otError OTCALL | otNetDataGetNextOnMeshPrefix (otInstance *aInstance, otNetworkDataIterator *aIterator, otBorderRouterConfig *aConfig) |
| This function gets the next On Mesh Prefix in the partition's Network Data. More... | |
| otError | otNetDataGetNextRoute (otInstance *aInstance, otNetworkDataIterator *aIterator, otExternalRouteConfig *aConfig) |
| This function gets the next external route in the partition's Network Data. More... | |
| OTAPI uint8_t OTCALL | otNetDataGetVersion (otInstance *aInstance) |
| Get the Network Data Version. More... | |
| OTAPI uint8_t OTCALL | otNetDataGetStableVersion (otInstance *aInstance) |
| Get the Stable Network Data Version. More... | |
| OTAPI otError OTCALL | otThreadSetEnabled (otInstance *aInstance, bool aEnabled) |
| This function starts Thread protocol operation. More... | |
| OTAPI bool OTCALL | otThreadGetAutoStart (otInstance *aInstance) |
| This function queries if the Thread stack is configured to automatically start on reinitialization. More... | |
| OTAPI otError OTCALL | otThreadSetAutoStart (otInstance *aInstance, bool aStartAutomatically) |
| This function configures the Thread stack to automatically start on reinitialization. More... | |
| OTAPI bool OTCALL | otThreadIsSingleton (otInstance *aInstance) |
| This function indicates whether a node is the only router on the network. More... | |
| OTAPI otError OTCALL | otThreadDiscover (otInstance *aInstance, uint32_t aScanChannels, uint16_t aPanId, bool aJoiner, bool aEnableEui64Filtering, otHandleActiveScanResult aCallback, void *aCallbackContext) |
| This function starts a Thread Discovery scan. More... | |
| OTAPI bool OTCALL | otThreadIsDiscoverInProgress (otInstance *aInstance) |
| This function determines if an MLE Thread Discovery is currently in progress. More... | |
| OTAPI uint32_t OTCALL | otThreadGetChildTimeout (otInstance *aInstance) |
| Get the Thread Child Timeout used when operating in the Child role. More... | |
| OTAPI void OTCALL | otThreadSetChildTimeout (otInstance *aInstance, uint32_t aTimeout) |
| Set the Thread Child Timeout used when operating in the Child role. More... | |
| OTAPI const otExtendedPanId *OTCALL | otThreadGetExtendedPanId (otInstance *aInstance) |
| Get the IEEE 802.15.4 Extended PAN ID. More... | |
| OTAPI otError OTCALL | otThreadSetExtendedPanId (otInstance *aInstance, const otExtendedPanId *aExtendedPanId) |
| Set the IEEE 802.15.4 Extended PAN ID. More... | |
| OTAPI otError OTCALL | otThreadGetLeaderRloc (otInstance *aInstance, otIp6Address *aLeaderRloc) |
| This function returns a pointer to the Leader's RLOC. More... | |
| OTAPI otLinkModeConfig OTCALL | otThreadGetLinkMode (otInstance *aInstance) |
| Get the MLE Link Mode configuration. More... | |
| OTAPI otError OTCALL | otThreadSetLinkMode (otInstance *aInstance, otLinkModeConfig aConfig) |
| Set the MLE Link Mode configuration. More... | |
| OTAPI const otMasterKey *OTCALL | otThreadGetMasterKey (otInstance *aInstance) |
| Get the thrMasterKey. More... | |
| OTAPI otError OTCALL | otThreadSetMasterKey (otInstance *aInstance, const otMasterKey *aKey) |
| Set the thrMasterKey. More... | |
| OTAPI const otIp6Address *OTCALL | otThreadGetMeshLocalEid (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local EID. More... | |
| OTAPI const otMeshLocalPrefix *OTCALL | otThreadGetMeshLocalPrefix (otInstance *aInstance) |
| This function returns a pointer to the Mesh Local Prefix. More... | |
| OTAPI otError OTCALL | otThreadSetMeshLocalPrefix (otInstance *aInstance, const otMeshLocalPrefix *aMeshLocalPrefix) |
| This function sets the Mesh Local Prefix. More... | |
| const otIp6Address * | otThreadGetLinkLocalIp6Address (otInstance *aInstance) |
| This function returns the Thread link-local IPv6 address. More... | |
| OTAPI const char *OTCALL | otThreadGetNetworkName (otInstance *aInstance) |
| Get the Thread Network Name. More... | |
| OTAPI otError OTCALL | otThreadSetNetworkName (otInstance *aInstance, const char *aNetworkName) |
| Set the Thread Network Name. More... | |
| OTAPI uint32_t OTCALL | otThreadGetKeySequenceCounter (otInstance *aInstance) |
| Get the thrKeySequenceCounter. More... | |
| OTAPI void OTCALL | otThreadSetKeySequenceCounter (otInstance *aInstance, uint32_t aKeySequenceCounter) |
| Set the thrKeySequenceCounter. More... | |
| OTAPI uint32_t OTCALL | otThreadGetKeySwitchGuardTime (otInstance *aInstance) |
| Get the thrKeySwitchGuardTime. More... | |
| OTAPI void OTCALL | otThreadSetKeySwitchGuardTime (otInstance *aInstance, uint32_t aKeySwitchGuardTime) |
| Set the thrKeySwitchGuardTime. More... | |
| OTAPI otError OTCALL | otThreadBecomeDetached (otInstance *aInstance) |
| Detach from the Thread network. More... | |
| OTAPI otError OTCALL | otThreadBecomeChild (otInstance *aInstance) |
| Attempt to reattach as a child. More... | |
| OTAPI otError OTCALL | otThreadGetNextNeighborInfo (otInstance *aInstance, otNeighborInfoIterator *aIterator, otNeighborInfo *aInfo) |
| This function gets the next neighbor information. More... | |
| OTAPI otDeviceRole OTCALL | otThreadGetDeviceRole (otInstance *aInstance) |
| Get the device role. More... | |
| OTAPI otError OTCALL | otThreadGetLeaderData (otInstance *aInstance, otLeaderData *aLeaderData) |
| This function get the Thread Leader Data. More... | |
| OTAPI uint8_t OTCALL | otThreadGetLeaderRouterId (otInstance *aInstance) |
| Get the Leader's Router ID. More... | |
| OTAPI uint8_t OTCALL | otThreadGetLeaderWeight (otInstance *aInstance) |
| Get the Leader's Weight. More... | |
| OTAPI uint32_t OTCALL | otThreadGetPartitionId (otInstance *aInstance) |
| Get the Partition ID. More... | |
| OTAPI uint16_t OTCALL | otThreadGetRloc16 (otInstance *aInstance) |
| Get the RLOC16. More... | |
| OTAPI otError OTCALL | otThreadGetParentInfo (otInstance *aInstance, otRouterInfo *aParentInfo) |
| The function retrieves diagnostic information for a Thread Router as parent. More... | |
| OTAPI otError OTCALL | otThreadGetParentAverageRssi (otInstance *aInstance, int8_t *aParentRssi) |
| The function retrieves the average RSSI for the Thread Parent. More... | |
| OTAPI otError OTCALL | otThreadGetParentLastRssi (otInstance *aInstance, int8_t *aLastRssi) |
| The function retrieves the RSSI of the last packet from the Thread Parent. More... | |
| void | otThreadSetReceiveDiagnosticGetCallback (otInstance *aInstance, otReceiveDiagnosticGetCallback aCallback, void *aCallbackContext) |
| This function registers a callback to provide received raw Network Diagnostic Get response payload. More... | |
| OTAPI otError OTCALL | otThreadSendDiagnosticGet (otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount) |
| Send a Network Diagnostic Get request. More... | |
| OTAPI otError OTCALL | otThreadSendDiagnosticReset (otInstance *aInstance, const otIp6Address *aDestination, const uint8_t aTlvTypes[], uint8_t aCount) |
| Send a Network Diagnostic Reset request. More... | |
| OTAPI const otIpCounters *OTCALL | otThreadGetIp6Counters (otInstance *aInstance) |
| Get the IPv6 counters. More... | |
| OTAPI const otMleCounters *OTCALL | otThreadGetMleCounters (otInstance *aInstance) |
| Get the Thread MLE counters. More... | |
| void | otThreadResetMleCounters (otInstance *aInstance) |
| Reset the Thread MLE counters. More... | |
| OTAPI otError OTCALL | otThreadRegisterParentResponseCallback (otInstance *aInstance, otThreadParentResponseCallback aCallback, void *aContext) |
| This function registers a callback to receive MLE Parent Response data. More... | |
Variables | |
| OT_TOOL_PACKED_BEGIN struct otMasterKey | OT_TOOL_PACKED_END |
This module includes functions for all Thread roles.
| typedef struct otOperationalDataset otOperationalDataset |
This structure represents an Active or Pending Operational Dataset.
Components in Dataset are optional. mComponets structure specifies which components are present in the Dataset.
| typedef void(* otReceiveDiagnosticGetCallback) (otMessage *aMessage, const otMessageInfo *aMessageInfo, void *aContext) |
This function pointer is called when Network Diagnostic Get response is received.
| [in] | aMessage | A pointer to the message buffer containing the received Network Diagnostic Get response payload. |
| [in] | aMessageInfo | A pointer to the message info for aMessage. |
| [in] | aContext | A pointer to application-specific context. |
| typedef void(OTCALL * otThreadParentResponseCallback) (otThreadParentResponseInfo *aInfo, void *aContext) |
This function pointer is called every time an MLE Parent Response message is received.
| [in] | aStats | pointer to a location on stack holding the stats data. |
| [in] | aContext | A pointer to callback client-specific context. |
| anonymous enum |
This enumeration defines the Security Policy TLV flags.
| enum otDeviceRole |
Represents a Thread device role.
| enum otMeshcopTlvType |
This enumeration represents meshcop TLV types.
| enum otRoutePreference |
Defines valid values for member mPreference in otExternalRouteConfig and otBorderRouterConfig.
| Enumerator | |
|---|---|
| OT_ROUTE_PREFERENCE_LOW | Low route preference. |
| OT_ROUTE_PREFERENCE_MED | Medium route preference. |
| OT_ROUTE_PREFERENCE_HIGH | High route preference. |
| OTAPI otError OTCALL otDatasetGetActive | ( | otInstance * | aInstance, |
| otOperationalDataset * | aDataset | ||
| ) |
This function gets the Active Operational Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aDataset | A pointer to where the Active Operational Dataset will be placed. |
| OT_ERROR_NONE | Successfully retrieved the Active Operational Dataset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI uint32_t OTCALL otDatasetGetDelayTimerMinimal | ( | otInstance * | aInstance | ) |
Get minimal delay timer.
| [in] | aInstance | A pointer to an OpenThread instance. |
| the | value of minimal delay timer (in ms). |
| OTAPI otError OTCALL otDatasetGetPending | ( | otInstance * | aInstance, |
| otOperationalDataset * | aDataset | ||
| ) |
This function gets the Pending Operational Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aDataset | A pointer to where the Pending Operational Dataset will be placed. |
| OT_ERROR_NONE | Successfully retrieved the Pending Operational Dataset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI bool OTCALL otDatasetIsCommissioned | ( | otInstance * | aInstance | ) |
This function indicates whether a valid network is present in the Active Operational Dataset or not.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otDatasetSendMgmtActiveGet | ( | otInstance * | aInstance, |
| const otOperationalDatasetComponents * | aDatasetComponents, | ||
| const uint8_t * | aTlvTypes, | ||
| uint8_t | aLength, | ||
| const otIp6Address * | aAddress | ||
| ) |
This function sends MGMT_ACTIVE_GET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDatasetComponents | A pointer to a Dataset Components structure specifying which components to request. |
| [in] | aTlvTypes | A pointer to array containing additional raw TLV types to be requested. |
| [in] | aLength | The length of aTlvTypes. |
| [in] | aAddress | A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSendMgmtActiveSet | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset, | ||
| const uint8_t * | aTlvs, | ||
| uint8_t | aLength | ||
| ) |
This function sends MGMT_ACTIVE_SET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to operational dataset. |
| [in] | aTlvs | A pointer to TLVs. |
| [in] | aLength | The length of TLVs. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSendMgmtPendingGet | ( | otInstance * | aInstance, |
| const otOperationalDatasetComponents * | aDatasetComponents, | ||
| const uint8_t * | aTlvTypes, | ||
| uint8_t | aLength, | ||
| const otIp6Address * | aAddress | ||
| ) |
This function sends MGMT_PENDING_GET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDatasetComponents | A pointer to a Dataset Components structure specifying which components to request. |
| [in] | aTlvTypes | A pointer to array containing additional raw TLV types to be requested. |
| [in] | aLength | The length of aTlvTypes. |
| [in] | aAddress | A pointer to the IPv6 destination, if it is NULL, will use Leader ALOC as default. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSendMgmtPendingSet | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset, | ||
| const uint8_t * | aTlvs, | ||
| uint8_t | aLength | ||
| ) |
This function sends MGMT_PENDING_SET.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to operational dataset. |
| [in] | aTlvs | A pointer to TLVs. |
| [in] | aLength | The length of TLVs. |
| OT_ERROR_NONE | Successfully send the meshcop dataset command. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to send. |
| OTAPI otError OTCALL otDatasetSetActive | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset | ||
| ) |
This function sets the Active Operational Dataset.
If the dataset does not include an Active Timestamp, the dataset is only partially complete.
If Thread is enabled on a device that has a partially complete Active Dataset, the device will attempt to attach to an existing Thread network using any existing information in the dataset. The minimum set of information needed to attach is the PAN ID and Thread Master Key.
If channel is not included in the dataset, the device will send MLE Announce messages across different channels to find neighbors on other channels.
If the device successfully attaches to a Thread network, the device will then retrieve the full Active Dataset from its Parent. Note that a router-capable device will not transition to the Router or Leader roles until it has a complete Active Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to the Active Operational Dataset. |
| OT_ERROR_NONE | Successfully set the Active Operational Dataset. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to set the Active Operational Dataset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI otError OTCALL otDatasetSetDelayTimerMinimal | ( | otInstance * | aInstance, |
| uint32_t | aDelayTimerMinimal | ||
| ) |
Set minimal delay timer.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDelayTimerMinimal | The value of minimal delay timer (in ms). |
| OT_ERROR_NONE | Successfully set minimal delay timer. |
| OT_ERROR_INVALID_ARGS | If aDelayTimerMinimal is not valid. |
| OTAPI otError OTCALL otDatasetSetPending | ( | otInstance * | aInstance, |
| const otOperationalDataset * | aDataset | ||
| ) |
This function sets the Pending Operational Dataset.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDataset | A pointer to the Pending Operational Dataset. |
| OT_ERROR_NONE | Successfully set the Pending Operational Dataset. |
| OT_ERROR_NO_BUFS | Insufficient buffer space to set the Pending Operational Dataset. |
| OT_ERROR_INVALID_ARGS | aDataset was NULL. |
| OTAPI otError OTCALL otNetDataGet | ( | otInstance * | aInstance, |
| bool | aStable, | ||
| uint8_t * | aData, | ||
| uint8_t * | aDataLength | ||
| ) |
This method provides a full or stable copy of the Leader's Thread Network Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aStable | TRUE when copying the stable version, FALSE when copying the full version. |
| [out] | aData | A pointer to the data buffer. |
| [in,out] | aDataLength | On entry, size of the data buffer pointed to by aData. On exit, number of copied bytes. |
| OTAPI otError OTCALL otNetDataGetNextOnMeshPrefix | ( | otInstance * | aInstance, |
| otNetworkDataIterator * | aIterator, | ||
| otBorderRouterConfig * | aConfig | ||
| ) |
This function gets the next On Mesh Prefix in the partition's Network Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the Network Data iterator context. To get the first on-mesh entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| [out] | aConfig | A pointer to where the On Mesh Prefix information will be placed. |
| OT_ERROR_NONE | Successfully found the next On Mesh prefix. |
| OT_ERROR_NOT_FOUND | No subsequent On Mesh prefix exists in the Thread Network Data. |
| otError otNetDataGetNextRoute | ( | otInstance * | aInstance, |
| otNetworkDataIterator * | aIterator, | ||
| otExternalRouteConfig * | aConfig | ||
| ) |
This function gets the next external route in the partition's Network Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the Network Data iterator context. To get the first external route entry it should be set to OT_NETWORK_DATA_ITERATOR_INIT. |
| [out] | aConfig | A pointer to where the External Route information will be placed. |
| OT_ERROR_NONE | Successfully found the next External Route. |
| OT_ERROR_NOT_FOUND | No subsequent external route entry exists in the Thread Network Data. |
| OTAPI uint8_t OTCALL otNetDataGetStableVersion | ( | otInstance * | aInstance | ) |
Get the Stable Network Data Version.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint8_t OTCALL otNetDataGetVersion | ( | otInstance * | aInstance | ) |
Get the Network Data Version.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otThreadBecomeChild | ( | otInstance * | aInstance | ) |
Attempt to reattach as a child.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OT_ERROR_NONE | Successfully begin attempt to become a child. |
| OT_ERROR_INVALID_STATE | Thread is disabled. |
| OTAPI otError OTCALL otThreadBecomeDetached | ( | otInstance * | aInstance | ) |
Detach from the Thread network.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OT_ERROR_NONE | Successfully detached from the Thread network. |
| OT_ERROR_INVALID_STATE | Thread is disabled. |
| OTAPI otError OTCALL otThreadDiscover | ( | otInstance * | aInstance, |
| uint32_t | aScanChannels, | ||
| uint16_t | aPanId, | ||
| bool | aJoiner, | ||
| bool | aEnableEui64Filtering, | ||
| otHandleActiveScanResult | aCallback, | ||
| void * | aCallbackContext | ||
| ) |
This function starts a Thread Discovery scan.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aScanChannels | A bit vector indicating which channels to scan (e.g. OT_CHANNEL_11_MASK). |
| [in] | aPanId | The PAN ID filter (set to Broadcast PAN to disable filter). |
| [in] | aJoiner | Value of the Joiner Flag in the Discovery Request TLV. |
| [in] | aEnableEui64Filtering | TRUE to filter responses on EUI-64, FALSE otherwise. |
| [in] | aCallback | A pointer to a function called on receiving an MLE Discovery Response or scan completes. |
| [in] | aCallbackContext | A pointer to application-specific context. |
| OT_ERROR_NONE | Accepted the Thread Discovery request. |
| OT_ERROR_BUSY | Already performing an Thread Discovery. |
| OTAPI bool OTCALL otThreadGetAutoStart | ( | otInstance * | aInstance | ) |
This function queries if the Thread stack is configured to automatically start on reinitialization.
| [in] | aInstance | A pointer to an OpenThread instance. |
| TRUE | It is configured to automatically start. |
| FALSE | It is not configured to automatically start. |
| OTAPI uint32_t OTCALL otThreadGetChildTimeout | ( | otInstance * | aInstance | ) |
Get the Thread Child Timeout used when operating in the Child role.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otDeviceRole OTCALL otThreadGetDeviceRole | ( | otInstance * | aInstance | ) |
Get the device role.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OT_DEVICE_ROLE_DISABLED | The Thread stack is disabled. |
| OT_DEVICE_ROLE_DETACHED | The device is not currently participating in a Thread network/partition. |
| OT_DEVICE_ROLE_CHILD | The device is currently operating as a Thread Child. |
| OT_DEVICE_ROLE_ROUTER | The device is currently operating as a Thread Router. |
| OT_DEVICE_ROLE_LEADER | The device is currently operating as a Thread Leader. |
| OTAPI const otExtendedPanId* OTCALL otThreadGetExtendedPanId | ( | otInstance * | aInstance | ) |
Get the IEEE 802.15.4 Extended PAN ID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otIpCounters* OTCALL otThreadGetIp6Counters | ( | otInstance * | aInstance | ) |
Get the IPv6 counters.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint32_t OTCALL otThreadGetKeySequenceCounter | ( | otInstance * | aInstance | ) |
Get the thrKeySequenceCounter.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint32_t OTCALL otThreadGetKeySwitchGuardTime | ( | otInstance * | aInstance | ) |
Get the thrKeySwitchGuardTime.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otThreadGetLeaderData | ( | otInstance * | aInstance, |
| otLeaderData * | aLeaderData | ||
| ) |
This function get the Thread Leader Data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aLeaderData | A pointer to where the leader data is placed. |
| OT_ERROR_NONE | Successfully retrieved the leader data. |
| OT_ERROR_DETACHED | Not currently attached. |
| OT_ERROR_INVALID_ARGS | aLeaderData is NULL. |
| OTAPI otError OTCALL otThreadGetLeaderRloc | ( | otInstance * | aInstance, |
| otIp6Address * | aLeaderRloc | ||
| ) |
This function returns a pointer to the Leader's RLOC.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aLeaderRloc | A pointer to the Leader's RLOC. |
| OT_ERROR_NONE | The Leader's RLOC was successfully written to aLeaderRloc. |
| OT_ERROR_INVALID_ARGS | aLeaderRloc was NULL. |
| OT_ERROR_DETACHED | Not currently attached to a Thread Partition. |
| OTAPI uint8_t OTCALL otThreadGetLeaderRouterId | ( | otInstance * | aInstance | ) |
Get the Leader's Router ID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint8_t OTCALL otThreadGetLeaderWeight | ( | otInstance * | aInstance | ) |
Get the Leader's Weight.
| [in] | aInstance | A pointer to an OpenThread instance. |
| const otIp6Address* otThreadGetLinkLocalIp6Address | ( | otInstance * | aInstance | ) |
This function returns the Thread link-local IPv6 address.
The Thread link local address is derived using IEEE802.15.4 Extended Address as Interface Identifier.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otLinkModeConfig OTCALL otThreadGetLinkMode | ( | otInstance * | aInstance | ) |
Get the MLE Link Mode configuration.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otMasterKey* OTCALL otThreadGetMasterKey | ( | otInstance * | aInstance | ) |
Get the thrMasterKey.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otIp6Address* OTCALL otThreadGetMeshLocalEid | ( | otInstance * | aInstance | ) |
This function returns a pointer to the Mesh Local EID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otMeshLocalPrefix* OTCALL otThreadGetMeshLocalPrefix | ( | otInstance * | aInstance | ) |
This function returns a pointer to the Mesh Local Prefix.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const otMleCounters* OTCALL otThreadGetMleCounters | ( | otInstance * | aInstance | ) |
Get the Thread MLE counters.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI const char* OTCALL otThreadGetNetworkName | ( | otInstance * | aInstance | ) |
Get the Thread Network Name.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otThreadGetNextNeighborInfo | ( | otInstance * | aInstance, |
| otNeighborInfoIterator * | aIterator, | ||
| otNeighborInfo * | aInfo | ||
| ) |
This function gets the next neighbor information.
It is used to go through the entries of the neighbor table.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in,out] | aIterator | A pointer to the iterator context. To get the first neighbor entry it should be set to OT_NEIGHBOR_INFO_ITERATOR_INIT. |
| [out] | aInfo | A pointer to the neighbor information. |
| OT_ERROR_NONE | Successfully found the next neighbor entry in table. |
| OT_ERROR_NOT_FOUND | No subsequent neighbor entry exists in the table. |
| OT_ERROR_INVALID_ARGS | aIterator or aInfo was NULL. |
| OTAPI otError OTCALL otThreadGetParentAverageRssi | ( | otInstance * | aInstance, |
| int8_t * | aParentRssi | ||
| ) |
The function retrieves the average RSSI for the Thread Parent.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aParentRssi | A pointer to where the parent RSSI should be placed. |
| OTAPI otError OTCALL otThreadGetParentInfo | ( | otInstance * | aInstance, |
| otRouterInfo * | aParentInfo | ||
| ) |
The function retrieves diagnostic information for a Thread Router as parent.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aParentInfo | A pointer to where the parent router information is placed. |
| OTAPI otError OTCALL otThreadGetParentLastRssi | ( | otInstance * | aInstance, |
| int8_t * | aLastRssi | ||
| ) |
The function retrieves the RSSI of the last packet from the Thread Parent.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [out] | aLastRssi | A pointer to where the last RSSI should be placed. |
| OT_ERROR_NONE | Successfully retrieved the RSSI data. |
| OT_ERROR_FAILED | Unable to get RSSI data. |
| OT_ERROR_INVALID_ARGS | aLastRssi is NULL. |
| OTAPI uint32_t OTCALL otThreadGetPartitionId | ( | otInstance * | aInstance | ) |
Get the Partition ID.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI uint16_t OTCALL otThreadGetRloc16 | ( | otInstance * | aInstance | ) |
Get the RLOC16.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI bool OTCALL otThreadIsDiscoverInProgress | ( | otInstance * | aInstance | ) |
This function determines if an MLE Thread Discovery is currently in progress.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI bool OTCALL otThreadIsSingleton | ( | otInstance * | aInstance | ) |
This function indicates whether a node is the only router on the network.
| [in] | aInstance | A pointer to an OpenThread instance. |
| TRUE | It is the only router in the network. |
| FALSE | It is a child or is not a single router in the network. |
| OTAPI otError OTCALL otThreadRegisterParentResponseCallback | ( | otInstance * | aInstance, |
| otThreadParentResponseCallback | aCallback, | ||
| void * | aContext | ||
| ) |
This function registers a callback to receive MLE Parent Response data.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aCallback | A pointer to a function that is called upon receiving an MLE Parent Response message. |
| [in] | aContext | A pointer to callback client-specific context. |
| OT_ERROR_NONE | On successful registration |
| OT_ERROR_DISABLED_FEATURE | If the feature is not supported |
| void otThreadResetMleCounters | ( | otInstance * | aInstance | ) |
Reset the Thread MLE counters.
| [in] | aInstance | A pointer to an OpenThread instance. |
| OTAPI otError OTCALL otThreadSendDiagnosticGet | ( | otInstance * | aInstance, |
| const otIp6Address * | aDestination, | ||
| const uint8_t | aTlvTypes[], | ||
| uint8_t | aCount | ||
| ) |
Send a Network Diagnostic Get request.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDestination | A pointer to destination address. |
| [in] | aTlvTypes | An array of Network Diagnostic TLV types. |
| [in] | aCount | Number of types in aTlvTypes |
| OTAPI otError OTCALL otThreadSendDiagnosticReset | ( | otInstance * | aInstance, |
| const otIp6Address * | aDestination, | ||
| const uint8_t | aTlvTypes[], | ||
| uint8_t | aCount | ||
| ) |
Send a Network Diagnostic Reset request.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aDestination | A pointer to destination address. |
| [in] | aTlvTypes | An array of Network Diagnostic TLV types. Currently only Type 9 is allowed. |
| [in] | aCount | Number of types in aTlvTypes |
| OTAPI otError OTCALL otThreadSetAutoStart | ( | otInstance * | aInstance, |
| bool | aStartAutomatically | ||
| ) |
This function configures the Thread stack to automatically start on reinitialization.
It has no effect on the current Thread state.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aStartAutomatically | TRUE to automatically start; FALSE to not automatically start. |
| OTAPI void OTCALL otThreadSetChildTimeout | ( | otInstance * | aInstance, |
| uint32_t | aTimeout | ||
| ) |
Set the Thread Child Timeout used when operating in the Child role.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aTimeout | The timeout value in seconds. |
| OTAPI otError OTCALL otThreadSetEnabled | ( | otInstance * | aInstance, |
| bool | aEnabled | ||
| ) |
This function starts Thread protocol operation.
The interface must be up when calling this function.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aEnabled | TRUE if Thread is enabled, FALSE otherwise. |
| OT_ERROR_NONE | Successfully started Thread protocol operation. |
| OT_ERROR_INVALID_STATE | The network interface was not not up. |
| OTAPI otError OTCALL otThreadSetExtendedPanId | ( | otInstance * | aInstance, |
| const otExtendedPanId * | aExtendedPanId | ||
| ) |
Set the IEEE 802.15.4 Extended PAN ID.
This function can only be called while Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aExtendedPanId | A pointer to the IEEE 802.15.4 Extended PAN ID. |
| OT_ERROR_NONE | Successfully set the Extended PAN ID. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| OTAPI void OTCALL otThreadSetKeySequenceCounter | ( | otInstance * | aInstance, |
| uint32_t | aKeySequenceCounter | ||
| ) |
Set the thrKeySequenceCounter.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aKeySequenceCounter | The thrKeySequenceCounter value. |
| OTAPI void OTCALL otThreadSetKeySwitchGuardTime | ( | otInstance * | aInstance, |
| uint32_t | aKeySwitchGuardTime | ||
| ) |
Set the thrKeySwitchGuardTime.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aKeySwitchGuardTime | The thrKeySwitchGuardTime value (in hours). |
| OTAPI otError OTCALL otThreadSetLinkMode | ( | otInstance * | aInstance, |
| otLinkModeConfig | aConfig | ||
| ) |
Set the MLE Link Mode configuration.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aConfig | A pointer to the Link Mode configuration. |
| OT_ERROR_NONE | Successfully set the MLE Link Mode configuration. |
| OTAPI otError OTCALL otThreadSetMasterKey | ( | otInstance * | aInstance, |
| const otMasterKey * | aKey | ||
| ) |
Set the thrMasterKey.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aKey | A pointer to a buffer containing the thrMasterKey. |
| OT_ERROR_NONE | Successfully set the thrMasterKey. |
| OT_ERROR_INVALID_ARGS | If aKeyLength is larger than 16. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| OTAPI otError OTCALL otThreadSetMeshLocalPrefix | ( | otInstance * | aInstance, |
| const otMeshLocalPrefix * | aMeshLocalPrefix | ||
| ) |
This function sets the Mesh Local Prefix.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aMeshLocalPrefix | A pointer to the Mesh Local Prefix. |
| OT_ERROR_NONE | Successfully set the Mesh Local Prefix. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| OTAPI otError OTCALL otThreadSetNetworkName | ( | otInstance * | aInstance, |
| const char * | aNetworkName | ||
| ) |
Set the Thread Network Name.
This function succeeds only when Thread protocols are disabled. A successful call to this function invalidates the Active and Pending Operational Datasets in non-volatile memory.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aNetworkName | A pointer to the Thread Network Name. |
| OT_ERROR_NONE | Successfully set the Thread Network Name. |
| OT_ERROR_INVALID_STATE | Thread protocols are enabled. |
| void otThreadSetReceiveDiagnosticGetCallback | ( | otInstance * | aInstance, |
| otReceiveDiagnosticGetCallback | aCallback, | ||
| void * | aCallbackContext | ||
| ) |
This function registers a callback to provide received raw Network Diagnostic Get response payload.
| [in] | aInstance | A pointer to an OpenThread instance. |
| [in] | aCallback | A pointer to a function that is called when Network Diagnostic Get response is received or NULL to disable the callback. |
| [in] | aCallbackContext | A pointer to application-specific context. |