#include <stdbool.h>
#include <stdint.h>
#include "../inc/hw_types.h"
#include "../inc/hw_memmap.h"
#include "../inc/hw_rfc_pwr.h"
#include "../inc/hw_rfc_dbell.h"
#include "../inc/hw_fcfg1.h"
#include "../inc/hw_adi_3_refsys.h"
#include "../inc/hw_adi.h"
#include "rf_common_cmd.h"
#include "rf_prop_cmd.h"
#include "rf_ble_cmd.h"
Data Structures | |
struct | rfTrim_t |
Macros | |
#define | RFC_MAX_SEARCH_DEPTH 5 |
#define | RFC_PA_TYPE_ADDRESS 0x21000385 |
#define | RFC_PA_TYPE_MASK 0x04 |
#define | RFC_PA_GAIN_ADDRESS 0x21000398 |
#define | RFC_PA_GAIN_MASK 0x003FFFFF |
#define | RFC_FE_MODE_ESCAPE_VALUE 0xFF |
#define | RFC_FE_OVERRIDE_ADDRESS 0x0703 |
#define | RFC_FE_OVERRIDE_MASK 0x0000FFFF |
Functions | |
static void | RFCClockEnable (void) |
Enable the RF core clocks. More... | |
static void | RFCClockDisable (void) |
Disable the RF core clocks. More... | |
static void | RFCCpeIntClear (uint32_t ui32Mask) |
Clear HW interrupt flags. More... | |
static void | RFCHwIntClear (uint32_t ui32Mask) |
Clear CPE interrupt flags. More... | |
static void | RFCCpe0IntSelect (uint32_t ui32Mask) |
Select interrupt sources to CPE0 (assign to INT_RFC_CPE_0 interrupt vector). More... | |
static void | RFCCpe1IntSelect (uint32_t ui32Mask) |
Select interrupt sources to CPE1 (assign to INT_RFC_CPE_1 interrupt vector). More... | |
static void | RFCCpeIntEnable (uint32_t ui32Mask) |
Enable CPEx interrupt sources. More... | |
static void | RFCCpe0IntSelectClearEnable (uint32_t ui32Mask) |
Select, clear, and enable interrupt sources to CPE0. More... | |
static void | RFCCpe1IntSelectClearEnable (uint32_t ui32Mask) |
Select, clear, and enable interrupt sources to CPE1. More... | |
static void | RFCHwIntEnable (uint32_t ui32Mask) |
Enable HW interrupt sources. More... | |
static void | RFCCpeIntDisable (uint32_t ui32Mask) |
Disable CPE interrupt sources. More... | |
static void | RFCHwIntDisable (uint32_t ui32Mask) |
Disable HW interrupt sources. More... | |
uint32_t | RFCCpeIntGetAndClear (uint32_t ui32Mask) |
Get and clear CPE interrupt flags. More... | |
static void | RFCAckIntClear (void) |
Clear ACK interrupt flag. More... | |
uint32_t | RFCDoorbellSendTo (uint32_t pOp) |
Send a radio operation to the doorbell and wait for an acknowledgment. More... | |
void | RFCSynthPowerDown (void) |
This function implements a fast way to turn off the synthesizer. More... | |
void | RFCCpePatchReset (void) |
Reset previously patched CPE RAM to a state where it can be patched again. More... | |
uint8_t | RFCOverrideSearch (const uint32_t *pOverride, const uint32_t pattern, const uint32_t mask, const uint8_t searchDepth) |
uint8_t | RFCOverrideUpdate (rfc_radioOp_t *pOpSetup, uint32_t *pParams) |
Function to update override list. More... | |
uint32_t | RFCHwIntGetAndClear (uint32_t ui32Mask) |
Get and clear HW interrupt flags. More... | |
static bool | RFCGetPaType (void) |
Get the type of currently selected PA. More... | |
static uint32_t | RFCGetPaGain (void) |
Get the gain of currently selected PA. More... | |
uint32_t | RFCAnaDivTxOverride (uint8_t loDivider, uint8_t frontEndMode) |
Function to calculate the proper override run-time for the High Gain PA. More... | |