![]() |
![]() |
TI BLE5-Stack API Documentation
2.00.04.00
|
ToF Security Handle. More...
Data Fields | |
CryptoKey | cryptoKey |
AES Encryption Crypto key. | |
ctrDrbgState_t | ctrDrbgState |
ctr DRBG State | |
AESECB_Handle | encHandleECB |
AESECB Encryption Handle. | |
uint8_t | enckey [ENC_KEY_LEN] |
AESECB Encryption key. | |
AESECB_Params | encParamsECB |
AESECB Encryption parameters. | |
uint16_t | numOfSyncWordsPerBuffer |
Length of double buffer, both buffers must be equal length. The number of bursts in double buffer mode is still numBurstSamples. | |
AESECB_Operation | operationECB |
AESECB Encryption operation parameters. | |
uint8_t * | pSyncWordBuffer1 |
Pointer to the sync word buffer, used in both single and double buffer mode. | |
uint8_t * | pSyncWordBuffer2 |
Pointer to the second sync word buffer, used in double buffer mode only. | |
uint8_t | seed [CTR_DRBG_SEEDLEN] |
ctr DRBG Seed | |
tofSecCfgPrms_t | tofSecCfgParams |
ToF Security Configuration Parameters. | |
TRNG_Handle | trngHandle |
TRNG Handle. | |
ToF Security Handle.