![]() |
![]() |
TI BLE5-Stack API Documentation
2.00.04.00
|
RTLS Control module interface.
This file contains the functions and structures specific to AoA.
Go to the source code of this file.
Macros | |
#define | HAL_ASSERT_CAUSE_OUT_OF_MEMORY 0x04 |
RTLS Assert Error code. | |
#define | RTLS_CMD_AOA_ENABLE 0x14 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_ANGLE 0x23 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_PAIR_ANGLES 0x25 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_RESULT_RAW 0x24 |
RTLS Node Manager command. | |
#define | RTLS_CMD_AOA_SET_PARAMS 0x13 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONN_PARAMS 0x02 |
RTLS Node Manager command. | |
#define | RTLS_CMD_CONNECT 0x03 |
RTLS Node Manager command. | |
#define | RTLS_CMD_IDENTIFY 0x00 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESERVED 0x01 |
RTLS Node Manager command. | |
#define | RTLS_CMD_RESET_DEVICE 0x20 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SCAN 0x04 |
RTLS Node Manager command. | |
#define | RTLS_CMD_SCAN_STOP 0x05 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TERMINATE_LINK 0x22 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_CALIBRATE 0x26 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_ENABLE 0x12 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_GET_SEC_SEED 0x10 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_RESULT_DIST 0x06 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_RESULT_RAW 0x08 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_RESULT_STAT 0x07 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_SET_PARAMS 0x11 |
RTLS Node Manager command. | |
#define | RTLS_CMD_TOF_SET_SEC_SEED 0x09 |
RTLS Node Manager command. | |
#define | RTLS_CTRL_ALL_EVENTS (RTLS_QUEUE_EVT) |
RTLS Task configuration. | |
#define | RTLS_CTRL_TASK_PRIORITY 2 |
RTLS Task configuration variable. | |
#define | RTLS_CTRL_TASK_STACK_SIZE 752 |
RTLS Task configuration variable. | |
#define | RTLS_EVT_ASSERT 0x80 |
RTLS async event. | |
#define | RTLS_EVT_DEBUG 0x82 |
RTLS async event. | |
#define | RTLS_EVT_ERROR 0x81 |
RTLS async event. | |
#define | RTLS_QUEUE_EVT UTIL_QUEUE_EVENT_ID |
Event_Id_30. | |
#define | RTLSUTIL_FREE(pFree) |
RTLSUTIL_FREE memory free without icall. More... | |
#define | RTLSUTIL_MALLOC(pAlloc, size) |
RTLSUTIL_MALLOC memory allocation without icall. More... | |
Functions | |
void * | RTLSCtrl_malloc (uint32_t sz) |
This function will allocate memory, if we were unable to allocate we will report to RTLS Host. More... | |