![]() |
![]() |
TI BLE5-Stack API Documentation
2.00.04.00
|
Macros | |
#define | OAD_DL_COMPLETE_EVT Event_Id_02 |
#define | OAD_OUT_OF_MEM_EVT Event_Id_03 |
#define | OAD_QUEUE_EVT Event_Id_01 |
#define OAD_DL_COMPLETE_EVT Event_Id_02 |
The download complete signifies that the OAD has completed and the candidate image has passed verification. When this event is received, the application should reset the device so that the BIM can perform further processing.
#define OAD_OUT_OF_MEM_EVT Event_Id_03 |
The out of memory event signifies that the OAD has run out of memory and could not allocate memory for a message to notify the application (for example in the case of a timeout).
#define OAD_QUEUE_EVT Event_Id_01 |
The queue event is posted whenever there is a new message in the OAD message queue from the BLE-Stack. Messages in the OAD queue must be processed in the applicatino context