|
Z-Stack API Reference
3.3.1
|
Data Structures | |
| struct | zclGeneral_Scene_extField_t |
| struct | zclGeneral_Scene_t |
| struct | zclIdentifyUpdateCommState_t |
| struct | zclGeneral_Alarm_t |
| struct | zclGetEventLog_t |
| struct | zclEventLogPayload_t |
| struct | zclPublishEventLog_t |
| struct | zclLocationAbsolute_t |
| struct | zclLocationDevCfg_t |
| struct | locationbits_t |
| union | location_t |
| struct | zclLocationGetData_t |
| struct | zclLocationDevCfgRsp_t |
| struct | zclLocationCalculated_t |
| struct | zclLocationData_t |
| struct | zclLocationDataRsp_t |
| struct | zclIdentify_t |
| struct | zclIdentifyQuery_t |
| struct | zclIdentifyTriggerEffect_t |
| struct | zclIdentifyQueryRsp_t |
| struct | zclOffWithEffect_t |
| struct | zclOnOffCtrlBits_t |
| union | zclOnOffCtrl_t |
| struct | zclOnWithTimedOff_t |
| struct | zclLCMoveToLevel_t |
| struct | zclLCMove_t |
| struct | zclLCStep_t |
| struct | zclGroupRsp_t |
| struct | zclSceneReq_t |
| struct | zclSceneRsp_t |
| struct | zclAlarm_t |
| struct | zclLocation_t |
| struct | zclLocationRsp_t |
| struct | zclGeneral_AppCallbacks_t |
Typedefs | |
| typedef void(* | zclGCB_BasicReset_t) (void) |
| typedef void(* | zclGCB_Identify_t) (zclIdentify_t *pCmd) |
| This callback is called to process an incoming Identify command. | |
| typedef void(* | zclGCB_IdentifyQuery_t) (zclIdentifyQuery_t *pCmd) |
| This callback is called to process an incoming Identify Query command. | |
| typedef void(* | zclGCB_IdentifyTriggerEffect_t) (zclIdentifyTriggerEffect_t *pCmd) |
| This callback is called to process an incoming Identify Trigger Effect command. | |
| typedef ZStatus_t(* | zclGCB_IdentifyUpdateCommState_t) (zclIdentifyUpdateCommState_t *pCmd) |
| This callback is called to process an incoming Identify Update Commission State command. | |
| typedef void(* | zclGCB_IdentifyQueryRsp_t) (zclIdentifyQueryRsp_t *pRsp) |
| This callback is called to process an incoming Identify Query Response command. | |
| typedef void(* | zclGCB_OnOff_t) (uint8 cmd) |
| This callback is called to process an incoming On, Off or Toggle command. | |
| typedef void(* | zclGCB_OnOff_OffWithEffect_t) (zclOffWithEffect_t *pCmd) |
| This callback is called to process an incoming Off with Effect. | |
| typedef void(* | zclGCB_OnOff_OnWithRecallGlobalScene_t) (void) |
| This callback is called to process an incoming On with Recall Global Scene command. | |
| typedef void(* | zclGCB_OnOff_OnWithTimedOff_t) (zclOnWithTimedOff_t *pCmd) |
| This callback is called to process an incoming On with Timed Off. | |
| typedef void(* | zclGCB_LevelControlMoveToLevel_t) (zclLCMoveToLevel_t *pCmd) |
| This callback is called to process a Level Control - Move to Level command. | |
| typedef void(* | zclGCB_LevelControlMove_t) (zclLCMove_t *pCmd) |
| This callback is called to process a Level Control - Move command. | |
| typedef void(* | zclGCB_LevelControlStep_t) (zclLCStep_t *pCmd) |
| This callback is called to process a Level Control - Step command. | |
| typedef void(* | zclGCB_LevelControlStop_t) (void) |
| This callback is called to process a Level Control - Stop command. | |
| typedef void(* | zclGCB_GroupRsp_t) (zclGroupRsp_t *pRsp) |
| typedef uint8(* | zclGCB_SceneStoreReq_t) (zclSceneReq_t *pReq) |
| typedef void(* | zclGCB_SceneRecallReq_t) (zclSceneReq_t *pReq) |
| typedef void(* | zclGCB_SceneRsp_t) (zclSceneRsp_t *pRsp) |
| typedef void(* | zclGCB_Alarm_t) (uint8 direction, zclAlarm_t *pAlarm) |
| This callback is called to process an incoming Alarm request or response command. | |
| typedef void(* | zclGCB_GetEventLog_t) (uint8 srcEP, afAddrType_t *srcAddr, zclGetEventLog_t *pEventLog, uint8 seqNum) |
| This callback is called to process an incoming Alarm Get Event Log command. | |
| typedef void(* | zclGCB_PublishEventLog_t) (afAddrType_t *srcAddr, zclPublishEventLog_t *pEventLog) |
| This callback is called to process an incoming Alarm Publish Event Log command. | |
| typedef void(* | zclGCB_Location_t) (zclLocation_t *pCmd) |
| This callback is called to to process an incoming RSSI Location command. | |
| typedef void(* | zclGCB_LocationRsp_t) (zclLocationRsp_t *pRsp) |
| typedef void(* zclGCB_BasicReset_t) (void) |
This callback is called to process an incoming Reset to Factory Defaults command. On receipt of this command, the device resets all the attributes of all its clusters to their factory defaults.
| typedef void(* zclGCB_GroupRsp_t) (zclGroupRsp_t *pRsp) |
This callback is called to process an received Group Response message. This means that this app sent the request message.
| typedef void(* zclGCB_LocationRsp_t) (zclLocationRsp_t *pRsp) |
This callback is called to process an incoming RSSI Location response command. This means that this app sent the request for this response.
| typedef void(* zclGCB_SceneRecallReq_t) (zclSceneReq_t *pReq) |
This callback is called to process an incoming Scene Recall request The app will use what's in the "extField" to restore to these settings.
| typedef void(* zclGCB_SceneRsp_t) (zclSceneRsp_t *pRsp) |
This callback is called to process an incoming Scene responses. This means that this app sent the request for this response.
| typedef uint8(* zclGCB_SceneStoreReq_t) (zclSceneReq_t *pReq) |
This callback is called to process an incoming Scene Store request. The app will fill in the "extField" with what is needed to restore its current settings. Before overwriting the content of the scene, App needs to verify if there was a change with the previous configuration. App function returns TRUE if there was a change, otherwise returns FALSE.