Data Fields
LCD_Command Struct Reference

Format of LCD commands used by the LCD controller. More...

#include <LCDDogm1286.h>

Data Fields

char displayStartLine
 
char adcSet
 
char outputMode
 
char displayType
 
char lcdBias
 
char powerControl
 
char boosterRadio0
 
char boosterRadio1
 
char contrastSet0
 
char contrastSet1
 
char contrastSet2
 
char staticIndicator0
 
char staticIndicator1
 
char displayEn
 
char setPage
 
char columnHi
 
char columnLo
 

Detailed Description

Format of LCD commands used by the LCD controller.

Field Documentation

§ displayStartLine

char LCD_Command::displayStartLine

§ adcSet

char LCD_Command::adcSet

§ outputMode

char LCD_Command::outputMode

§ displayType

char LCD_Command::displayType

§ lcdBias

char LCD_Command::lcdBias

§ powerControl

char LCD_Command::powerControl

§ boosterRadio0

char LCD_Command::boosterRadio0

§ boosterRadio1

char LCD_Command::boosterRadio1

§ contrastSet0

char LCD_Command::contrastSet0

§ contrastSet1

char LCD_Command::contrastSet1

§ contrastSet2

char LCD_Command::contrastSet2

§ staticIndicator0

char LCD_Command::staticIndicator0

§ staticIndicator1

char LCD_Command::staticIndicator1

§ displayEn

char LCD_Command::displayEn

§ setPage

char LCD_Command::setPage

§ columnHi

char LCD_Command::columnHi

§ columnLo

char LCD_Command::columnLo

The documentation for this struct was generated from the following file:
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale