![]() |
![]() |
CBC Parameters. More...
#include <AESCBC.h>
Data Fields | |
AESCBC_ReturnBehavior | returnBehavior |
AESCBC_CallbackFxn | callbackFxn |
uint32_t | timeout |
void * | custom |
CBC Parameters.
CBC Parameters are used to with the AESCBC_open() call. Default values for these parameters are set using AESCBC_Params_init().
AESCBC_ReturnBehavior AESCBC_Params::returnBehavior |
Blocking, callback, or polling return behavior
AESCBC_CallbackFxn AESCBC_Params::callbackFxn |
Callback function pointer
uint32_t AESCBC_Params::timeout |
Timeout before the driver returns an error in AESCBC_RETURN_BEHAVIOR_BLOCKING
void* AESCBC_Params::custom |
Custom argument used by driver implementation