Data Fields
DisplaySharp_HWAttrsV1 Struct Reference

#include <DisplaySharp.h>

Data Fields

uint32_t spiIndex
 
uint32_t csPin
 
uint32_t powerPin
 
uint32_t enablePin
 
uint16_t pixelHeight
 
uint16_t pixelWidth
 
void * displayBuf
 

Field Documentation

§ spiIndex

uint32_t DisplaySharp_HWAttrsV1::spiIndex

§ csPin

uint32_t DisplaySharp_HWAttrsV1::csPin

§ powerPin

uint32_t DisplaySharp_HWAttrsV1::powerPin

§ enablePin

uint32_t DisplaySharp_HWAttrsV1::enablePin

§ pixelHeight

uint16_t DisplaySharp_HWAttrsV1::pixelHeight

§ pixelWidth

uint16_t DisplaySharp_HWAttrsV1::pixelWidth

§ displayBuf

void* DisplaySharp_HWAttrsV1::displayBuf

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale