Data Fields
AESGCMCC26XX_Object Struct Reference

AESGCMCC26XX Object. More...

#include <AESGCMCC26XX.h>

Collaboration diagram for AESGCMCC26XX_Object:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
int_fast16_t returnStatus
 
AESGCM_ReturnBehavior returnBehavior
 
AESGCM_OperationType operationType
 
uint32_t semaphoreTimeout
 
AESGCM_CallbackFxn callbackFxn
 
AESGCM_Operationoperation
 

Detailed Description

AESGCMCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool AESGCMCC26XX_Object::isOpen

§ operationInProgress

bool AESGCMCC26XX_Object::operationInProgress

§ operationCanceled

bool AESGCMCC26XX_Object::operationCanceled

§ returnStatus

int_fast16_t AESGCMCC26XX_Object::returnStatus

§ returnBehavior

AESGCM_ReturnBehavior AESGCMCC26XX_Object::returnBehavior

§ operationType

AESGCM_OperationType AESGCMCC26XX_Object::operationType

§ semaphoreTimeout

uint32_t AESGCMCC26XX_Object::semaphoreTimeout

§ callbackFxn

AESGCM_CallbackFxn AESGCMCC26XX_Object::callbackFxn

§ operation

AESGCM_Operation* AESGCMCC26XX_Object::operation

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale