Data Fields
AESCTRCC26XX_Object Struct Reference

AESCTRCC26XX Object. More...

#include <AESCTRCC26XX.h>

Collaboration diagram for AESCTRCC26XX_Object:
Collaboration graph
[legend]

Data Fields

bool isOpen
 
bool operationInProgress
 
bool operationCanceled
 
bool threadSafe
 
int_fast16_t returnStatus
 
AESCTR_ReturnBehavior returnBehavior
 
AESCTR_OperationType operationType
 
uint32_t semaphoreTimeout
 
AESCTR_CallbackFxn callbackFxn
 
AESCTR_Operationoperation
 

Detailed Description

AESCTRCC26XX Object.

The application must not access any member variables of this structure!

Field Documentation

§ isOpen

bool AESCTRCC26XX_Object::isOpen

§ operationInProgress

bool AESCTRCC26XX_Object::operationInProgress

§ operationCanceled

bool AESCTRCC26XX_Object::operationCanceled

§ threadSafe

bool AESCTRCC26XX_Object::threadSafe

§ returnStatus

int_fast16_t AESCTRCC26XX_Object::returnStatus

§ returnBehavior

AESCTR_ReturnBehavior AESCTRCC26XX_Object::returnBehavior

§ operationType

AESCTR_OperationType AESCTRCC26XX_Object::operationType

§ semaphoreTimeout

uint32_t AESCTRCC26XX_Object::semaphoreTimeout

§ callbackFxn

AESCTR_CallbackFxn AESCTRCC26XX_Object::callbackFxn

§ operation

AESCTR_Operation* AESCTRCC26XX_Object::operation

The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale