Data Fields
ADCBuf_Config Struct Reference

ADC driver's custom configuration structure. More...

#include <ADCBuf.h>

Collaboration diagram for ADCBuf_Config:
Collaboration graph
[legend]

Data Fields

const ADCBuf_FxnTablefxnTablePtr
 
void * object
 
void const * hwAttrs
 

Detailed Description

ADC driver's custom configuration structure.

See also
ADCBuf_init()
ADCBuf_open()

Field Documentation

§ fxnTablePtr

const ADCBuf_FxnTable* ADCBuf_Config::fxnTablePtr

Pointer to a function pointer table with driver-specific implementations of ADC APIs

§ object

void* ADCBuf_Config::object

Pointer to a driver specific data object.

§ hwAttrs

void const* ADCBuf_Config::hwAttrs

Pointer to a driver specific hardware attributes structure.


The documentation for this struct was generated from the following file:
© Copyright 1995-2022, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale