TI BLE Stack API Documentation
2.03.11
|
#include <gattservapp.h>
Public Attributes | |
uint8 | format |
Format of the value of this characteristic. | |
int8 | exponent |
A sign integer which represents the exponent of an integer. | |
uint16 | unit |
Unit of this attribute as defined in the data dictionary. | |
uint8 | nameSpace |
Name space of the description. | |
uint16 | desc |
Description of this attribute as defined in a higher layer profile. | |
GATT Structure for Characteristic Presentation Format Value.