TI BLE Stack API Documentation
2.03.11
|
Functions | |
void | GATT_SetHostToAppFlowCtrl (uint16 heapSize, uint8 flowCtrlMode) |
This API is used by the Application to turn flow control on or off for GATT messages sent from the Host to the Application. More... | |
void | GATT_AppCompletedMsg (gattMsgEvent_t *pMsg) |
This API is used by the Application to notify GATT that the processing of a message has been completed. More... | |
void GATT_AppCompletedMsg | ( | gattMsgEvent_t * | pMsg | ) |
This API is used by the Application to notify GATT that the processing of a message has been completed.
pMsg | - pointer to the processed GATT message |
void GATT_SetHostToAppFlowCtrl | ( | uint16 | heapSize, |
uint8 | flowCtrlMode | ||
) |
This API is used by the Application to turn flow control on or off for GATT messages sent from the Host to the Application.
Note: If the flow control is enabled then the Application must call the GATT_AppCompletedMsg() API when it completes processing an incoming GATT message.
heapSize | - internal heap size |
flowCtrlMode | - flow control mode: TRUE or FALSE |