TI BLE Stack API Documentation  2.03.11
Functions
GAP API Functions

Functions

bStatus_t GAP_DeviceInit (uint8 taskID, uint8 profileRole, uint8 maxScanResponses, uint8 *pIRK, uint8 *pSRK, uint32 *pSignCounter)
 Called to setup the device. Call just once on initialization. More...
 
bStatus_t GAP_SetAdvToken (gapAdvDataToken_t *pToken)
 Called to setup a GAP Advertisement/Scan Response data token. More...
 
gapAdvDataToken_t * GAP_GetAdvToken (uint8 adType)
 Called to read a GAP Advertisement/Scan Response data token. More...
 
gapAdvDataToken_t * GAP_RemoveAdvToken (uint8 adType)
 Called to remove a GAP Advertisement/Scan Response data token. More...
 
bStatus_t GAP_UpdateAdvTokens (void)
 Called to rebuild and load Advertisement and Scan Response data from existing GAP Advertisement Tokens. More...
 
bStatus_t GAP_SetParamValue (gapParamIDs_t paramID, uint16 paramValue)
 Set a GAP Parameter value. Use this function to change the default GAP parameter values. More...
 
uint16 GAP_GetParamValue (gapParamIDs_t paramID)
 Get a GAP Parameter value. More...
 
bStatus_t GAP_ConfigDeviceAddr (uint8 addrMode, uint8 *pStaticAddr)
 Setup the device's address type. If ADDRMODE_PRIVATE_RESOLVE is selected, the address will change periodically. More...
 
void GAP_RegisterForMsgs (uint8 taskID)
 Register your task ID to receive extra (unprocessed) HCI status and complete, and Host events. More...
 
void GAP_RegisterBondMgrCBs (gapBondMgrCBs_t *pCBs)
 Register bond manager call backs. More...
 
bStatus_t GAP_DeviceDiscoveryRequest (gapDevDiscReq_t *pParams)
 Start a device discovery scan. More...
 
bStatus_t GAP_DeviceDiscoveryCancel (uint8 taskID)
 Cancel an existing device discovery request. More...
 
bStatus_t GAP_MakeDiscoverable (uint8 taskID, gapAdvertisingParams_t *pParams)
 Setup or change advertising. Also starts advertising. More...
 
bStatus_t GAP_UpdateAdvertisingData (uint8 taskID, uint8 adType, uint8 dataLen, uint8 *pAdvertData)
 Setup or change advertising and scan response data. More...
 
bStatus_t GAP_EndDiscoverable (uint8 taskID)
 Stops advertising. More...
 
bStatus_t GAP_ResolvePrivateAddr (uint8 *pIRK, uint8 *pAddr)
 Resolves a private address against an IRK. More...
 
bStatus_t GAP_EstablishLinkReq (gapEstLinkReq_t *pParams)
 Establish a link to a slave device. More...
 
bStatus_t GAP_TerminateLinkReq (uint8 taskID, uint16 connectionHandle, uint8 reason)
 Terminate a link connection. More...
 
bStatus_t GAP_UpdateLinkParamReq (gapUpdateLinkParamReq_t *pParams)
 Update the link parameters to a Master or Slave device. More...
 
bStatus_t GAP_UpdateLinkParamReqReply (gapUpdateLinkParamReqReply_t *pParams)
 Reply to a Connection Parameter Update Request sent from a remote device. More...
 
uint8 GAP_NumActiveConnections (void)
 Returns the number of active connections. More...
 
bStatus_t GAP_Authenticate (gapAuthParams_t *pParams, gapPairingReq_t *pPairReq)
 Start the Authentication process with the requested device. This function is used to Initiate/Allow pairing. Called by both master and slave device (Central and Peripheral). More...
 
bStatus_t GAP_TerminateAuth (uint16 connectionHandle, uint8 reason)
 Send a Pairing Failed message and end any existing pairing. More...
 
bStatus_t GAP_PasskeyUpdate (uint8 *pPasskey, uint16 connectionHandle)
 Update the passkey in string format. This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message. More...
 
bStatus_t GAP_PasscodeUpdate (uint32 passcode, uint16 connectionHandle)
 Update the passkey in a numeric value (not string). This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message. More...
 
bStatus_t GAP_SendSlaveSecurityRequest (uint16 connectionHandle, uint8 authReq)
 Generate a Slave Requested Security message to the master. More...
 
bStatus_t GAP_Signable (uint16 connectionHandle, uint8 authenticated, smSigningInfo_t *pParams)
 Set up the connection to accept signed data. More...
 
bStatus_t GAP_Bond (uint16 connectionHandle, uint8 authenticated, uint8 secureConnections, smSecurityInfo_t *pParams, uint8 startEncryption)
 Set up the connection's bound paramaters. More...
 

Detailed Description

Function Documentation

§ GAP_Authenticate()

bStatus_t GAP_Authenticate ( gapAuthParams_t *  pParams,
gapPairingReq_t *  pPairReq 
)

Start the Authentication process with the requested device. This function is used to Initiate/Allow pairing. Called by both master and slave device (Central and Peripheral).

NOTE: This function is called after the link is established.

Parameters
pParams- Authentication parameters
pPairReq- Enter these parameters if the Pairing Request was already received. NULL, if waiting for Pairing Request or if initiating.
Returns
SUCCESS,
bleIncorrectMode: Not correct profile role,
INVALIDPARAMETER,
bleNotConnected,
bleAlreadyInRequestedMode,
FAILURE - not workable.

§ GAP_Bond()

bStatus_t GAP_Bond ( uint16  connectionHandle,
uint8  authenticated,
uint8  secureConnections,
smSecurityInfo_t *  pParams,
uint8  startEncryption 
)

Set up the connection's bound paramaters.

NOTE: This function is called after the link is established.

Parameters
connectionHandle- connection handle of the signing information
authenticated- TRUE if bond is authenticated.
secureConnections- TRUE if bond has Secure Connections strength.
pParams- the connected device's security parameters
startEncryption- whether or not to start encryption
Returns
SUCCESS,
bleIncorrectMode: Not correct profile role,
INVALIDPARAMETER,
bleNotConnected,
FAILURE: not workable.

§ GAP_ConfigDeviceAddr()

bStatus_t GAP_ConfigDeviceAddr ( uint8  addrMode,
uint8 *  pStaticAddr 
)

Setup the device's address type. If ADDRMODE_PRIVATE_RESOLVE is selected, the address will change periodically.

Parameters
addrMode- GAP Addressing Modes
pStaticAddr- Only used with ADDRMODE_STATIC or ADDRMODE_PRIVATE_NONRESOLVE type.
NULL to auto generate otherwise the application can specify the address value
Returns
SUCCESS: address type updated,
bleNotReady: Can't be called until GAP_DeviceInit() is called and the init process is completed,
bleIncorrectMode: can't change with an active connection,
or INVALIDPARAMETER.

If return value isn't SUCCESS, the address type remains the same as before this call.

§ GAP_DeviceDiscoveryCancel()

bStatus_t GAP_DeviceDiscoveryCancel ( uint8  taskID)

Cancel an existing device discovery request.

Parameters
taskID- used to return GAP_DEVICE_DISCOVERY_EVENT
Returns
SUCCESS: cancel started,
bleInvalidTaskID: Not the task that started discovery,
bleIncorrectMode: not in discovery mode

§ GAP_DeviceDiscoveryRequest()

bStatus_t GAP_DeviceDiscoveryRequest ( gapDevDiscReq_t *  pParams)

Start a device discovery scan.

Parameters
pParams- Device Discovery parameters
Returns
SUCCESS: scan started,
bleIncorrectMode: invalid profile role,
bleAlreadyInRequestedMode: not available

§ GAP_DeviceInit()

bStatus_t GAP_DeviceInit ( uint8  taskID,
uint8  profileRole,
uint8  maxScanResponses,
uint8 *  pIRK,
uint8 *  pSRK,
uint32 *  pSignCounter 
)

Called to setup the device. Call just once on initialization.

NOTE: When initialization is complete, the calling app will be sent the GAP_DEVICE_INIT_DONE_EVENT

Parameters
taskID- Default task ID to send events.
profileRole- GAP Profile Roles: GAP Profile Roles
maxScanResponses- maximum number to scan responses we can receive during a device discovery.
pIRK- pointer to Identity Root Key, NULLKEY (all zeroes) if the app wants the GAP to generate the key.
pSRK- pointer to Sign Resolving Key, NULLKEY if the app wants the GAP to generate the key.
pSignCounter- 32 bit value used in the SM Signing algorithm that shall be initialized to zero and incremented with every new signing. This variable must also be maintained by the application.
Returns
SUCCESS - Processing, expect GAP_DEVICE_INIT_DONE_EVENT,
INVALIDPARAMETER - for invalid profile role or role combination,
bleIncorrectMode - trouble communicating with HCI

§ GAP_EndDiscoverable()

bStatus_t GAP_EndDiscoverable ( uint8  taskID)

Stops advertising.

Parameters
taskID- of task that called GAP_MakeDiscoverable
Returns
SUCCESS: stopping discoverable mode,
bleIncorrectMode: not in discoverable mode,
bleInvalidTaskID: not correct task

§ GAP_EstablishLinkReq()

bStatus_t GAP_EstablishLinkReq ( gapEstLinkReq_t *  pParams)

Establish a link to a slave device.

Parameters
pParams- link establishment parameters
Returns
SUCCESS: started establish link process,
bleIncorrectMode: invalid profile role,
bleNotReady: a scan is in progress,
bleAlreadyInRequestedMode: can't process now,
bleNoResources: Too many links

§ GAP_GetAdvToken()

gapAdvDataToken_t* GAP_GetAdvToken ( uint8  adType)

Called to read a GAP Advertisement/Scan Response data token.

Parameters
adType- Advertisement type to get
Returns
pointer to the advertisement data token structure, NULL if not found.

§ GAP_GetParamValue()

uint16 GAP_GetParamValue ( gapParamIDs_t  paramID)

Get a GAP Parameter value.

Parameters
paramID- parameter ID: GAP Parameter IDs
Returns
GAP Parameter value or 0xFFFF if invalid

§ GAP_MakeDiscoverable()

bStatus_t GAP_MakeDiscoverable ( uint8  taskID,
gapAdvertisingParams_t *  pParams 
)

Setup or change advertising. Also starts advertising.

Parameters
taskID- used to return GAP_DISCOVERABLE_RESPONSE_EVENT
pParams- advertising parameters
Returns
SUCCESS: advertising started,
bleIncorrectMode: invalid profile role,
bleAlreadyInRequestedMode: not available at this time,
bleNotReady: advertising data isn't set up yet.

§ GAP_NumActiveConnections()

uint8 GAP_NumActiveConnections ( void  )

Returns the number of active connections.

Returns
Number of active connections.

§ GAP_PasscodeUpdate()

bStatus_t GAP_PasscodeUpdate ( uint32  passcode,
uint16  connectionHandle 
)

Update the passkey in a numeric value (not string). This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message.

NOTE: This function is the same as GAP_PasskeyUpdate(), except that the passkey is passed in as a non-string format.

Parameters
passcode- not string - range: 0 - 999,999.
connectionHandle- connection handle.
Returns
SUCCESS: will start pairing with this entry,
bleIncorrectMode: Link not found,
INVALIDPARAMETER: passkey == NULL or passkey isn't formatted properly.

§ GAP_PasskeyUpdate()

bStatus_t GAP_PasskeyUpdate ( uint8 *  pPasskey,
uint16  connectionHandle 
)

Update the passkey in string format. This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message.

NOTE: This function is the same as GAP_PasscodeUpdate(), except that the passkey is passed in as a string format.

Parameters
pPasskey- new passkey - pointer to numeric string (ie. "019655" ). This string's range is "000000" to "999999".
connectionHandle- connection handle.
Returns
SUCCESS: will start pairing with this entry,
bleIncorrectMode: Link not found,
INVALIDPARAMETER: passkey == NULL or passkey isn't formatted properly.

§ GAP_RegisterBondMgrCBs()

void GAP_RegisterBondMgrCBs ( gapBondMgrCBs_t *  pCBs)

Register bond manager call backs.

Parameters
pCBs- pointer to Bond Manager Callbacks.
Returns
none

§ GAP_RegisterForMsgs()

void GAP_RegisterForMsgs ( uint8  taskID)

Register your task ID to receive extra (unprocessed) HCI status and complete, and Host events.

Parameters
taskID- Default task ID to send events.
Returns
none

§ GAP_RemoveAdvToken()

gapAdvDataToken_t* GAP_RemoveAdvToken ( uint8  adType)

Called to remove a GAP Advertisement/Scan Response data token.

Parameters
adType- Advertisement type to remove
Returns
pointer to the token structure removed from the GAP ADType list NULL if the requested adType wasn't found.

§ GAP_ResolvePrivateAddr()

bStatus_t GAP_ResolvePrivateAddr ( uint8 *  pIRK,
uint8 *  pAddr 
)

Resolves a private address against an IRK.

Parameters
pIRK- pointer to the IRK
pAddr- pointer to the Resolvable Private address
Returns
SUCCESS: match,
FAILURE: don't match,
INVALIDPARAMETER: parameters invalid

§ GAP_SendSlaveSecurityRequest()

bStatus_t GAP_SendSlaveSecurityRequest ( uint16  connectionHandle,
uint8  authReq 
)

Generate a Slave Requested Security message to the master.

Parameters
connectionHandle- connection handle.
authReq- Authentication Requirements: Bit 2: MITM, Bits 0-1: bonding (0 - no bonding, 1 - bonding) Bit 3: Secure Connections
Returns
SUCCESS: will send,
bleNotConnected: Link not found,
bleIncorrectMode: wrong GAP role, must be a Peripheral Role

§ GAP_SetAdvToken()

bStatus_t GAP_SetAdvToken ( gapAdvDataToken_t *  pToken)

Called to setup a GAP Advertisement/Scan Response data token.

NOTE: The data in these items are stored as low byte first (OTA format). The passed in structure "token" should be allocated by the calling app/profile and not released until after calling GAP_RemoveAdvToken().

Parameters
pToken- Advertisement/Scan response token to write.
Returns
SUCCESS - advertisement token added to the GAP list
INVALIDPARAMETER - Invalid Advertisement Type or pAttrData is NULL
INVALID_MEM_SIZE - The tokens take up too much space and don't fit into Advertisement data and Scan Response Data
bleInvalidRange - token ID already exists.
bleIncorrectMode - not a peripheral device
bleMemAllocError - memory allocation failure,

§ GAP_SetParamValue()

bStatus_t GAP_SetParamValue ( gapParamIDs_t  paramID,
uint16  paramValue 
)

Set a GAP Parameter value. Use this function to change the default GAP parameter values.

Parameters
paramID- parameter ID: GAP Parameter IDs
paramValue- new param value
Returns
SUCCESS or INVALIDPARAMETER (invalid paramID)

§ GAP_Signable()

bStatus_t GAP_Signable ( uint16  connectionHandle,
uint8  authenticated,
smSigningInfo_t *  pParams 
)

Set up the connection to accept signed data.

NOTE: This function is called after the link is established.

Parameters
connectionHandle- connection handle of the signing information
authenticated- TRUE if the signing information is authenticated, FALSE otherwise
pParams- signing parameters
Returns
SUCCESS,
bleIncorrectMode: Not correct profile role,
INVALIDPARAMETER,
bleNotConnected,
FAILURE: not workable.

§ GAP_TerminateAuth()

bStatus_t GAP_TerminateAuth ( uint16  connectionHandle,
uint8  reason 
)

Send a Pairing Failed message and end any existing pairing.

Parameters
connectionHandle- connection handle.
reason- Pairing Failed reason code.
Returns
SUCCESS - function was successful,
bleMemAllocError - memory allocation error,
INVALIDPARAMETER - one of the parameters were invalid,
bleNotConnected - link not found,
bleInvalidRange - one of the parameters were not within range.

§ GAP_TerminateLinkReq()

bStatus_t GAP_TerminateLinkReq ( uint8  taskID,
uint16  connectionHandle,
uint8  reason 
)

Terminate a link connection.

Parameters
taskID- requesting app's task id.
connectionHandle- connection handle of link to terminate or GAP Special Connection Handles
reason- terminate reason.
Returns
SUCCESS: Terminate started,
bleIncorrectMode: No Link to terminate,
bleInvalidTaskID: not app that established link

§ GAP_UpdateAdvertisingData()

bStatus_t GAP_UpdateAdvertisingData ( uint8  taskID,
uint8  adType,
uint8  dataLen,
uint8 *  pAdvertData 
)

Setup or change advertising and scan response data.

NOTE: if the return status from this function is SUCCESS, the task isn't complete until the GAP_ADV_DATA_UPDATE_DONE_EVENT is sent to the calling application task.

Parameters
taskID- task ID of the app requesting the change
adType- TRUE - advertisement data, FALSE - scan response data
dataLen- Octet length of advertData
pAdvertData- advertising or scan response data
Returns
SUCCESS: data accepted,
bleIncorrectMode: invalid profile role,

§ GAP_UpdateAdvTokens()

bStatus_t GAP_UpdateAdvTokens ( void  )

Called to rebuild and load Advertisement and Scan Response data from existing GAP Advertisement Tokens.

Returns
SUCCESS or bleIncorrectMode

§ GAP_UpdateLinkParamReq()

bStatus_t GAP_UpdateLinkParamReq ( gapUpdateLinkParamReq_t *  pParams)

Update the link parameters to a Master or Slave device.

Parameters
pParams- link update parameters
Returns
SUCCESS: started update link process,
INVALIDPARAMETER: one of the parameters were invalid,
bleIncorrectMode: invalid profile role,
bleAlreadyInRequestedMode: already updating link parameters,
bleNotConnected: not in a connection

§ GAP_UpdateLinkParamReqReply()

bStatus_t GAP_UpdateLinkParamReqReply ( gapUpdateLinkParamReqReply_t *  pParams)

Reply to a Connection Parameter Update Request sent from a remote device.

Parameters
pParams- local device's desired connection parameters.
Returns
SUCCESS: reply sent successfully,
INVALIDPARAMETER: one of the parameters were invalid,
bleIncorectMode: invalid profile role,
bleAlreadyInRequestedMode: already updating link parameters,
bleNotConnected: not in a connection