TI BLE Stack API Documentation  2.03.10
Macros

Macros

#define GAP_DEVICE_INIT_DONE_EVENT   0x00
 Sent when the Device Initialization is complete. This event is sent as an OSAL message defined as gapDeviceInitDoneEvent_t.
 
#define GAP_DEVICE_DISCOVERY_EVENT   0x01
 Sent when the Device Discovery Process is complete. This event is sent as an OSAL message defined as gapDevDiscEvent_t.
 
#define GAP_ADV_DATA_UPDATE_DONE_EVENT   0x02
 Sent when the Advertising Data or SCAN_RSP Data has been updated. This event is sent as an OSAL message defined as gapAdvDataUpdateEvent_t.
 
#define GAP_MAKE_DISCOVERABLE_DONE_EVENT   0x03
 Sent when the Make Discoverable Request is complete. This event is sent as an OSAL message defined as gapMakeDiscoverableRspEvent_t.
 
#define GAP_END_DISCOVERABLE_DONE_EVENT   0x04
 Sent when the Advertising has ended. This event is sent as an OSAL message defined as gapEndDiscoverableRspEvent_t.
 
#define GAP_LINK_ESTABLISHED_EVENT   0x05
 Sent when the Establish Link Request is complete. This event is sent as an OSAL message defined as gapEstLinkReqEvent_t.
 
#define GAP_LINK_TERMINATED_EVENT   0x06
 Sent when a connection was terminated. This event is sent as an OSAL message defined as gapTerminateLinkEvent_t.
 
#define GAP_LINK_PARAM_UPDATE_EVENT   0x07
 Sent when an Update Parameters Event is received. This event is sent as an OSAL message defined as gapLinkUpdateEvent_t.
 
#define GAP_RANDOM_ADDR_CHANGED_EVENT   0x08
 Sent when a random address was changed. This event is sent as an OSAL message defined as gapRandomAddrEvent_t.
 
#define GAP_SIGNATURE_UPDATED_EVENT   0x09
 Sent when the device's signature counter is updated. This event is sent as an OSAL message defined as gapSignUpdateEvent_t.
 
#define GAP_AUTHENTICATION_COMPLETE_EVENT   0x0A
 Sent when the Authentication (pairing) process is complete. This event is sent as an OSAL message defined as gapAuthCompleteEvent_t.
 
#define GAP_PASSKEY_NEEDED_EVENT   0x0B
 Sent when a Passkey is needed. This is part of the pairing process. This event is sent as an OSAL message defined as gapPasskeyNeededEvent_t.
 
#define GAP_SLAVE_REQUESTED_SECURITY_EVENT   0x0C
 Sent when a Slave Security Request is received. This event is sent as an OSAL message defined as gapSlaveSecurityReqEvent_t.
 
#define GAP_DEVICE_INFO_EVENT   0x0D
 Sent during the Device Discovery Process when a device is discovered. This event is sent as an OSAL message defined as gapDeviceInfoEvent_t.
 
#define GAP_BOND_COMPLETE_EVENT   0x0E
 Sent when the bonding(bound) process is complete. This event is sent as an OSAL message defined as gapBondCompleteEvent_t.
 
#define GAP_PAIRING_REQ_EVENT   0x0F
 Sent when an unexpected Pairing Request is received. This event is sent as an OSAL message defined as gapPairingReqEvent_t.
 
#define GAP_AUTHENTICATION_FAILURE_EVT   0x10
 Sent when pairing fails, no GAP_AUTHENTICATION_COMPLETE_EVENT is sent and GBM_QUEUE_PAIRINGS. This event is sent as an OSAL message defined as osal_event_hdr_t.
 
#define GAP_UPDATE_LINK_PARAM_REQ_EVENT   0x11
 Sent when during a Connection Parameter Update Procedure. This event is sent as an OSAL message defined as gapConnParamUpdate_t.
 

Detailed Description