TI BLE Stack API Documentation
2.03.10
|
Macros | |
#define | bleInvalidTaskID INVALID_TASK |
Task ID isn't setup properly. | |
#define | bleNotReady 0x10 |
Not ready to perform task. | |
#define | bleAlreadyInRequestedMode 0x11 |
Already performing that task. | |
#define | bleIncorrectMode 0x12 |
Not setup properly to perform that task. | |
#define | bleMemAllocError 0x13 |
Memory allocation error occurred. | |
#define | bleNotConnected 0x14 |
Can't perform function when not in a connection. | |
#define | bleNoResources 0x15 |
There are no resource available. | |
#define | blePending 0x16 |
Waiting. | |
#define | bleTimeout 0x17 |
Timed out performing function. | |
#define | bleInvalidRange 0x18 |
A parameter is out of range. | |
#define | bleLinkEncrypted 0x19 |
The link is already encrypted. | |
#define | bleProcedureComplete 0x1A |
The Procedure is completed. | |
#define | bleInvalidMtuSize 0x1B |
MTU size is out of range. | |
#define | bleGAPUserCanceled 0x30 |
The user canceled the task. | |
#define | bleGAPConnNotAcceptable 0x31 |
The connection was not accepted. | |
#define | bleGAPBondRejected 0x32 |
The bound information was rejected. | |
#define | bleInvalidPDU 0x40 |
The attribute PDU is invalid. | |
#define | bleInsufficientAuthen 0x41 |
The attribute has insufficient authentication. | |
#define | bleInsufficientEncrypt 0x42 |
The attribute has insufficient encryption. | |
#define | bleInsufficientKeySize 0x43 |
The attribute has insufficient encryption key size. | |
#define | INVALID_TASK_ID 0xFF |
Task ID isn't setup properly. | |
returned as bStatus_t