Macros | |
#define | SPIFFSNVS_STATUS_SUCCESS (0) |
Successful status code returned by: SPIFFSNVS_config() More... | |
#define | SPIFFSNVS_STATUS_ERROR (-1) |
Generic error status code returned by: SPIFFSNVS_config() More... | |
#define | SPIFFSNVS_STATUS_INV_NVS_IDX (-2) |
An error status code returned by SPIFFSNVS_config() More... | |
#define | SPIFFSNVS_STATUS_INV_BLOCK_SIZE (-3) |
An error status code returned by SPIFFSNVS_config() More... | |
#define | SPIFFSNVS_STATUS_INV_PAGE_SIZE (-4) |
An error status code returned by SPIFFSNVS_config() More... | |
#define SPIFFSNVS_STATUS_SUCCESS (0) |
Successful status code returned by: SPIFFSNVS_config()
Returned if the API was executed successfully.
#define SPIFFSNVS_STATUS_ERROR (-1) |
Generic error status code returned by: SPIFFSNVS_config()
Returned if the API was not executed successfully.
#define SPIFFSNVS_STATUS_INV_NVS_IDX (-2) |
An error status code returned by SPIFFSNVS_config()
SPIFFSNVS_config() will return this value if the NVS index is invalid.
#define SPIFFSNVS_STATUS_INV_BLOCK_SIZE (-3) |
An error status code returned by SPIFFSNVS_config()
Error status code returned if the logicalBlockSize argument is not an integer multiple of the physical block size. (e.g., logicalBlockSize = n * physicalBlockSize; where n is a positive integer)
#define SPIFFSNVS_STATUS_INV_PAGE_SIZE (-4) |
An error status code returned by SPIFFSNVS_config()
Error status code returned if the logicalBlockSize argument is not an integer multiple of the logicalPageSize argument. (e.g., logicalBlockSize = n * logicalPageSize; where n is a positive integer)