Macros | |
Operation finished normally | |
#define | PROP_DONE_OK 0x3400 |
Operation ended normally. More... | |
#define | PROP_DONE_RXTIMEOUT 0x3401 |
Operation stopped after end trigger while waiting for sync. More... | |
#define | PROP_DONE_BREAK 0x3402 |
Rx stopped due to timeout in the middle of a packet. More... | |
#define | PROP_DONE_ENDED 0x3403 |
Operation stopped after end trigger during reception. More... | |
#define | PROP_DONE_STOPPED 0x3404 |
Operation stopped after stop command. More... | |
#define | PROP_DONE_ABORT 0x3405 |
Operation aborted by abort command. More... | |
#define | PROP_DONE_RXERR 0x3406 |
Operation ended after receiving packet with CRC error. More... | |
#define | PROP_DONE_IDLE 0x3407 |
Carrier sense operation ended because of idle channel. More... | |
#define | PROP_DONE_BUSY 0x3408 |
Carrier sense operation ended because of busy channel. More... | |
#define | PROP_DONE_IDLETIMEOUT 0x3409 |
Carrier sense operation ended because of timeout with csConf.timeoutRes = 1. More... | |
#define | PROP_DONE_BUSYTIMEOUT 0x340A |
Carrier sense operation ended because of timeout with csConf.timeoutRes = 0. More... | |
Operation finished with error | |
#define | PROP_ERROR_PAR 0x3800 |
Illegal parameter. More... | |
#define | PROP_ERROR_RXBUF 0x3801 |
No available Rx buffer at the start of a packet. More... | |
#define | PROP_ERROR_RXFULL 0x3802 |
Out of Rx buffer during reception in a partial read buffer. More... | |
#define | PROP_ERROR_NO_SETUP 0x3803 |
Radio was not set up in proprietary mode. More... | |
#define | PROP_ERROR_NO_FS 0x3804 |
Synth was not programmed when running Rx or Tx. More... | |
#define | PROP_ERROR_RXOVF 0x3805 |
Rx overflow observed during operation. More... | |
#define | PROP_ERROR_TXUNF 0x3806 |
#define PROP_DONE_ABORT 0x3405 |
Operation aborted by abort command.
#define PROP_DONE_BREAK 0x3402 |
Rx stopped due to timeout in the middle of a packet.
#define PROP_DONE_BUSY 0x3408 |
Carrier sense operation ended because of busy channel.
#define PROP_DONE_BUSYTIMEOUT 0x340A |
Carrier sense operation ended because of timeout with csConf.timeoutRes = 0.
#define PROP_DONE_ENDED 0x3403 |
Operation stopped after end trigger during reception.
#define PROP_DONE_IDLE 0x3407 |
Carrier sense operation ended because of idle channel.
#define PROP_DONE_IDLETIMEOUT 0x3409 |
Carrier sense operation ended because of timeout with csConf.timeoutRes = 1.
#define PROP_DONE_OK 0x3400 |
Operation ended normally.
#define PROP_DONE_RXERR 0x3406 |
Operation ended after receiving packet with CRC error.
#define PROP_DONE_RXTIMEOUT 0x3401 |
Operation stopped after end trigger while waiting for sync.
#define PROP_DONE_STOPPED 0x3404 |
Operation stopped after stop command.
#define PROP_ERROR_NO_FS 0x3804 |
Synth was not programmed when running Rx or Tx.
#define PROP_ERROR_NO_SETUP 0x3803 |
Radio was not set up in proprietary mode.
#define PROP_ERROR_PAR 0x3800 |
Illegal parameter.
#define PROP_ERROR_RXBUF 0x3801 |
No available Rx buffer at the start of a packet.
#define PROP_ERROR_RXFULL 0x3802 |
Out of Rx buffer during reception in a partial read buffer.
#define PROP_ERROR_RXOVF 0x3805 |
Rx overflow observed during operation.
#define PROP_ERROR_TXUNF 0x3806 |
Tx underflow observed during operation