TI BLE Stack API Documentation
2.03.09
|
Modules | |
Security Manager API Functions | |
Classes | |
struct | smNewRandKeyEvent_t |
struct | smEventHdr_t |
struct | smEccKeysEvt_t |
struct | smDhKeyEvt_t |
struct | keyDist_t |
struct | smEccKeys_t |
struct | smLinkSecurityReq_t |
struct | smSecurityInfo_t |
struct | smIdentityInfo_t |
struct | smSigningInfo_t |
struct | authReq_t |
Macros | |
#define | SM_ECC_KEYS_EVENT 0x00 |
#define | SM_DH_KEY_EVENT 0x01 |
Typedefs | |
typedef void(* | smCB_t) (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY) |
Functions | |
void | SM_Init (uint8 task_id) |
uint16 | SM_ProcessEvent (uint8 task_id, uint16 events) |
void | SM_p256KeyCB (hciEvt_BLEReadP256PublicKeyComplete_t *pK, uint8 *privateKey) |
void | SM_dhKeyCB (hciEvt_BLEGenDHKeyComplete_t *pDhKey) |
Variables | |
osal_event_hdr_t | smNewRandKeyEvent_t::hdr |
SM_NEW_RAND_KEY_EVENT and status. | |
uint8 | smNewRandKeyEvent_t::newKey [16] |
New key value - if status is SUCCESS. | |
osal_event_hdr_t | smEventHdr_t::hdr |
uint8 | smEventHdr_t::opcode |
osal_event_hdr_t | smEccKeysEvt_t::hdr |
SM_MSG_EVENT and status. | |
uint8 | smEccKeysEvt_t::opcode |
SM_ECC_KEYS_EVENT. | |
uint8 | smEccKeysEvt_t::privateKey [32] |
ECC private key. | |
uint8 | smEccKeysEvt_t::publicKeyX [32] |
ECC public key X-coordinate. | |
uint8 | smEccKeysEvt_t::publicKeyY [32] |
ECC public key Y-coordinate. | |
osal_event_hdr_t | smDhKeyEvt_t::hdr |
SM_MSG_EVENT and status. | |
uint8 | smDhKeyEvt_t::opcode |
SM_DH_KEY_EVENT. | |
uint8 | smDhKeyEvt_t::dhKey [32] |
ECC Diffie-Hellman key. | |
unsigned int | keyDist_t::sEncKey:1 |
Set to distribute slave encryption key. | |
unsigned int | keyDist_t::sIdKey:1 |
Set to distribute slave identity key. | |
unsigned int | keyDist_t::sSign:1 |
Set to distribute slave signing key. | |
unsigned int | keyDist_t::sLinkKey:1 |
Set to derive slave link key from slave LTK. | |
unsigned int | keyDist_t::sReserved:4 |
Reserved for slave - don't use. | |
unsigned int | keyDist_t::mEncKey:1 |
Set to distribute master encryption key. | |
unsigned int | keyDist_t::mIdKey:1 |
Set to distribute master identity key. | |
unsigned int | keyDist_t::mSign:1 |
Set to distribute master signing key. | |
unsigned int | keyDist_t::mLinkKey:1 |
Set to derive master link key from master LTK. | |
unsigned int | keyDist_t::mReserved:4 |
Reserved for master - don't use. | |
uint8 | smEccKeys_t::isUsed |
FALSE if not used. USE_PKEYS if public keys only. USE_ALL_KEYS if public and private keys. | |
uint8 | smEccKeys_t::sK [32] |
private key (only used if supplied by Bond Manager) | |
uint8 | smEccKeys_t::pK_x [32] |
public key X-coordinate | |
uint8 | smEccKeys_t::pK_y [32] |
public key Y-coordinate | |
uint8 | smLinkSecurityReq_t::ioCaps |
I/O Capabilities (ie. | |
uint8 | smLinkSecurityReq_t::oobAvailable |
True if remote Out-of-band key available. | |
uint8 | smLinkSecurityReq_t::oob [16] |
Out-Of-Bounds key from remote device. | |
uint8 | smLinkSecurityReq_t::oobConfirm [16] |
Out-Of-Bounds confirm from remote device. Secure Connections only. | |
uint8 | smLinkSecurityReq_t::localOobAvailable |
True if local Out-of-band key available. Secure Connections only. | |
uint8 | smLinkSecurityReq_t::localOob [16] |
Out-Of-Bounds local data. Secure Connections only. | |
uint8 | smLinkSecurityReq_t::isSCOnlyMode |
TRUE if Secure Connections Only Mode. Secure Connections only. | |
smEccKeys_t | smLinkSecurityReq_t::eccKeys |
Optionally specified ECC keys for pairing. Secure Connections only. | |
uint8 | smLinkSecurityReq_t::authReq |
Authentication Requirements. | |
keyDist_t | smLinkSecurityReq_t::keyDist |
Key Distribution mask. | |
uint8 | smLinkSecurityReq_t::maxEncKeySize |
Maximum Encryption Key size (7-16 bytes) | |
uint8 | smSecurityInfo_t::ltk [16] |
Long Term Key (LTK) | |
uint16 | smSecurityInfo_t::div |
LTK Diversifier. | |
uint8 | smSecurityInfo_t::rand [8] |
LTK random number. | |
uint8 | smSecurityInfo_t::keySize |
LTK Key Size (7-16 bytes) | |
uint8 | smIdentityInfo_t::irk [16] |
Identity Resolving Key (IRK) | |
uint8 | smIdentityInfo_t::addrType |
Address type for BD_ADDR. | |
uint8 | smIdentityInfo_t::bd_addr [6] |
The advertiser may set this to zeroes to not disclose its BD_ADDR (public address). | |
uint8 | smSigningInfo_t::srk [16] |
Signature Resolving Key (CSRK) | |
uint32 | smSigningInfo_t::signCounter |
Sign Counter. | |
unsigned int | authReq_t::bonding:2 |
Bonding flags. | |
unsigned int | authReq_t::mitm:1 |
Man-In-The-Middle (MITM) | |
unsigned int | authReq_t::sc:1 |
LE Secure Connections (SC) | |
unsigned int | authReq_t::kp:1 |
LE SC Keypress Notifications. | |
unsigned int | authReq_t::reserved:3 |
Reserved - don't use. | |
typedef void(* smCB_t) (uint8 *secretKey, uint8 *publicKeyX, uint8 *publicKeyY) |
Application callback to the SM for ECC keys and Diffie-Hellman Shared Secret (ECDH).
void SM_Init | ( | uint8 | task_id | ) |
End SM_API