474 #include "hal_assert.h"   492 #define HCI_SUCCESS                                                         0x00    493 #define HCI_ERROR_CODE_UNKNOWN_HCI_CMD                                      0x01    494 #define HCI_ERROR_CODE_UNKNOWN_CONN_ID                                      0x02    495 #define HCI_ERROR_CODE_HW_FAILURE                                           0x03    496 #define HCI_ERROR_CODE_PAGE_TIMEOUT                                         0x04    497 #define HCI_ERROR_CODE_AUTH_FAILURE                                         0x05    498 #define HCI_ERROR_CODE_PIN_KEY_MISSING                                      0x06    499 #define HCI_ERROR_CODE_MEM_CAP_EXCEEDED                                     0x07    500 #define HCI_ERROR_CODE_CONN_TIMEOUT                                         0x08    501 #define HCI_ERROR_CODE_CONN_LIMIT_EXCEEDED                                  0x09    502 #define HCI_ERROR_CODE_SYNCH_CONN_LIMIT_EXCEEDED                            0x0A    503 #define HCI_ERROR_CODE_ACL_CONN_ALREADY_EXISTS                              0x0B    504 #define HCI_ERROR_CODE_CMD_DISALLOWED                                       0x0C    505 #define HCI_ERROR_CODE_CONN_REJ_LIMITED_RESOURCES                           0x0D    506 #define HCI_ERROR_CODE_CONN_REJECTED_SECURITY_REASONS                       0x0E    507 #define HCI_ERROR_CODE_CONN_REJECTED_UNACCEPTABLE_BDADDR                    0x0F    508 #define HCI_ERROR_CODE_CONN_ACCEPT_TIMEOUT_EXCEEDED                         0x10    509 #define HCI_ERROR_CODE_UNSUPPORTED_FEATURE_PARAM_VALUE                      0x11    510 #define HCI_ERROR_CODE_INVALID_HCI_CMD_PARAMS                               0x12    511 #define HCI_ERROR_CODE_REMOTE_USER_TERM_CONN                                0x13    512 #define HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES                0x14    513 #define HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF                    0x15    514 #define HCI_ERROR_CODE_CONN_TERM_BY_LOCAL_HOST                              0x16    515 #define HCI_ERROR_CODE_REPEATED_ATTEMPTS                                    0x17    516 #define HCI_ERROR_CODE_PAIRING_NOT_ALLOWED                                  0x18    517 #define HCI_ERROR_CODE_UNKNOWN_LMP_PDU                                      0x19    518 #define HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE                           0x1A    519 #define HCI_ERROR_CODE_SCO_OFFSET_REJ                                       0x1B    520 #define HCI_ERROR_CODE_SCO_INTERVAL_REJ                                     0x1C    521 #define HCI_ERROR_CODE_SCO_AIR_MODE_REJ                                     0x1D    522 #define HCI_ERROR_CODE_INVALID_LMP_PARAMS                                   0x1E    523 #define HCI_ERROR_CODE_UNSPECIFIED_ERROR                                    0x1F    524 #define HCI_ERROR_CODE_UNSUPPORTED_LMP_PARAM_VAL                            0x20    525 #define HCI_ERROR_CODE_ROLE_CHANGE_NOT_ALLOWED                              0x21    526 #define HCI_ERROR_CODE_LMP_LL_RESP_TIMEOUT                                  0x22    527 #define HCI_ERROR_CODE_LMP_ERR_TRANSACTION_COLLISION                        0x23    528 #define HCI_ERROR_CODE_LMP_PDU_NOT_ALLOWED                                  0x24    529 #define HCI_ERROR_CODE_ENCRYPT_MODE_NOT_ACCEPTABLE                          0x25    530 #define HCI_ERROR_CODE_LINK_KEY_CAN_NOT_BE_CHANGED                          0x26    531 #define HCI_ERROR_CODE_REQ_QOS_NOT_SUPPORTED                                0x27    532 #define HCI_ERROR_CODE_INSTANT_PASSED                                       0x28    533 #define HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED                  0x29    534 #define HCI_ERROR_CODE_DIFFERENT_TRANSACTION_COLLISION                      0x2A    535 #define HCI_ERROR_CODE_RESERVED1                                            0x2B    536 #define HCI_ERROR_CODE_QOS_UNACCEPTABLE_PARAM                               0x2C    537 #define HCI_ERROR_CODE_QOS_REJ                                              0x2D    538 #define HCI_ERROR_CODE_CHAN_ASSESSMENT_NOT_SUPPORTED                        0x2E    539 #define HCI_ERROR_CODE_INSUFFICIENT_SECURITY                                0x2F    540 #define HCI_ERROR_CODE_PARAM_OUT_OF_MANDATORY_RANGE                         0x30    541 #define HCI_ERROR_CODE_RESERVED2                                            0x31    542 #define HCI_ERROR_CODE_ROLE_SWITCH_PENDING                                  0x32    543 #define HCI_ERROR_CODE_RESERVED3                                            0x33    544 #define HCI_ERROR_CODE_RESERVED_SLOT_VIOLATION                              0x34    545 #define HCI_ERROR_CODE_ROLE_SWITCH_FAILED                                   0x35    546 #define HCI_ERROR_CODE_EXTENDED_INQUIRY_RESP_TOO_LARGE                      0x36    547 #define HCI_ERROR_CODE_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST                 0x37    548 #define HCI_ERROR_CODE_HOST_BUSY_PAIRING                                    0x38    549 #define HCI_ERROR_CODE_CONN_REJ_NO_SUITABLE_CHAN_FOUND                      0x39    550 #define HCI_ERROR_CODE_CONTROLLER_BUSY                                      0x3A    551 #define HCI_ERROR_CODE_UNACCEPTABLE_CONN_PARAMETERS                         0x3B    552 #define HCI_ERROR_CODE_DIRECTED_ADV_TIMEOUT                                 0x3C    553 #define HCI_ERROR_CODE_CONN_TERM_MIC_FAILURE                                0x3D    554 #define HCI_ERROR_CODE_CONN_FAILED_TO_ESTABLISH                             0x3E    555 #define HCI_ERROR_CODE_MAC_CONN_FAILED                                      0x3F    556 #define HCI_ERROR_CODE_COARSE_CLOCK_ADJUST_REJECTED                         0x40    563 #define HCI_MAX_NUM_CMD_BUFFERS                        LL_MAX_NUM_CMD_BUFFERS     564 #if defined(CC2540) || defined(CC2541) || defined(CC2541S)   565 #define HCI_MAX_NUM_DATA_BUFFERS                       LL_MAX_NUM_DATA_BUFFERS  //<! Max Num Data Buffers   566 #endif // CC2540 | CC2541 | CC2541S   573 #define FIRST_PKT_HOST_TO_CTRL                         LL_DATA_FIRST_PKT_HOST_TO_CTRL          574 #define CONTINUING_PKT                                 LL_DATA_CONTINUATION_PKT                575 #define FIRST_PKT_CTRL_TO_HOST                         LL_DATA_FIRST_PKT_CTRL_TO_HOST          579 #define HCI_RSSI_NOT_AVAILABLE                         LL_RSSI_NOT_AVAILABLE   584 #define HCI_DISCONNECT_AUTH_FAILURE                    HCI_ERROR_CODE_AUTH_FAILURE                                 585 #define HCI_DISCONNECT_REMOTE_USER_TERM                HCI_ERROR_CODE_REMOTE_USER_TERM_CONN                        586 #define HCI_DISCONNECT_REMOTE_DEV_LOW_RESOURCES        HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES        587 #define HCI_DISCONNECT_REMOTE_DEV_POWER_OFF            HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF            588 #define HCI_DISCONNECT_UNSUPPORTED_REMOTE_FEATURE      HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE                   589 #define HCI_DISCONNECT_KEY_PAIRING_NOT_SUPPORTED       HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED          590 #define HCI_DISCONNECT_UNACCEPTABLE_CONN_INTERVAL      HCI_ERROR_CODE_UNACCEPTABLE_CONN_INTERVAL                   597 #define HCI_READ_CURRENT_TX_POWER_LEVEL                LL_READ_CURRENT_TX_POWER_LEVEL              598 #define HCI_READ_MAX_TX_POWER_LEVEL                    LL_READ_MAX_TX_POWER_LEVEL                  604 #define HCI_CTRL_TO_HOST_FLOW_CTRL_OFF                 0           605 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_OFF    1           606 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_OFF_SYNCH_ON    2           607 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_ON     3           613 #define HCI_PUBLIC_DEVICE_ADDRESS                      LL_DEV_ADDR_TYPE_PUBLIC         614 #define HCI_RANDOM_DEVICE_ADDRESS                      LL_DEV_ADDR_TYPE_RANDOM         620 #define HCI_CONNECTABLE_UNDIRECTED_ADV                 LL_ADV_CONNECTABLE_UNDIRECTED_EVT           621 #define HCI_CONNECTABLE_DIRECTED_HDC_ADV               LL_ADV_CONNECTABLE_DIRECTED_HDC_EVT         622 #define HCI_SCANNABLE_UNDIRECTED                       LL_ADV_SCANNABLE_UNDIRECTED_EVT             623 #define HCI_NONCONNECTABLE_UNDIRECTED_ADV              LL_ADV_NONCONNECTABLE_UNDIRECTED_EVT        624 #define HCI_CONNECTABLE_DIRECTED_LDC_ADV               LL_ADV_CONNECTABLE_DIRECTED_LDC_EVT         630 #define HCI_ADV_CHAN_37                                LL_ADV_CHAN_37          631 #define HCI_ADV_CHAN_38                                LL_ADV_CHAN_38          632 #define HCI_ADV_CHAN_39                                LL_ADV_CHAN_39          633 #define HCI_ADV_CHAN_ALL                               (LL_ADV_CHAN_37 | LL_ADV_CHAN_38 | LL_ADV_CHAN_39)      639 #define HCI_ADV_WL_POLICY_ANY_REQ                      LL_ADV_WL_POLICY_ANY_REQ                640 #define HCI_ADV_WL_POLICY_WL_SCAN_REQ                  LL_ADV_WL_POLICY_WL_SCAN_REQ            641 #define HCI_ADV_WL_POLICY_WL_CONNECT_REQ               LL_ADV_WL_POLICY_WL_CONNECT_REQ         642 #define HCI_ADV_WL_POLICY_WL_ALL_REQ                   LL_ADV_WL_POLICY_WL_ALL_REQ             648 #define HCI_ENABLE_ADV                                 LL_ADV_MODE_ON          649 #define HCI_DISABLE_ADV                                LL_ADV_MODE_OFF         655 #define HCI_SCAN_PASSIVE                               LL_SCAN_PASSIVE         656 #define HCI_SCAN_ACTIVE                                LL_SCAN_ACTIVE          662 // Scan White List Policy   663 #define HCI_SCAN_WL_POLICY_ANY_ADV_PKTS                LL_SCAN_WL_POLICY_ANY_ADV_PKTS          664 #define HCI_SCAN_WL_POLICY_USE_WHITE_LIST              LL_SCAN_WL_POLICY_USE_WHITE_LIST        671 #define HCI_FILTER_REPORTS_DISABLE                     LL_FILTER_REPORTS_DISABLE       672 #define HCI_FILTER_REPORTS_ENABLE                      LL_FILTER_REPORTS_ENABLE        679 #define HCI_SCAN_STOP                                  LL_SCAN_STOP        680 #define HCI_SCAN_START                                 LL_SCAN_START       686 #define HCI_INIT_WL_POLICY_USE_PEER_ADDR               LL_INIT_WL_POLICY_USE_PEER_ADDR         687 #define HCI_INIT_WL_POLICY_USE_WHITE_LIST              LL_INIT_WL_POLICY_USE_WHITE_LIST        693 #define HCI_ENCRYPTION_OFF                             LL_ENCRYPTION_OFF           694 #define HCI_ENCRYPTION_ON                              LL_ENCRYPTION_ON            700 #define HCI_DIRECT_TEST_PAYLOAD_PRBS9                  LL_DIRECT_TEST_PAYLOAD_PRBS9        701 #define HCI_DIRECT_TEST_PAYLOAD_0x0F                   LL_DIRECT_TEST_PAYLOAD_0x0F         702 #define HCI_DIRECT_TEST_PAYLOAD_0x55                   LL_DIRECT_TEST_PAYLOAD_0x55         703 #define HCI_DIRECT_TEST_PAYLOAD_PRBS15                 LL_DIRECT_TEST_PAYLOAD_PRBS15       704 #define HCI_DIRECT_TEST_PAYLOAD_0xFF                   LL_DIRECT_TEST_PAYLOAD_0xFF         705 #define HCI_DIRECT_TEST_PAYLOAD_0x00                   LL_DIRECT_TEST_PAYLOAD_0x00         706 #define HCI_DIRECT_TEST_PAYLOAD_0xF0                   LL_DIRECT_TEST_PAYLOAD_0xF0         707 #define HCI_DIRECT_TEST_PAYLOAD_0xAA                   LL_DIRECT_TEST_PAYLOAD_0xAA         713 #define HCI_DTM_STANDARD_MODULATION_INDEX              LL_DTM_STANDARD_MODULATION_INDEX        714 #define HCI_DTM_STABLE_MODULATION_INDEX                LL_DTM_STABLE_MODULATION_INDEX          720 #define HCI_DISABLE_ADDR_RESOLUTION                    LL_DISABLE_ADDR_RESOLUTION          721 #define HCI_ENABLE_ADDR_RESOLUTION                     LL_ENABLE_ADDR_RESOLUTION           727 #define HCI_PHY_USE_PHY_PARAM                          LL_PHY_USE_PHY_PARAM        728 #define HCI_PHY_USE_ANY_PHY                            LL_PHY_USE_ANY_PHY          734 #define HCI_PHY_1_MBPS                                 LL_PHY_1_MBPS               735 #define HCI_PHY_2_MBPS                                 LL_PHY_2_MBPS               741 #define HCI_EXT_RX_GAIN_STD                            LL_EXT_RX_GAIN_STD          742 #define HCI_EXT_RX_GAIN_HIGH                           LL_EXT_RX_GAIN_HIGH         748 #if defined( CC26XX ) || defined( CC13XX )   749 #define HCI_EXT_TX_POWER_MINUS_21_DBM                  LL_EXT_TX_POWER_MINUS_21_DBM     750 #define HCI_EXT_TX_POWER_MINUS_18_DBM                  LL_EXT_TX_POWER_MINUS_18_DBM     751 #define HCI_EXT_TX_POWER_MINUS_15_DBM                  LL_EXT_TX_POWER_MINUS_15_DBM     752 #define HCI_EXT_TX_POWER_MINUS_12_DBM                  LL_EXT_TX_POWER_MINUS_12_DBM     753 #define HCI_EXT_TX_POWER_MINUS_9_DBM                   LL_EXT_TX_POWER_MINUS_9_DBM     754 #define HCI_EXT_TX_POWER_MINUS_6_DBM                   LL_EXT_TX_POWER_MINUS_6_DBM     755 #define HCI_EXT_TX_POWER_MINUS_3_DBM                   LL_EXT_TX_POWER_MINUS_3_DBM     756 #define HCI_EXT_TX_POWER_0_DBM                         LL_EXT_TX_POWER_0_DBM     757 #define HCI_EXT_TX_POWER_1_DBM                         LL_EXT_TX_POWER_1_DBM     758 #define HCI_EXT_TX_POWER_2_DBM                         LL_EXT_TX_POWER_2_DBM     759 #define HCI_EXT_TX_POWER_3_DBM                         LL_EXT_TX_POWER_3_DBM     760 #define HCI_EXT_TX_POWER_4_DBM                         LL_EXT_TX_POWER_4_DBM     761 #define HCI_EXT_TX_POWER_5_DBM                         LL_EXT_TX_POWER_5_DBM     763 #define HCI_EXT_TX_POWER_MINUS_23_DBM                  LL_EXT_TX_POWER_MINUS_23_DBM    764 #define HCI_EXT_TX_POWER_MINUS_6_DBM                   LL_EXT_TX_POWER_MINUS_6_DBM     765 #define HCI_EXT_TX_POWER_0_DBM                         LL_EXT_TX_POWER_0_DBM           766 #define HCI_EXT_TX_POWER_4_DBM                         LL_EXT_TX_POWER_4_DBM           767 #endif // CC26XX/CC13XX   773 #define HCI_EXT_ENABLE_ONE_PKT_PER_EVT                 LL_EXT_ENABLE_ONE_PKT_PER_EVT       774 #define HCI_EXT_DISABLE_ONE_PKT_PER_EVT                LL_EXT_DISABLE_ONE_PKT_PER_EVT      780 #define HCI_EXT_ENABLE_CLK_DIVIDE_ON_HALT              LL_EXT_ENABLE_CLK_DIVIDE_ON_HALT    781 #define HCI_EXT_DISABLE_CLK_DIVIDE_ON_HALT             LL_EXT_DISABLE_CLK_DIVIDE_ON_HALT       787 #define HCI_EXT_NV_IN_USE                              LL_EXT_NV_IN_USE            788 #define HCI_EXT_NV_NOT_IN_USE                          LL_EXT_NV_NOT_IN_USE        794 #define HCI_EXT_ENABLE_FAST_TX_RESP_TIME               LL_EXT_ENABLE_FAST_TX_RESP_TIME     795 #define HCI_EXT_DISABLE_FAST_TX_RESP_TIME              LL_EXT_DISABLE_FAST_TX_RESP_TIME    801 #define HCI_EXT_ENABLE_SL_OVERRIDE                     LL_EXT_ENABLE_SL_OVERRIDE       802 #define HCI_EXT_DISABLE_SL_OVERRIDE                    LL_EXT_DISABLE_SL_OVERRIDE      808 #define HCI_EXT_TX_MODULATED_CARRIER                   LL_EXT_TX_MODULATED_CARRIER     809 #define HCI_EXT_TX_UNMODULATED_CARRIER                 LL_EXT_TX_UNMODULATED_CARRIER    815 #define HCI_PTM_SET_FREQ_TUNE_DOWN                     LL_EXT_SET_FREQ_TUNE_DOWN       816 #define HCI_PTM_SET_FREQ_TUNE_UP                       LL_EXT_SET_FREQ_TUNE_UP         821 #define HCI_EXT_PM_IO_PORT_P0                          LL_EXT_PM_IO_PORT_P0   822 #define HCI_EXT_PM_IO_PORT_P1                          LL_EXT_PM_IO_PORT_P1   823 #define HCI_EXT_PM_IO_PORT_P2                          LL_EXT_PM_IO_PORT_P2   824 #define HCI_EXT_PM_IO_PORT_NONE                        LL_EXT_PM_IO_PORT_NONE   826 #define HCI_EXT_PM_IO_PORT_PIN0                        LL_EXT_PM_IO_PORT_PIN0   827 #define HCI_EXT_PM_IO_PORT_PIN1                        LL_EXT_PM_IO_PORT_PIN1   828 #define HCI_EXT_PM_IO_PORT_PIN2                        LL_EXT_PM_IO_PORT_PIN2   829 #define HCI_EXT_PM_IO_PORT_PIN3                        LL_EXT_PM_IO_PORT_PIN3   830 #define HCI_EXT_PM_IO_PORT_PIN4                        LL_EXT_PM_IO_PORT_PIN4   831 #define HCI_EXT_PM_IO_PORT_PIN5                        LL_EXT_PM_IO_PORT_PIN5   832 #define HCI_EXT_PM_IO_PORT_PIN6                        LL_EXT_PM_IO_PORT_PIN6   833 #define HCI_EXT_PM_IO_PORT_PIN7                        LL_EXT_PM_IO_PORT_PIN7   839 #define HCI_EXT_PER_RESET                              LL_EXT_PER_RESET        840 #define HCI_EXT_PER_READ                               LL_EXT_PER_READ         846 #define HCI_EXT_HALT_DURING_RF_DISABLE                 LL_EXT_HALT_DURING_RF_DISABLE       847 #define HCI_EXT_HALT_DURING_RF_ENABLE                  LL_EXT_HALT_DURING_RF_ENABLE        853 #define HCI_EXT_SET_USER_REVISION                      LL_EXT_SET_USER_REVISION        854 #define HCI_EXT_READ_BUILD_REVISION                    LL_EXT_READ_BUILD_REVISION      860 #define HCI_EXT_RESET_SYSTEM_HARD                      LL_EXT_RESET_SYSTEM_HARD        861 #define HCI_EXT_RESET_SYSTEM_SOFT                      LL_EXT_RESET_SYSTEM_SOFT        867 #define HCI_EXT_DISABLE_OVERLAPPED_PROCESSING          LL_EXT_DISABLE_OVERLAPPED_PROCESSING    868 #define HCI_EXT_ENABLE_OVERLAPPED_PROCESSING           LL_EXT_ENABLE_OVERLAPPED_PROCESSING     874 #define HCI_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT        LL_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT      875 #define HCI_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT         LL_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT       881 #define HCI_EXT_DISABLE_SCAN_REQUEST_REPORT            LL_EXT_DISABLE_SCAN_REQUEST_REPORT      882 #define HCI_EXT_ENABLE_SCAN_REQUEST_REPORT             LL_EXT_ENABLE_SCAN_REQUEST_REPORT       890 // HCI Link Type for Buffer Overflow   891 #define HCI_LINK_TYPE_SCO_BUFFER_OVERFLOW              0       892 #define HCI_LINK_TYPE_ACL_BUFFER_OVERFLOW              1       902 typedef uint8 hciStatus_t;
  1135   uint8 p256Key[LL_SC_P256_KEY_LEN]; 
  1144   uint8 dhKey[LL_SC_DHKEY_LEN];   
  1188 #if defined( CC26XX ) || defined( CC13XX )  1189 PACKED_TYPEDEF_STRUCT
  1192 #endif // CC26XX/CC13XX  1196   uint8 addr[LL_DEVICE_ADDR_LEN];         
  1200 #if defined( CC26XX ) || defined( CC13XX )  1201 PACKED_TYPEDEF_STRUCT
  1204 #endif // CC26XX/CC13XX  1246 extern void *HCI_bm_alloc( uint16 size );
  1266                                       uint16 connIntervalMax,
  1268                                       uint16 connTimeout );
  1457                                           uint8  hostSyncPktLen,
  1458                                           uint16 hostTotalNumAclPkts,
  1459                                           uint16 hostTotalNumSyncPkts );
  1490                                                uint16 *connHandles,
  1491                                                uint16 *numCompletedPkts );
  1504                                                   uint16 *aptoValue );
  1656                                           uint16 advIntervalMax,
  1659                                           uint8  directAddrType,
  1661                                           uint8  advChannelMap,
  1662                                           uint8  advFilterPolicy );
  1735                                            uint16 scanInterval,
  1738                                            uint8  filterPolicy );
  1754                                             uint8 filterDuplicates );
  1790                                          uint8  initFilterPolicy,
  1794                                          uint16 connIntervalMin,
  1795                                          uint16 connIntervalMax,
  1878                                          uint16 connIntervalMin,
  1879                                          uint16 connIntervalMax,
  2081                                                       uint16 connIntervalMin,
  2082                                                       uint16 connIntervalMax,
  2203                                                             uint8 *peerIdAddr );
  2247                                                         uint8 *peerIdAddr );
  2267                                                          uint8 *localIdAddr );
  3028                                            uint8         *numActiveConns,
 osal_event_hdr_t hdr
osal event header 
Definition: hci.h:928
hciStatus_t HCI_EXT_OverlappedProcessingCmd(uint8 mode)
This HCI Extension API is used to enable or disable overlapped processing. 
uint16 pktLen
packet length 
Definition: hci.h:1169
uint8 pbFlag
flag 
Definition: hci.h:1168
hciStatus_t HCI_EXT_ExtendRfRangeCmd(void)
This HCI Extension API is used to Extend Rf Range using the TI CC2590 2.4 GHz RF Front End device...
uint8 status
status of event 
Definition: hci.h:1098
uint8 role
device connection role 
Definition: hci.h:1195
hciStatus_t HCI_EXT_ScanEventNoticeCmd(uint8 taskID, uint16 taskEvent)
Scan Event Notice Command. 
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:988
hciStatus_t HCI_LE_SetDataLenCmd(uint16 connHandle, uint16 txOctets, uint16 txTime)
Set Data Length. 
hciStatus_t HCI_LE_ReadChannelMapCmd(uint16 connHandle)
Read a connection's data channel map. 
LE Read P256 Public Key Complete Event. 
Definition: hci.h:1130
hciEvt_BLEConnComplete_t legEvt
connection complete event 
Definition: hci.h:947
hciStatus_t HCI_LE_ReadLocalResolvableAddressCmd(uint8 localIdAddrType, uint8 *localIdAddr)
Read Local Resolvable Private Address. 
union _hciEvt_BLEConnComplete_u_ hciEvt_BLEConnComplete_u
LE Connection Complete Event. 
hciEvt_DevInfo_t * devInfo
pointer to the array of devInfo 
Definition: hci.h:968
uint16 connectionHandle
connection handle 
Definition: hci.h:931
hciStatus_t HCI_EXT_NumComplPktsLimitCmd(uint8 limit, uint8 flushOnEvt)
This HCI Extension API is used to set the minimum number of completed packets which must be met befor...
LE Advertising Packet Report Event. 
Definition: hci.h:963
uint8 clockAccuracy
connection clock accuracy 
Definition: hci.h:922
uint16 connectionHandle
connection handle 
Definition: hci.h:1003
uint16 cmdOpcode
command opcode 
Definition: hci.h:1041
uint16 maxRxTime
maximum receive time 
Definition: hci.h:1126
uint8 * pEventParam
event parameters 
Definition: hci.h:1051
uint8 status
status of event 
Definition: hci.h:990
uint8 BLEEventCode
BLE Event code. 
Definition: hci.h:1133
void HCI_ExtTaskRegister(uint8 taskID)
HCI vendor specific registration for Host extended commands. 
uint16 connHandle
connection handle 
Definition: hci.h:1099
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1089
hciStatus_t HCI_LE_ClearWhiteListCmd(void)
Clear the white list. 
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:1097
uint16 maxTxOctets
maximum transmission bytes 
Definition: hci.h:1123
uint8 encEnable
encryption enabled or not 
Definition: hci.h:1014
hciStatus_t HCI_EXT_ModemHopTestTxCmd(void)
Start Modem Hop Tx Test. 
uint16 * pNumCompletedPackets
pointer to the number of completed packets array 
Definition: hci.h:1033
uint16 connLatency
connection latency 
Definition: hci.h:993
hciEvt_BLEEnhConnComplete_t enhEvt
enhanced connection complete event 
Definition: hci.h:948
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1120
uint16 connTimeout
connection supervision timeout 
Definition: hci.h:994
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:965
uint16 connTimeout
connection supervision timeout 
Definition: hci.h:921
hciStatus_t HCI_LE_EnhancedTxTestCmd(uint8 txChan, uint8 payloadLen, uint8 payloadType, uint8 txPhy)
Start Enhanced TX Test. 
uint16 connInterval
connection interval 
Definition: hci.h:935
uint8 reason
reason 
Definition: hci.h:1013
uint16 cmdOpcode
command opcode 
Definition: hci.h:1050
int8 rssi
report RSSI 
Definition: hci.h:959
hciStatus_t HCI_LE_WriteSuggestedDefaultDataLenCmd(uint16 txOctets, uint16 txTime)
Write Suggested Default Data Length. 
uint16 connHandle
connection handle 
Definition: hci.h:1122
hciStatus_t HCI_WriteAuthPayloadTimeoutCmd(uint16 connHandle, uint16 aptoValue)
Used to write the connection's Authenticated Payload Timeout value. 
uint8 clockAccuracy
connection clock accuracy 
Definition: hci.h:938
hciStatus_t HCI_HostNumCompletedPktCmd(uint8 numHandles, uint16 *connHandles, uint16 *numCompletedPkts)
This BT API is used by the Host to notify the Controller of the number of HCI data packets that have ...
void HCI_SMPTaskRegister(uint8 taskID)
HCI vendor specific registration for Host SMP. 
#define B_ADDR_LEN
Default Public and Random Address Length. 
Definition: bcomdef.h:114
hciStatus_t HCI_ReadTransmitPowerLevelCmd(uint16 connHandle, uint8 txPwrType)
Read the transmit power level. 
hciStatus_t HCI_ReadLocalSupportedCommandsCmd(void)
Read the locally supported commands. 
hciStatus_t HCI_LE_ReadLocalP256PublicKeyCmd(void)
Read local P-256 Public Key. 
hciStatus_t HCI_LE_ConnUpdateCmd(uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen)
Update the connection parameters. 
hciStatus_t HCI_EXT_SetFreqTuneCmd(uint8 step)
This HCI Extension API is used to set the frequency tuning up or down. Setting the mode up/down decre...
uint8 addrType
peer device address type 
Definition: hci.h:1197
LE Encryption Change Event. 
Definition: hci.h:1008
uint16 connHandle
connection handle 
Definition: hci.h:1022
uint16 dataPktLen
data packet length 
Definition: hci.h:1151
hciStatus_t HCI_EXT_SetSCACmd(uint16 scaInPPM)
This API is used to set this device's Sleep Clock Accuracy. 
hciStatus_t HCI_EXT_MapPmIoPortCmd(uint8 ioPort, uint8 ioPin)
This HCI Extension API is used to configure and map a CC254x I/O Port as a General Purpose I/O (GPIO)...
uint16 numPkts
total number of rx packets 
Definition: hci.h:1206
osal_event_hdr_t hdr
OSAL Event header. 
Definition: hci.h:1165
LE Read Remote Used Features Complete Event. 
Definition: hci.h:998
hciStatus_t HCI_EXT_ConnEventNoticeCmd(uint16 connHandle, uint8 taskID, uint16 taskEvent)
This HCI Extension API is used to enable or disable a notification to the specified task using the sp...
uint16 connectionHandle
connection handle 
Definition: hci.h:991
uint8 reason
reason 
Definition: hci.h:1076
uint16 connHandle
connection handle 
Definition: hci.h:1012
void HCI_TestAppTaskRegister(uint8 taskID)
HCI vendor specific registration for HCI Test Application. 
osal_event_hdr_t hdr
OSAL event header. 
Definition: hci.h:1158
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:912
int8 rssi
report RSSI 
Definition: hci.h:982
hciStatus_t HCI_LE_SetAdvParamCmd(uint16 advIntervalMin, uint16 advIntervalMax, uint8 advType, uint8 ownAddrType, uint8 directAddrType, uint8 *directAddr, uint8 advChannelMap, uint8 advFilterPolicy)
Set the Advertising parameters. 
hciStatus_t HCI_LE_SetScanEnableCmd(uint8 scanEnable, uint8 filterDuplicates)
Turn Scanning on or off. 
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:975
hciStatus_t HCI_EXT_DecryptCmd(uint8 *key, uint8 *encText)
This HCI Extension API is used to decrypt encrypted data using AES128. 
uint8 status
status of event 
Definition: hci.h:1150
uint16 numEvents
number of connection events 
Definition: hci.h:1208
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1141
hciStatus_t HCI_LE_LtkReqNegReplyCmd(uint16 connHandle)
This LE API is used by the Host to send to the Controller a negative LTK reply. 
uint16 encryptedDiversifier
encrypted diversifier 
Definition: hci.h:1024
uint8 peerAddrType
peer address type 
Definition: hci.h:917
hciStatus_t HCI_EXT_LLTestModeCmd(uint8 testCase)
This HCI Extension API is used to send a LL Test Mode test case. 
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:929
uint8 dataLen
length of report data 
Definition: hci.h:957
hciStatus_t HCI_EXT_DelaySleepCmd(uint16 delay)
This HCI Extension API is used set the sleep delay. 
hciStatus_t HCI_LE_SetAddressResolutionEnableCmd(uint8 addrResolutionEnable)
Disable / Enable Address Resolution. 
hciStatus_t HCI_LE_AddWhiteListCmd(uint8 addrType, uint8 *devAddr)
Add a white list entry. 
hciStatus_t HCI_LE_RandCmd(void)
Generate a random number. 
hciStatus_t HCI_LE_SetAdvEnableCmd(uint8 advEnable)
Turn Advertising on or off. 
hciStatus_t HCI_LE_ReadSuggestedDefaultDataLenCmd(void)
Read Suggested Default Data Length. 
hciStatus_t HCI_LE_SetScanParamCmd(uint8 scanType, uint16 scanInterval, uint16 scanWindow, uint8 ownAddrType, uint8 filterPolicy)
Set the Scan parameters. 
LE Data Length Change Event. 
Definition: hci.h:1118
uint8 connId
device connection handle 
Definition: hci.h:1194
hciStatus_t HCI_HostBufferSizeCmd(uint16 hostAclPktLen, uint8 hostSyncPktLen, uint16 hostTotalNumAclPkts, uint16 hostTotalNumSyncPkts)
This BT API is used by the Host to notify the Controller of the maximum size ACL buffer size the Cont...
uint8 status
status 
Definition: hci.h:1143
uint16 connHandle
connection handle 
Definition: hci.h:1075
hciStatus_t HCI_EXT_DisconnectImmedCmd(uint16 connHandle)
This HCI Extension API is used to disconnect the connection immediately. 
hciStatus_t HCI_DisconnectCmd(uint16 connHandle, uint8 reason)
This BT API is used to terminate a connection. 
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1039
uint8 * pData
data 
Definition: hci.h:1170
hciStatus_t HCI_LE_ReceiverTestCmd(uint8 rxChan)
Start the receiver Direct Test Mode test. 
uint8 ownAddrType
public or random address type 
Definition: hci.h:979
hciStatus_t HCI_ResetCmd(void)
Reset the Link Layer. 
hciStatus_t HCI_LE_AddDeviceToResolvingListCmd(uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 *peerIRK, uint8 *localIRK)
Add a device to the resolving list. 
hciStatus_t HCI_EXT_EndModemTestCmd(void)
This API is used to shutdown a modem test. A complete Controller reset will take place. 
hciStatus_t HCI_LE_RemoveWhiteListCmd(uint8 addrType, uint8 *devAddr)
Remove a white list entry. 
uint8 status
status of event 
Definition: hci.h:1002
uint16 connInterval
connection interval 
Definition: hci.h:919
hciStatus_t HCI_EXT_AdvEventNoticeCmd(uint8 taskID, uint16 taskEvent)
This HCI Extension API is used to enable or disable a notification to the specified task using the sp...
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1066
uint8 addrType
public or random address type 
Definition: hci.h:955
hciStatus_t HCI_LE_ReadPeerResolvableAddressCmd(uint8 peerIdAddrType, uint8 *peerIdAddr)
Read the Peer Resolvable Address. 
hciStatus_t HCI_EXT_SaveFreqTuneCmd(void)
This HCI Extension API is used to save the frequency tuning value to flash. 
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:1021
Command Complete Event. 
Definition: hci.h:1037
LE Generate DHKey Complete Event. 
Definition: hci.h:1139
uint16 Interval_Max
maximum connection interval 
Definition: hci.h:1101
hciStatus_t HCI_LE_SetPhyCmd(uint16 connHandle, uint8 allPhys, uint8 txPhy, uint8 rxPhy)
This LE API is used to request a change to the transmitter and receiver PHY for a connection...
hciStatus_t HCI_LE_StartEncyptCmd(uint16 connHandle, uint8 *random, uint8 *encDiv, uint8 *ltk)
Start encryption in a connection. 
Vendor Specific Command Complete Event. 
Definition: hci.h:1046
hciStatus_t HCI_SetEventMaskCmd(uint8 *pMask)
This BT API is used to set the HCI event mask, which is used to determine which events are supported...
hciStatus_t HCI_ReadBDADDRCmd(void)
Read this device's BLE address (BDADDR). 
uint8 hardwareCode
hardware error code 
Definition: hci.h:1067
uint16 connHandle
connection handle 
Definition: hci.h:1167
hciStatus_t HCI_EXT_ModemTestTxCmd(uint8 cwMode, uint8 txChan)
This API is used start a continuous transmitter modem test, using either a modulated or unmodulated c...
Command Status Event. 
Definition: hci.h:1055
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1073
hciStatus_t HCI_EXT_SetMaxDtmTxPowerCmd(uint8 txPower)
This HCI Extension API is used to set the maximum transmit output power for Direct Test Mode...
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:1121
hciStatus_t HCI_EXT_SetLocalSupportedFeaturesCmd(uint8 *localFeatures)
This HCI Extension API is used to write this device's supported features. 
hciStatus_t HCI_LE_RemoveDeviceFromResolvingListCmd(uint8 peerIdAddrType, uint8 *peerIdAddr)
Remove a device from the whitelist. 
uint8 eventType
scan request event type 
Definition: hci.h:976
LE Connection Complete Event. 
Definition: hci.h:945
uint8 pktType
packet type 
Definition: hci.h:1166
hciStatus_t HCI_LE_ReadMaxDataLenCmd(void)
Read max data length. 
hciStatus_t HCI_EXT_GetConnInfoCmd(uint8 *numAllocConns, uint8 *numActiveConns, hciConnInfo_t *activeConnInfo)
Get Connection Info. 
uint16 connLatency
connection latency 
Definition: hci.h:936
uint8 * pReturnParam
pointer to the return parameter 
Definition: hci.h:1042
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1109
uint16 connHandle
connection handle 
Definition: hci.h:1090
hciStatus_t HCI_SetControllerToHostFlowCtrlCmd(uint8 flowControlEnable)
This BT API is used by the Host to turn flow control on or off for data sent from the Controller to H...
Number of Completed Packets Event. 
Definition: hci.h:1028
uint8 status
status 
Definition: hci.h:1134
uint8 HCI_ValidConnTimeParams(uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout)
This API is used to check that the connection time parameter ranges are valid, and that the connectio...
hciStatus_t HCI_LE_ReadBufSizeCmd(void)
This LE API is used by the Host to determine the maximum ACL data packet size allowed by the Controll...
uint8 role
role of connection 
Definition: hci.h:916
hciStatus_t HCI_ReadRssiCmd(uint16 connHandle)
Read RSSI of last packet. 
hciStatus_t HCI_EXT_ModemTestRxCmd(uint8 rxChan)
Start Modem Hop RX Test. 
uint16 * pConnectionHandle
pointer to the connection handle array 
Definition: hci.h:1032
LE Connection Update Complete Event. 
Definition: hci.h:986
HCI Data Packet. 
Definition: hci.h:1163
uint8 numHciCmdPkt
number of HCI Command Packet 
Definition: hci.h:1040
hciStatus_t HCI_SendDataPkt(uint16 connHandle, uint8 pbFlag, uint16 pktLen, uint8 *pData)
This API is used to send a ACL data packet over a connection. 
hciStatus_t HCI_EXT_SetFastTxResponseTimeCmd(uint8 control)
This HCI Extension API is used to set whether transmit data is sent as soon as possible even when sla...
uint8 numDataPkts
number of data packets 
Definition: hci.h:1152
hciStatus_t HCI_ReadAuthPayloadTimeoutCmd(uint16 connHandle, uint16 *aptoValue)
Read the connection's Authenticated Payload Timeout value. 
hciStatus_t HCI_LE_SetDefaultPhyCmd(uint8 allPhys, uint8 txPhy, uint8 rxPhy)
Set Default PHY. 
hciStatus_t HCI_LE_RemoteConnParamReqReplyCmd(uint16 connHandle, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen)
This LE API is used to positively reply to the HCI LE Remote Connection Parameter Request event from ...
uint16 connectionHandle
connection handle 
Definition: hci.h:915
LE Enhanced Connection Complete Event. 
Definition: hci.h:926
hciStatus_t HCI_LE_ReadLocalSupportedFeaturesCmd(void)
Read the LE locally supported features. 
void HCI_GAPTaskRegister(uint8 taskID)
HCI vendor specific registration for Host GAP. 
hciStatus_t HCI_LE_LtkReqReplyCmd(uint16 connHandle, uint8 *ltk)
This LE API is used by the Host to send to the Controller a positive LTK reply. 
hciStatus_t HCI_ReadRemoteVersionInfoCmd(uint16 connHandle)
This BT API is used to request version information from the the remote device in a connection...
hciStatus_t HCI_LE_TransmitterTestCmd(uint8 txChan, uint8 dataLen, uint8 pktPayload)
This LE API is used to start the transmit Direct Test Mode test. 
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1030
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1057
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1048
#define B_MAX_ADV_LEN
BLE Maximum Advertising Packet Length. 
Definition: bcomdef.h:129
uint8 * pData
data 
Definition: hci.h:1159
hciStatus_t HCI_LE_CreateConnCancelCmd(void)
Cancel connection. 
uint8 status
status of event 
Definition: hci.h:930
uint16 connInterval
connection interval 
Definition: hci.h:992
hciStatus_t HCI_LE_ReadAdvChanTxPowerCmd(void)
Read transmit power when Advertising. 
hciStatus_t HCI_LE_RemoteConnParamReqNegReplyCmd(uint16 connHandle, uint8 reason)
Negatively reply to the Conneciton Parameter Update Request. 
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:974
hciStatus_t HCI_EXT_PERbyChanCmd(uint16 connHandle, perByChan_t *perByChan)
This HCI Extension API is used to start or end Packet Error Rate by Channel counter accumulation for ...
hciStatus_t HCI_LE_GenerateDHKeyCmd(uint8 *publicKey)
Generate Diffie-Hellman Key. 
VS LE Scan Request Report Event. 
Definition: hci.h:972
LE Remote Connection Parameter Request Event. 
Definition: hci.h:1094
hciStatus_t HCI_LE_SetAdvDataCmd(uint8 dataLen, uint8 *pData)
Set the Advertising data. 
Disconnection Complete Event. 
Definition: hci.h:1071
hciStatus_t HCI_LE_ReadSupportedStatesCmd(void)
Read the Controller's supported states. 
hciStatus_t HCI_EXT_OnePktPerEvtCmd(uint8 control)
This HCI Extension API is used to set whether a connection will be limited to one packet per event...
uint8 txPhy
TX PHY. 
Definition: hci.h:1113
hciStatus_t HCI_LE_SetRandomAddressCmd(uint8 *pRandAddr)
Set this device's Random address. 
uint8 status
status of event 
Definition: hci.h:1111
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:913
hciStatus_t HCI_EXT_SetRxGainCmd(uint8 rxGain)
Set the receiver gain. 
uint8 eventType
advertisement or scan response event type 
Definition: hci.h:954
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:1001
uint16 connHandle
connection handle 
Definition: hci.h:1112
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1082
hciStatus_t HCI_LE_ReadResolvingListSizeCmd(void)
Read Resolving List Size. 
hciStatus_t HCI_EXT_ClkDivOnHaltCmd(uint8 control)
Set whether the system clock will be divided when the MCU is halted. 
hciStatus_t HCI_LE_EnhancedRxTestCmd(uint8 rxChan, uint8 rxPhy, uint8 modIndex)
Start Enhanced RX Test. 
uint8 numHandles
number of handles 
Definition: hci.h:1031
hciStatus_t HCI_SetEventMaskPage2Cmd(uint8 *pMask)
This BT API is used to set the HCI event mask page 2, which is used to determine which events are sup...
hciStatus_t HCI_EXT_ResetSystemCmd(uint8 mode)
This HCI Extension API is used to issue a soft or hard system reset. 
HCI Packet event. 
Definition: hci.h:1156
hciStatus_t HCI_LE_ReadWhiteListSizeCmd(void)
Read the white list. 
hciStatus_t HCI_LE_SetHostChanClassificationCmd(uint8 *chanMap)
Update the current data channel map. 
uint8 length
length of parametric data, in bytes 
Definition: hci.h:1049
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:1011
uint16 connLatency
connection latency 
Definition: hci.h:920
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:989
hciStatus_t HCI_EXT_SetBDADDRCmd(uint8 *bdAddr)
This API is used to set this device's BLE address (BDADDR). 
hciStatus_t HCI_EXT_SetMaxDataLenCmd(uint16 txOctets, uint16 txTime, uint16 rxOctets, uint16 rxTime)
This LE API is used to set the maximum supported Rx and Tx Octets (in bytes) and Time (in us)...
hciStatus_t HCI_LE_TestEndCmd(void)
End the Direct Test Mode test. 
hciStatus_t HCI_ReadLocalVersionInfoCmd(void)
Read the local version information. 
Hardware Error Event. 
Definition: hci.h:1064
hciStatus_t HCI_EXT_BuildRevisionCmd(uint8 mode, uint16 userRevNum)
This HCI Extension API is used set a user revision number or read the build revision number...
hciStatus_t HCI_LE_ClearResolvingListCmd(void)
Remove all devices from the whitelist. 
Authenticated Payload Timeout Expired Event. 
Definition: hci.h:1087
hciStatus_t HCI_LE_SetEventMaskCmd(uint8 *pEventMask)
This LE API is used to set the HCI LE event mask, which is used to determine which LE events are supp...
hciStatus_t HCI_EXT_HaltDuringRfCmd(uint8 mode)
Halt During RF Command. 
uint16 maxTxTime
maximum transmission time 
Definition: hci.h:1124
hciStatus_t HCI_EXT_EnablePTMCmd(void)
This HCI Extension API is used to enable Production Test Mode. 
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:1142
uint16 Interval_Min
minimum connection interval 
Definition: hci.h:1100
hciStatus_t HCI_EXT_SetSlaveLatencyOverrideCmd(uint8 control)
This HCI Extension API is used to to enable or disable suspending slave latency. 
LE Phy Update Complete Event. 
Definition: hci.h:1107
hciStatus_t HCI_ReadLocalSupportedFeaturesCmd(void)
Read the locally supported features. 
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1020
uint8 bleChan
BLE channel. 
Definition: hci.h:981
uint16 numMMissedEvents
number missed connection events 
Definition: hci.h:1209
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1000
uint8 peerAddrType
peer address type 
Definition: hci.h:977
hciStatus_t HCI_LE_EncryptCmd(uint8 *key, uint8 *plainText)
Perform an encryption using AES128. 
uint8 role
role of connection 
Definition: hci.h:932
hciStatus_t HCI_EXT_SetTxPowerCmd(uint8 txPower)
Set the transmit power. 
hciStatus_t HCI_LE_ReadRemoteUsedFeaturesCmd(uint16 connHandle)
Read the remote device's used features. 
Data structure for HCI Command Complete Event Return Parameter. 
Definition: hci.h:1148
uint8 peerAddrType
peer address type 
Definition: hci.h:933
#define B_RANDOM_NUM_SIZE
BLE Random Number Size. 
Definition: bcomdef.h:132
hciStatus_t HCI_EXT_PacketErrorRateCmd(uint16 connHandle, uint8 command)
This function is used to Reset or Read the Packet Error Rate counters for a connection. 
uint16 connTimeout
connection supervision timeout 
Definition: hci.h:937
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1096
hciStatus_t HCI_LE_CreateConnCmd(uint16 scanInterval, uint16 scanWindow, uint8 initFilterPolicy, uint8 addrTypePeer, uint8 *peerAddr, uint8 ownAddrType, uint16 connIntervalMin, uint16 connIntervalMax, uint16 connLatency, uint16 connTimeout, uint16 minLen, uint16 maxLen)
Create a connection. 
LE Connection Complete Event. 
Definition: hci.h:910
void HCI_L2CAPTaskRegister(uint8 taskID)
HCI vendor specific registration for Host L2CAP. 
uint16 numCrcErr
number rx packets with CRC error 
Definition: hci.h:1207
uint16 maxRxOctets
maximum receive bytes 
Definition: hci.h:1125
hciStatus_t HCI_EXT_DeclareNvUsageCmd(uint8 mode)
This HCI Extension API is used to indicate to the Controller whether or not the Host will be using th...
uint16 cmdOpcode
command opcode 
Definition: hci.h:1060
uint16 Latency
slave latency 
Definition: hci.h:1102
uint8 status
status of event 
Definition: hci.h:914
uint8 numDevices
number of discovered devices 
Definition: hci.h:967
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:966
Data Buffer Overflow Event. 
Definition: hci.h:1080
uint16 Timeout
supervision timeout 
Definition: hci.h:1103
hciStatus_t HCI_LE_ReadPhyCmd(uint16 connHandle)
Read the current transmitter and receiver PHY. 
LE Advertising Report Event. 
Definition: hci.h:952
uint8 BLEEventCode
BLE Event Code. 
Definition: hci.h:1110
uint8 numHciCmdPkt
number of HCI command packets 
Definition: hci.h:1059
uint8 rxPhy
RX PHY. 
Definition: hci.h:1114
uint8 linkType
synchronous or asynchronous buffer overflow 
Definition: hci.h:1083
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1010
hciStatus_t HCI_LE_SetScanRspDataCmd(uint8 dataLen, uint8 *pData)
Set the Advertising Scan Response data. 
LE Long Term Key Requested Event. 
Definition: hci.h:1018
osal_event_hdr_t hdr
osal event header 
Definition: hci.h:1132
uint8 cmdStatus
command status 
Definition: hci.h:1058
hciStatus_t HCI_LE_SetResolvablePrivateAddressTimeoutCmd(uint16 rpaTimeout)
Set Resolvable Private Address Timeout. 
hciStatus_t HCI_EXT_ScanReqRptCmd(uint8 mode)
This LE API is used to enable/disable Scan Request Reports. 
uint8 status
status of event 
Definition: hci.h:1074