|
TI BLE Stack API Documentation
2.03.06
|
Functions | |
| bStatus_t | GAP_DeviceInit (uint8 taskID, uint8 profileRole, uint8 maxScanResponses, uint8 *pIRK, uint8 *pSRK, uint32 *pSignCounter) |
| Called to setup the device. Call just once on initialization. More... | |
| bStatus_t | GAP_SetAdvToken (gapAdvDataToken_t *pToken) |
| Called to setup a GAP Advertisement/Scan Response data token. More... | |
| gapAdvDataToken_t * | GAP_GetAdvToken (uint8 adType) |
| Called to read a GAP Advertisement/Scan Response data token. More... | |
| gapAdvDataToken_t * | GAP_RemoveAdvToken (uint8 adType) |
| Called to remove a GAP Advertisement/Scan Response data token. More... | |
| bStatus_t | GAP_UpdateAdvTokens (void) |
| Called to rebuild and load Advertisement and Scan Response data from existing GAP Advertisement Tokens. More... | |
| bStatus_t | GAP_SetParamValue (gapParamIDs_t paramID, uint16 paramValue) |
| Set a GAP Parameter value. Use this function to change the default GAP parameter values. More... | |
| uint16 | GAP_GetParamValue (gapParamIDs_t paramID) |
| Get a GAP Parameter value. More... | |
| bStatus_t | GAP_ConfigDeviceAddr (uint8 addrMode, uint8 *pStaticAddr) |
| Setup the device's address type. If ADDRMODE_PRIVATE_RESOLVE is selected, the address will change periodically. More... | |
| void | GAP_RegisterForMsgs (uint8 taskID) |
| Register your task ID to receive extra (unprocessed) HCI status and complete, and Host events. More... | |
| void | GAP_RegisterBondMgrCBs (gapBondMgrCBs_t *pCBs) |
| Register bond manager call backs. More... | |
| bStatus_t | GAP_DeviceDiscoveryRequest (gapDevDiscReq_t *pParams) |
| Start a device discovery scan. More... | |
| bStatus_t | GAP_DeviceDiscoveryCancel (uint8 taskID) |
| Cancel an existing device discovery request. More... | |
| bStatus_t | GAP_MakeDiscoverable (uint8 taskID, gapAdvertisingParams_t *pParams) |
| Setup or change advertising. Also starts advertising. More... | |
| bStatus_t | GAP_UpdateAdvertisingData (uint8 taskID, uint8 adType, uint8 dataLen, uint8 *pAdvertData) |
| Setup or change advertising and scan response data. More... | |
| bStatus_t | GAP_EndDiscoverable (uint8 taskID) |
| Stops advertising. More... | |
| bStatus_t | GAP_ResolvePrivateAddr (uint8 *pIRK, uint8 *pAddr) |
| Resolves a private address against an IRK. More... | |
| bStatus_t | GAP_EstablishLinkReq (gapEstLinkReq_t *pParams) |
| Establish a link to a slave device. More... | |
| bStatus_t | GAP_TerminateLinkReq (uint8 taskID, uint16 connectionHandle, uint8 reason) |
| Terminate a link connection. More... | |
| bStatus_t | GAP_UpdateLinkParamReq (gapUpdateLinkParamReq_t *pParams) |
| Update the link parameters to a Master or Slave device. More... | |
| bStatus_t | GAP_UpdateLinkParamReqReply (gapUpdateLinkParamReqReply_t *pParams) |
| Reply to a Connection Parameter Update Request sent from a remote device. More... | |
| uint8 | GAP_NumActiveConnections (void) |
| Returns the number of active connections. More... | |
| bStatus_t | GAP_Authenticate (gapAuthParams_t *pParams, gapPairingReq_t *pPairReq) |
| Start the Authentication process with the requested device. This function is used to Initiate/Allow pairing. Called by both master and slave device (Central and Peripheral). More... | |
| bStatus_t | GAP_TerminateAuth (uint16 connectionHandle, uint8 reason) |
| Send a Pairing Failed message and end any existing pairing. More... | |
| bStatus_t | GAP_PasskeyUpdate (uint8 *pPasskey, uint16 connectionHandle) |
| Update the passkey in string format. This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message. More... | |
| bStatus_t | GAP_PasscodeUpdate (uint32 passcode, uint16 connectionHandle) |
| Update the passkey in a numeric value (not string). This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message. More... | |
| bStatus_t | GAP_SendSlaveSecurityRequest (uint16 connectionHandle, uint8 authReq) |
| Generate a Slave Requested Security message to the master. More... | |
| bStatus_t | GAP_Signable (uint16 connectionHandle, uint8 authenticated, smSigningInfo_t *pParams) |
| Set up the connection to accept signed data. More... | |
| bStatus_t | GAP_Bond (uint16 connectionHandle, uint8 authenticated, uint8 secureConnections, smSecurityInfo_t *pParams, uint8 startEncryption) |
| Set up the connection's bound paramaters. More... | |
| bStatus_t GAP_Authenticate | ( | gapAuthParams_t * | pParams, |
| gapPairingReq_t * | pPairReq | ||
| ) |
Start the Authentication process with the requested device. This function is used to Initiate/Allow pairing. Called by both master and slave device (Central and Peripheral).
NOTE: This function is called after the link is established.
| pParams | - Authentication parameters |
| pPairReq | - Enter these parameters if the Pairing Request was already received. NULL, if waiting for Pairing Request or if initiating. |
| bStatus_t GAP_Bond | ( | uint16 | connectionHandle, |
| uint8 | authenticated, | ||
| uint8 | secureConnections, | ||
| smSecurityInfo_t * | pParams, | ||
| uint8 | startEncryption | ||
| ) |
Set up the connection's bound paramaters.
NOTE: This function is called after the link is established.
| connectionHandle | - connection handle of the signing information |
| authenticated | - TRUE if bond is authenticated. |
| secureConnections | - TRUE if bond has Secure Connections strength. |
| pParams | - the connected device's security parameters |
| startEncryption | - whether or not to start encryption |
| bStatus_t GAP_ConfigDeviceAddr | ( | uint8 | addrMode, |
| uint8 * | pStaticAddr | ||
| ) |
Setup the device's address type. If ADDRMODE_PRIVATE_RESOLVE is selected, the address will change periodically.
| addrMode | - GAP Addressing Modes |
| pStaticAddr | - Only used with ADDRMODE_STATIC or ADDRMODE_PRIVATE_NONRESOLVE type. NULL to auto generate otherwise the application can specify the address value |
If return value isn't SUCCESS, the address type remains the same as before this call.
| bStatus_t GAP_DeviceDiscoveryCancel | ( | uint8 | taskID | ) |
Cancel an existing device discovery request.
| taskID | - used to return GAP_DEVICE_DISCOVERY_EVENT |
| bStatus_t GAP_DeviceDiscoveryRequest | ( | gapDevDiscReq_t * | pParams | ) |
Start a device discovery scan.
| pParams | - Device Discovery parameters |
| bStatus_t GAP_DeviceInit | ( | uint8 | taskID, |
| uint8 | profileRole, | ||
| uint8 | maxScanResponses, | ||
| uint8 * | pIRK, | ||
| uint8 * | pSRK, | ||
| uint32 * | pSignCounter | ||
| ) |
Called to setup the device. Call just once on initialization.
NOTE: When initialization is complete, the calling app will be sent the GAP_DEVICE_INIT_DONE_EVENT
| taskID | - Default task ID to send events. |
| profileRole | - GAP Profile Roles: GAP Profile Roles |
| maxScanResponses | - maximum number to scan responses we can receive during a device discovery. |
| pIRK | - pointer to Identity Root Key, NULLKEY (all zeroes) if the app wants the GAP to generate the key. |
| pSRK | - pointer to Sign Resolving Key, NULLKEY if the app wants the GAP to generate the key. |
| pSignCounter | - 32 bit value used in the SM Signing algorithm that shall be initialized to zero and incremented with every new signing. This variable must also be maintained by the application. |
| bStatus_t GAP_EndDiscoverable | ( | uint8 | taskID | ) |
Stops advertising.
| taskID | - of task that called GAP_MakeDiscoverable |
| bStatus_t GAP_EstablishLinkReq | ( | gapEstLinkReq_t * | pParams | ) |
Establish a link to a slave device.
| pParams | - link establishment parameters |
| gapAdvDataToken_t* GAP_GetAdvToken | ( | uint8 | adType | ) |
Called to read a GAP Advertisement/Scan Response data token.
| adType | - Advertisement type to get |
| uint16 GAP_GetParamValue | ( | gapParamIDs_t | paramID | ) |
Get a GAP Parameter value.
| paramID | - parameter ID: GAP Parameter IDs |
| bStatus_t GAP_MakeDiscoverable | ( | uint8 | taskID, |
| gapAdvertisingParams_t * | pParams | ||
| ) |
Setup or change advertising. Also starts advertising.
| taskID | - used to return GAP_DISCOVERABLE_RESPONSE_EVENT |
| pParams | - advertising parameters |
| uint8 GAP_NumActiveConnections | ( | void | ) |
Returns the number of active connections.
| bStatus_t GAP_PasscodeUpdate | ( | uint32 | passcode, |
| uint16 | connectionHandle | ||
| ) |
Update the passkey in a numeric value (not string). This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message.
NOTE: This function is the same as GAP_PasskeyUpdate(), except that the passkey is passed in as a non-string format.
| passcode | - not string - range: 0 - 999,999. |
| connectionHandle | - connection handle. |
| bStatus_t GAP_PasskeyUpdate | ( | uint8 * | pPasskey, |
| uint16 | connectionHandle | ||
| ) |
Update the passkey in string format. This function is called by the application/profile in response to receiving the GAP_PASSKEY_NEEDED_EVENT message.
NOTE: This function is the same as GAP_PasscodeUpdate(), except that the passkey is passed in as a string format.
| pPasskey | - new passkey - pointer to numeric string (ie. "019655" ). This string's range is "000000" to "999999". |
| connectionHandle | - connection handle. |
| void GAP_RegisterBondMgrCBs | ( | gapBondMgrCBs_t * | pCBs | ) |
Register bond manager call backs.
| pCBs | - pointer to Bond Manager Callbacks. |
| void GAP_RegisterForMsgs | ( | uint8 | taskID | ) |
Register your task ID to receive extra (unprocessed) HCI status and complete, and Host events.
| taskID | - Default task ID to send events. |
| gapAdvDataToken_t* GAP_RemoveAdvToken | ( | uint8 | adType | ) |
Called to remove a GAP Advertisement/Scan Response data token.
| adType | - Advertisement type to remove |
| bStatus_t GAP_ResolvePrivateAddr | ( | uint8 * | pIRK, |
| uint8 * | pAddr | ||
| ) |
Resolves a private address against an IRK.
| pIRK | - pointer to the IRK |
| pAddr | - pointer to the Resolvable Private address |
| bStatus_t GAP_SendSlaveSecurityRequest | ( | uint16 | connectionHandle, |
| uint8 | authReq | ||
| ) |
Generate a Slave Requested Security message to the master.
| connectionHandle | - connection handle. |
| authReq | - Authentication Requirements: Bit 2: MITM, Bits 0-1: bonding (0 - no bonding, 1 - bonding) Bit 3: Secure Connections |
| bStatus_t GAP_SetAdvToken | ( | gapAdvDataToken_t * | pToken | ) |
Called to setup a GAP Advertisement/Scan Response data token.
NOTE: The data in these items are stored as low byte first (OTA format). The passed in structure "token" should be allocated by the calling app/profile and not released until after calling GAP_RemoveAdvToken().
| pToken | - Advertisement/Scan response token to write. |
| bStatus_t GAP_SetParamValue | ( | gapParamIDs_t | paramID, |
| uint16 | paramValue | ||
| ) |
Set a GAP Parameter value. Use this function to change the default GAP parameter values.
| paramID | - parameter ID: GAP Parameter IDs |
| paramValue | - new param value |
| bStatus_t GAP_Signable | ( | uint16 | connectionHandle, |
| uint8 | authenticated, | ||
| smSigningInfo_t * | pParams | ||
| ) |
Set up the connection to accept signed data.
NOTE: This function is called after the link is established.
| connectionHandle | - connection handle of the signing information |
| authenticated | - TRUE if the signing information is authenticated, FALSE otherwise |
| pParams | - signing parameters |
| bStatus_t GAP_TerminateAuth | ( | uint16 | connectionHandle, |
| uint8 | reason | ||
| ) |
Send a Pairing Failed message and end any existing pairing.
| connectionHandle | - connection handle. |
| reason | - Pairing Failed reason code. |
| bStatus_t GAP_TerminateLinkReq | ( | uint8 | taskID, |
| uint16 | connectionHandle, | ||
| uint8 | reason | ||
| ) |
Terminate a link connection.
| taskID | - requesting app's task id. |
| connectionHandle | - connection handle of link to terminate or GAP Special Connection Handles |
| reason | - terminate reason. |
| bStatus_t GAP_UpdateAdvertisingData | ( | uint8 | taskID, |
| uint8 | adType, | ||
| uint8 | dataLen, | ||
| uint8 * | pAdvertData | ||
| ) |
Setup or change advertising and scan response data.
NOTE: if the return status from this function is SUCCESS, the task isn't complete until the GAP_ADV_DATA_UPDATE_DONE_EVENT is sent to the calling application task.
| taskID | - task ID of the app requesting the change |
| adType | - TRUE - advertisement data, FALSE - scan response data |
| dataLen | - Octet length of advertData |
| pAdvertData | - advertising or scan response data |
| bStatus_t GAP_UpdateAdvTokens | ( | void | ) |
Called to rebuild and load Advertisement and Scan Response data from existing GAP Advertisement Tokens.
| bStatus_t GAP_UpdateLinkParamReq | ( | gapUpdateLinkParamReq_t * | pParams | ) |
Update the link parameters to a Master or Slave device.
| pParams | - link update parameters |
| bStatus_t GAP_UpdateLinkParamReqReply | ( | gapUpdateLinkParamReqReply_t * | pParams | ) |
Reply to a Connection Parameter Update Request sent from a remote device.
| pParams | - local device's desired connection parameters. |
1.8.12