TI BLE Stack API Documentation  2.03.06
Macros
GAP Bond Manager Parameters

Macros

#define GAPBOND_PAIRING_MODE   0x400
 Pairing Mode: GAP Bond Manager Pairing Modes. Read/Write. Size is uint8. Default is GAPBOND_PAIRING_MODE_WAIT_FOR_REQ.
 
#define GAPBOND_INITIATE_WAIT   0x401
 Pairing Mode Initiate wait timeout. This is the time it will wait for a Pairing Request before sending the Slave Initiate Request. Read/Write. Size is uint16. Default is 1000(in milliseconds).
 
#define GAPBOND_MITM_PROTECTION   0x402
 Man-In-The-Middle (MITM) basically turns on Passkey protection in the pairing algorithm. Read/Write. Size is uint8. Default is 0(disabled).
 
#define GAPBOND_IO_CAPABILITIES   0x403
 I/O capabilities. Read/Write. Size is uint8. Default is GAPBOND_IO_CAP_DISPLAY_ONLY GAP Bond Manager I/O Capabilities.
 
#define GAPBOND_OOB_ENABLED   0x404
 OOB data available for pairing algorithm. Read/Write. Size is uint8. Default is 0(disabled).
 
#define GAPBOND_OOB_DATA   0x405
 OOB Data. Read/Write. size uint8[16]. Default is all 0's.
 
#define GAPBOND_BONDING_ENABLED   0x406
 Request Bonding during the pairing process if enabled. Read/Write. Size is uint8. Default is 0(disabled).
 
#define GAPBOND_KEY_DIST_LIST   0x407
 The key distribution list for bonding. size is uint8. GAP Bond Manager Key Distribution. Default is sEncKey, sIdKey, mIdKey, mSign enabled.
 
#define GAPBOND_DEFAULT_PASSCODE   0x408
 The default passcode for MITM protection. size is uint32. Range is 0 - 999,999. Default is 0.
 
#define GAPBOND_ERASE_ALLBONDS   0x409
 Erase all of the bonded devices. Write Only. No Size.
 
#define GAPBOND_AUTO_FAIL_PAIRING   0x40A
 TEST MODE (DO NOT USE) to automatically send a Pairing Fail when a Pairing Request is received. Read/Write. size is uint8. Default is 0 (disabled).
 
#define GAPBOND_AUTO_FAIL_REASON   0x40B
 TEST MODE (DO NOT USE) Pairing Fail reason when auto failing. Read/Write. size is uint8. Default is 0x05 (SMP_PAIRING_FAILED_NOT_SUPPORTED).
 
#define GAPBOND_KEYSIZE   0x40C
 Key Size used in pairing. Read/Write. size is uint8. Default is 16.
 
#define GAPBOND_AUTO_SYNC_WL   0x40D
 Clears the White List adds to it each unique address stored by bonds in NV. Read/Write. Size is uint8. Default is FALSE.
 
#define GAPBOND_BOND_COUNT   0x40E
 Gets the total number of bonds stored in NV. Read Only. Size is uint8. Default is 0 (no bonds).
 
#define GAPBOND_BOND_FAIL_ACTION   0x40F
 Possible actions Central may take upon an unsuccessful bonding. Write Only. Size is uint8. Default is 0x02 (Terminate link upon unsuccessful bonding).
 
#define GAPBOND_ERASE_SINGLEBOND   0x410
 Erase a single bonded device. Write only. Must provide address type followed by device address.
 
#define GAPBOND_SECURE_CONNECTION   0x411
 Defines Secure Connections usage. Read/Write. size is uint8. Secure Connections only. GAPBOND_SECURE_CONNECTIONS_DEFINES.
 
#define GAPBOND_ECCKEY_REGEN_POLICY   0x412
 Count of how many times an ECC keypair may be reused before regeneration. Write only. Range is 0-254. Default is 0. Secure Connections only. GAP Bond Manager ECC Re-use count before regeneration.
 
#define GAPBOND_ECC_KEYS   0x413
 Use application requested public-private keypair for Secure Connections. Read/Write. size is gapBondEccKeys_t. Secure Connections only.
 
#define GAPBOND_REMOTE_OOB_SC_ENABLED   0x414
 Secure Connections OOB data from remote device availabe. Read/Write. Size is uint8. Default is 0 (disabled). Secure Connections only.
 
#define GAPBOND_REMOTE_OOB_SC_DATA   0x415
 Secure Connections OOB data. Read/Write. Size is gapBondOobSC_t. Default is all 0's. Secure Connections only.
 
#define GAPBOND_LOCAL_OOB_SC_ENABLED   0x416
 Secure Connection local OOB data is available. Read/Write. Size is uint8. Default is 0 (disabled). Secure Connections only.
 
#define GAPBOND_LOCAL_OOB_SC_DATA   0x417
 Local OOB Data. Read/Write. size uint8[16]. Default is all 0's. Secure Connections only.
 
#define GAPBOND_LRU_BOND_REPLACEMENT   0x418
 Remote Least Recently Used Bond when newly bonded device is added and the all entries are full. Read/Write. size uint8. Default is FALSE.
 

Detailed Description