|
TI BLE Stack API Documentation
2.03.05
|
#include <gap.h>
Public Attributes | |
| uint8 | eventType |
| Advertise Event Type: GAP Advertising Event Types. | |
| uint8 | initiatorAddrType |
| Initiator's address type: Address Types as defined by BLE Spec. | |
| uint8 | initiatorAddr [6] |
| Initiator's addr - used only with connectable directed eventType (ADV_EVTTYPE_CONNECTABLE_DIRECTED). | |
| uint8 | channelMap |
| Channel Map: Bit mask GAP Advertisement Channel Map. | |
| uint8 | filterPolicy |
| Filer Policy: GAP Advertiser Filter Scan Parameters. Ignored when directed advertising is used. | |
Advertising Parameters
1.8.12