TI BLE Stack API Documentation  2.03.03
Public Attributes | List of all members
hciEvt_BLERemoteConnParamReq_t Struct Reference

LE Remote Connection Parameter Request Event. More...

#include <hci.h>

Public Attributes

osal_event_hdr_t hdr
 osal event header
 
uint8 BLEEventCode
 BLE Event Code.
 
uint8 status
 status of event
 
uint16 connHandle
 connection handle
 
uint16 Interval_Min
 minimum connection interval
 
uint16 Interval_Max
 maximum connection interval
 
uint16 Latency
 slave latency
 
uint16 Timeout
 supervision timeout
 

Detailed Description

LE Remote Connection Parameter Request Event.


The documentation for this struct was generated from the following file: