TI BLE Stack API Documentation  2.03.03
Public Attributes | List of all members
hciEvt_BLEDataLengthChange_t Struct Reference

LE Data Length Change Event. More...

#include <hci.h>

Public Attributes

osal_event_hdr_t hdr
 osal event header
 
uint8 BLEEventCode
 BLE Event Code.
 
uint16 connHandle
 connection handle
 
uint16 maxTxOctets
 maximum transmission bytes
 
uint16 maxTxTime
 maximum transmission time
 
uint16 maxRxOctets
 maximum receive bytes
 
uint16 maxRxTime
 maximum receive time
 

Detailed Description

LE Data Length Change Event.


The documentation for this struct was generated from the following file: