TRNG Parameters. More...
#include <TRNG.h>
Data Fields | |
TRNG_ReturnBehavior | returnBehavior |
TRNG_CallbackFxn | callbackFxn |
uint32_t | timeout |
void * | custom |
TRNG Parameters.
TRNG Parameters are used to with the TRNG_open() call. Default values for these parameters are set using TRNG_Params_init().
TRNG_ReturnBehavior TRNG_Params_::returnBehavior |
Blocking, callback, or polling return behavior
TRNG_CallbackFxn TRNG_Params_::callbackFxn |
Callback function pointer
uint32_t TRNG_Params_::timeout |
Timeout before the driver returns an error in TRNG_RETURN_BEHAVIOR_BLOCKING
void* TRNG_Params_::custom |
Custom argument used by driver implementation